System Settings

For best possible performance, machine vision cameras require suitable accessories and a proper setup of your system.

Find tested accessories for your Allied Vision camera on our website: https://www.alliedvision.com/en/products

All operating systems

GigE cameras

  • Use Category 6 or higher rated Ethernet cables

  • Use only one camera per Ethernet port

Optimize the NIC settings:

  • Disable all unused NIC services and protocols (for example, activate only filter drivers for IPv4 and GigE on Windows)

  • Enable Auto Negotiation (not Fixed Link Speed)

  • Windows only: Use the Filter Driver provided with Vimba X

  • Windows: Enable Jumbo Frames on your NIC

  • Detailed information is availabe in the documentation for your camera, see https://www.alliedvision.com/en/support

USB cameras

Linux and ARM

Additionally to the topics mentioned above, consider the following recommendations.

Real-time thread scheduling policies

You can enable real-time thread scheduling policies by setting EnableLinuxRealTimeSchedulingPolicies in VmbC.xml to “true”. Additionally, the user must be appropriately configured on the host.

In /etc/security/limits.conf, insert the following lines (replacing username with the user’s username):

username - rtprio 99
username - memlock unlimited

In /etc/pam.d/common-session, insert the following line:

session required pam_limits.so

Then log out and log in. Run, for example, the asynchronous grab example for VmbC and, in another terminal, check that the output of “ps -eLo pid,tid,cls,rtprio,pri,cmd | grep AsynchronousGrab_VmbC” looks something like:

12867   13079  FF     70 110 ./AsynchronousGrab_VmbC

If the configuration failed, the output looks something like:

19029   19250  TS      -  19 ./AsynchronousGrab_VmbC

and the logs will contain a warning that includes the text “normal scheduling will be attempted”.

Additional settings

If the real-time scheduling does not work, try the following:

In /etc/security/limits.conf, insert

username soft rtprio 50
username hard rtprio 99
username soft nice -10
username hard nice -20
username soft memlock 512000
username hard memlock unlimited

Make all the same insertions in /etc/security/limits.d/90-realtime.conf (if present) as were inserted in /etc/security/limits.conf above.

For non-Debian/Ubuntu systems, insert “session required pam_limits.so” also in /etc/pam.d/system-auth and /etc/pam.d/password-auth, as was inserted in /etc/pam.d/common-session above.

For non-interactive use, insert “session required pam_limits.so” also in /etc/pam.d/common-session-noninteractive, as was inserted in /etc/pam.d/common-session above.

USB cameras

Increasing the USBFS buffer size:

By default, the USBFS buffer size may be 16 MB. This value is too low for image sizes > 2 MB or high frame rates. Check the USBFS buffer size:

cat /sys/module/usbcore/parameters/usbfs_memory_mb

Increase the USBFS buffer size until the next reboot (here: example value 1000):

sudo sh -c 'echo 1000 > /sys/module/usbcore/parameters/usbfs_memory_mb'

Increase the USBFS buffer size permanently

To increase the buffer size permanently, add the kernel parameter usbcore.usbfs_memory_mb=1000 the bootloader configuration. If and how this is possible depends on the bootloader on your system.

Note

Before changing the bootloader configuration, create a backup of your system.

A faulty bootloader may cause that your system doesn’t start up. A fix might require an external boot media or reinstallation of the system. Note that changing the bootloader configuration is at your own risk.

Syslinux: Edit /boot/extlinux/extlinux.conf, add usbcore.usbfs_memory_mb=1000 to the APPEND line, and reboot the system.

If you have installed GRUB 2:

  1. Open /etc/default/grub. Replace: GRUB_CMDLINE_LINUX_DEFAULT=”quiet splash” (or other contents within the quotation marks depending on your system) with: GRUB_CMDLINE_LINUX_DEFAULT=”quiet splash usbcore.usbfs_memory_mb=1000”

  2. Update grub: sudo update-grub and reboot the system.

Other bootloaders: To configure additional kernel parameters of other bootloaders, please see the manual of your bootloader.

Increasing MaxTransferSize:

If frames are incomplete, you can try to increase the MaxTransferSize in the VimbaUSBTL.xml file to 1,048,576 or higher.

GigE cameras

Setting the MTU of the internal host adapter: Set the MTU of the internal host adapter, assuming the camera is connected to Ethernet port eth0:

sudo ip link set eth0 down
sudo ip link set eth0 mtu 9000
sudo ip link set eth0 up

Additionally, set the feature GVSPBurstSize to 32 or higher for usage with 5GigE cameras.

Increasing the OS receive buffer size:

If your use case requires high bandwidth, we recommend increasing the OS receive buffer size (these settings affect all types of connections on the system):

sudo sysctl -w net.core.rmem_max=33554432
sudo sysctl -w net.core.wmem_max=33554432
sudo sysctl -w net.core.rmem_default=33554432
sudo sysctl -w net.core.wmem_default=33554432

Optimizing your SOM

To optimize your NVIDIA Jetson SOM, read: https://www.alliedvision.com/assets/documents/products/software/embedded/Optimizing-Performance-Jetson_appnote.pdf

macOS

Additionally to the topics mentioned above, consider the following recommendations.

USB cameras

For best performance on MacMini, use the USB ports. They have a higher performance than the Thunderbolt ports combined with a USB adapter.

GigE cameras

MTU size and Speed

Check and set the MTU size and Speed:

  • Open System Settings

  • Go to Network

  • Select the relevant interface and select Details.

  • Set MTU size to Jumbo Frames and set the highest possible speed for your interface.

Increase the GigE receive buffer size

Display the current settings:

# Display current settings
# Current UDP receive buffer size
sysctl -n net.inet.udp.recvspace
# Default: 131.072

# Current TCP receive buffer size
sysctl -n net.inet.tcp.recvspace
# Default: 131.072

# Current TCP send buffer size
sysctl -n net.inet.tcp.sendspace
# Default: 131.072

# The buffer sizes are limited by the maxsockbuf value
sysctl -a | egrep nmbcl\|maxsockb
# Default:
# maxsockbuf=8.388.608
# nmbclusters=262.144

# recvspace + sendspace < maxsockbuf
# maxsockbuf = (nmbclusters*2048)/16

Note that after rebooting with a new nmbclusters /ncl value, the maxsockbufs value is not necessarily adjusted to its maximum automatically. You can adjust the value via sysctl -w as described below.

Prepare increasing the receive buffer size (requires disabling System Integrity Protection):

Warning

Disabling SIP (System Integrity Protection) fully or partly is done at your own risk. Without SIP, your computer is vulnerable to malicious code. Disabling System Integrity Protection might lead to unknown system behavior.

  1. While turning on your Mac, press and hold the power button until the boot menu appears.

  2. Select Utilities and launch the Terminal.

  3. To disable System Integrity Protection at your own risk, run:

    csrutil disable
    
  4. Reboot your Mac as usual.

  5. Open a Terminal window and run the commands:

    sudo nvram boot-args="ncl=524288"
    sudo shutdown -r now`
    

After the reboot is complete, the next steps are different for non-persistent and persistent changes.

Non-persistent changes:

Open a Terminal window and run the commands:

sudo sysctl -w kern.ipc.maxsockbuf=67108864
sudo sysctl -w net.inet.udp.recvspace=33554432

Persistent changes:

Open a Terminal window and run the command:

sudo nano /Library/LaunchDaemons/AlliedVision.sysctl.plist

Paste the following lines into the editor and save the file:

<?xml version="1.0" encoding="UTF-8"?>
<!DOCTYPE plist PUBLIC "-//Apple//DTD PLIST 1.0//EN" "http://www.apple.com/DTDs/PropertyList-1.0.dtd">
<plist version="1.0">
<dict>
    <key>Label</key>
    <string>sysctl</string>
    <key>ProgramArguments</key>
    <array>
        <string>/usr/sbin/sysctl</string>
        <string>-w</string>
        <string>kern.ipc.maxsockbuf=67108864</string>
        <string>net.inet.udp.recvspace=33554432</string>
    </array>
    <key>RunAtLoad</key>
    <true/>
</dict>
</plist>

Because changes to the boot arguments were made, SIP (System Integrity Protection) cannot fully be enabled again, because this would remove the boot-arg and therefore also reset the depending receive buffer size to its default value.

Leave SIP disabled: If you do nothing, SIP is disabled.

Partly enable SIP:

  1. While turning on your Mac, press and hold the power button until the boot menu appears.

  2. Select Utilities and launch the Terminal. Run:

    csrutil enable --without nvram
    
  3. Restart your Mac.

Restore default values:

  1. Temporarily disable System Integrity Protection (see above).

  2. Open a terminal window and run the commands:

    sudo nvram boot-args=""
    sudo shutdown -r now
    
  3. Enable System Integrity Protection again (see above).