About Vimba X

Vimba X is Allied Vision’s fully GenICam-compliant SDK.

  • You can use GenICam-compliant cameras and transport layers for all camera interfaces from all manufacturers.

  • Usage with cameras and TLs from third-party vendors is free of charge. You don’t need any additional licenses.

  • Advanced configuration of devices such as frame grabbers and of the TLs is possible.

Compatibility

Tested operating systems, transport layers and cameras are listed in the release notes.

Note

Alvium MIPI camera users: The camera driver must be installed before using Vimba. It is available at:

https://github.com/alliedvision

Note

FireWire (IEEE 1394) is not supported because this interface is not GenICam-compliant.

Supported features

Additionally to GenICam-compliant features, Vimba X supports legacy chunk and event features of Manta, Mako, Goldeye, and Prosilica GigE cameras.

Installation

Windows

To automatically install the USB driver, connect your USB camera before starting the Vimba X installation. After the installation, you can always use Vimba Driver Installer, see Driver Installer Manual.

Silent installation: The VimbaX_Install*.exe can be called with the following command line options:

  • /S : Silent install

  • /D : Sets the default installation directory

The VimbaX_Uninstall.exe can be called with the following command line options:

/S : Silent uninstall

Linux and ARM

To install Vimba X:

  • Uncompress the archive with the command tar -xf ./VimbaX.tgz to a directory you have writing privileges for like /opt. Under this directory, Vimba X will be installed in its own folder. In the following, we will refer to this path as [InstallDir].

  • Go to [InstallDir]/cti/and call (as needed, using sudo) Install_GenTL_Path.sh.

  • Reboot your system.

To uninstall the transport layers, call (as needed, using sudo) Uninstall_GenTL_Path.sh.

If you have issues, see Troubleshooting.

macOS

Vimba X comes as a .dmg file. Do not drag & drop it into the Applications folder.

Install Vimba X

  1. Double-click the .dmg file to mount it.

  2. Open Vimba X installer.pkg and follow the instructions. If you get an error message, go to Settings → Privacy & Security, select “App Store and identified developers” and click “Open Anyway” for “Vimba X Installer.pkg”.

Now you can start working with Vimba X.

To install Vimba X via command line:

  1. Extract the tar.gz file and open a terminal in this directory.

sudo hdiutil attach Vimba\ X\ Installer.pkg
sudo installer -package /Volumes/Vimba\ X\ Vimba\ X\ Installer.pkg -target /
sudo hdiutil detach /Volumes/Vimba\ X

Please log out and then log in again. Please make sure to quit the Terminal app if it is still open, so that it can find the new environment variable when you open it again. Opening a new Terminal window without quitting the application is not sufficient.

Uninstall Vimba X

To uninstall Vimba X, use the Vimba X Removal Assistant.