Firmware Updater Manual

Firmware Updater

Vimba X Firmware Updater supports firmware uploads to Alvium, Goldeye, and Goldeye Pro cameras. New firmware for each connected camera is automatically detected and selected. You can update several cameras in one step. Uploading older firmware to the camera is also possible. If you prefer to upload firmware via command line, see Command line Firmware Updater.

On Windows and Linux, Vimba X Firmware Updater is available in the Vimba X install directory/bin.

On macOS, Firmware Updater is available as Vimba X Firmware Updater app.

See also

Download the latest firmware from our website:

Uploading firmware

To upload new firmware to your cameras, perform the following steps:

  1. Connect your Allied Vision cameras and start Vimba X Firmware Updater.

  2. Click Open and select a firmware container file. Optional: Click Info to get details about the selected firmware.

  3. Click Update cameras to upload the automatically selected firmware to your cameras.

Firmware Updater

Firmware Updater

If the firmware has a lower version number, Vimba X Firmware Updater interprets this as a older version and doesn’t update the firmware automatically.

To select the new firmware manually, go to the New firmware drop-down list.

Select firmware

Select firmware

Aborting a firmware upload

The firmware upload to several cameras takes some time. During the upload, Abort finishes the upload to the current camera, but does not upload firmware to the next models.

Troubleshooting

If your camera is not detected or the firmware cannot be updated:

  • Make sure no other application uses the camera.

  • Check if the camera works with Vimba X Viewer.

  • Reboot the system.

  • Start the firmware upload again. If it does not work, start the command line Firmware Updater and use repair mode or contact our support team: https://www.alliedvision.com/en/company/contact-us/technical-support-and-repair-rma

  • Windows only: with USB cameras, start Vimba Driver Installer and make sure the Vimba USB driver is in use.

  • If you connected your USB camera to a hub, unplug the hub from the PC and disconnect its power supply. Reconnect it and try again.

  • Connect your USB camera to a different USB 3.0 input or a different hub.

Command line Firmware Updater

On Windows and Linux, Vimba X Firmware Updater Console is available in the Vimba X install directory/bin.

On macOS, it is available at /Applications/Vimba\ X/Firmware\ Updater.app/Contents/bin/VimbaXFirmwareUpdaterConsole.

To update firmware via command line, use FWUpdaterConsole.exe. This tool provides two main functionalities:

  • --show or -s displays information about camera firmware or a firmware file.

  • --write or -w performs the actual update.

See the following list of use cases:

Use case

Parameters

Show device info for list of cameras

--show --device “list of ids”

Show a list of matching firmware sets
for all cameras

--show --container “file” --device all

Show detailed info about matching
firmware sets for one camera

--show --container “file” --device “id”

Show firmware set info for one set

--show --container “file” --index “index”

Show firmware set info for list of sets

--show --container “file” --index
“list of indices”

Show firmware set info for whole container

--show --container “file”

Write one firmware set to one camera

--write --container “file” --device
“id” --index “index”

Write ‘best’ (latest) firmware set to list
of cameras

--write --container “file” --device
“list of ids”

Write ‘best’ (latest) firmware set to
all cameras

--write --container “file” --device all

Write one firmware set to one camera
in repair mode

--write --repair --container “file”
--device “id” --index “index”

The following options may be added to the “show” or ” the “write” functionality:

Option

Parameters

Show full information

--verbose, -v

Force writing

--force, -f

Repair device firmware during write

--repair, -r

Tip

By calling FWUpdaterConsole --help [command/option], you get more details about the tool or its parameters.