Python API Manual
Introduction to the API
The Python API (VmbPy) is a Python wrapper around the VmbC API. It provides all functions from VmbC, but enables you to program with less lines of code.
We recommend using VmbPy for:
Quick prototyping
Getting started with programming machine vision or embedded vision applications
Easy interfacing with deep learning frameworks and libraries such as OpenCV via NumPy arrays
Is this the best API for you?
Vimba X provides three APIs:
The Python API is ideal for quick prototyping. We also recommend this API for an easy start with machine vision or embedded vision applications. For best performance and deterministic behavior, the C and C++ APIs are a better choice. To ease migration, the structure of VmbPy is very similar to VmbCPP.
The C API is easy-to-use, but requires more lines of code than the Python API. It can also be used as API for C++ applications.
The C++ API has an elaborate class architecture. It is designed as a highly efficient and sophisticated API for advanced object-oriented programming including the STL (standard template library), shared pointers, and interface classes. If you prefer an API with less design patterns, we recommend the C API.
All Vimba X APIs cover the following functions:
Listing currently connected cameras
Controlling camera features
Receiving images from the camera
Getting notifications about camera connections and disconnections
Compatibility
Supported operating systems and cameras are listed in the Release Notes for your operating system.
Compatible Python version: Python 3.10. or higher. For 64-bit operating systems, we recommend using a 64-bit Python interpreter.
Installation
Prerequisites
Note
Python is not provided with the Vimba X SDK. To use the Python API, install Python version 3.10 or higher as described below.
Note
Updating Vimba X to a higher version does not automatically update any installed Vimba X Python site packages. Please install the .whl file of VmbPy as described below again manually, especially if the error “Invalid VmbC Version” occurs.
Installing Python - Windows
Tip
If your system requires multiple, coexisting Python versions, consider using pyenv-win, available at https://github.com/pyenv-win/pyenv-win to install and maintain multiple Python installations.
Download the latest Python release from python.org, available at https://www.python.org/downloads/windows/.
Execute the downloaded installer and ensure that the latest pip version is installed.
If you don’t have admin privileges for all directories, read the instructions for all operating systems below.
To verify the installation, open the command prompt and enter:
python --version
python -m pip --version
Please ensure that the Python version is 3.10 or higher and pip uses this Python version.
Optionally, install NumPy and OpenCV as extras. NumPy enables conversion of VmbPy.Frame
objects to numpy arrays. Opencv ensures that the numPy arrays are valid OpenCV images.
# Install Python with NumPy and OpenCV export
python -m pip install '/path/to/vmbpy-X.Y.Z-py-none-any.whl[numpy,opencv]'
Installing Python - Linux
On Linux systems, the Python installation process depends heavily on the distribution. If python 3.10 is not available for your distribution or your system requires multiple python versions to coexist, use pyenv, available at https://realpython.com/intro-to-pyenv/ instead.
If you don’t have admin privileges for all directories, read the instructions for all operating systems below.
Install or update python 3.10 with the packet manager of your distribution.
Install or update pip with the packet manager of your distribution.
To verify the installation, open a console and enter:
python3 --version
python3 -m pip --version
Optionally, install NumPy and OpenCV as extras. NumPy enables conversion of VmbPy.Frame
objects to numpy arrays. Opencv ensures that the numPy arrays are valid OpenCV images.
# Install Python with NumPy and OpenCV export
python3 -m pip install '/path/to/vmbpy-X.Y.Z-py-none-any.whl[numpy,opencv]'
Yocto on NXP i.MX8 and OpenCV
The GPU in the i.MX8 systems requires using the system-wide opencv-python package.
When you create the Python environment, please use the --system-site-packages
flag to include the system-wide OpenCV package.
If you don’t set up a separate environment, a warning is shown during the VmbPy installation. You can ignore this warning.
Installing Python - macOS
Download the latest Python release from python.org, available at https://www.python.org/downloads/macos/.
Execute the downloaded installer.
Check if Python and pip are installed:
python3 --version
pip3 --version
Install VmbPy
VmbPy is provided as .whl file in the Vimba X installation directory. We recommed using this fle. You can install it
with pip install (Windows) or pip3 install (some Linux distros and macOS).
pip documentation: https://pip.pypa.io/en/stable/cli/pip_install/
The sources of VmbPy are available on GitHub:
https://github.com/alliedvision/VmbPy
Note
Please note that Allied Vision can offer only limited support if an application uses a modified version of the API.
Additionally, you can install VmbPy from PyPI. Note that this does not include other essential Vimba X components such as the transport layers and drivers.
General aspects of the API
Entry point
The entry point of VmbPy is the Vimba X singleton representing the underlying Vimba X System.
Entity documentation
All entities of the Python API are documented via docstring.
Context manager
The Vimba X singleton implements a context manager. The context entry initializes:
System features discovery
Interface and transport layer (TL) detection
Camera detection
The context entry always handles:
API startup (including an optional method for advanced TL configuration) and shutdown
Opening and closing cameras, interfaces, and TLs
Feature discovery for the opened entity
Always call all methods for Camera, Feature, and Interface within the scope of a with statement:
from vmbpy import *
with VmbSystem.get_instance() as vmb:
cams = vmb.get_all_cameras()
See also
For details about the optional method for advanced TL configuration, see the SDK Manual, chapter TL activation and deactivation and the ListCameras example.
Classes
The Camera class implements a context manager. On entering the Camera’s context, all camera features
are detected and can be accessed only within the with statement. Additionally to getting and setting
camera features, the Camera class handles the camera access mode (default: Full Access).
Note
For changing the pixel format, always use the convenience functions instead of the camera feature, see section Changing the pixel format.
The Frame class stores raw image data and metadata of a single frame. The Frame class implements deepcopy semantics. Additionally, it provides methods for pixel format conversion and ancillary data access. Like all objects containing Features, AncillaryData implements a context manager that must be entered before features can be accessed. The Frame class offers methods for NumPy and OpenCV export.
The following code snippet shows how to:
Acquire a single frame
Convert the pixel format to Mono8
Store it using opencv-python
import cv2
from vmbpy import *
with VmbSystem.get_instance() as vmb:
cams = vmb.get_all_cameras()
with cams[0] as cam:
frame = cam.get_frame()
frame.convert_pixel_format(PixelFormat.Mono8)
cv2.imwrite('frame.jpg', frame.as_opencv_image())
Tip
Optionally, this transformation can use a pre allocated destination_buffer to reduce possible overhead from memory allocations and garbage collection (see the convert_pixel_format.py example).
The Interface class contains all data of detected hardware interfaces that cameras are connected to.
An Interface has associated features. The Interfaces can be queried from the VmbSystem and Interface
features can be accessed within the with scope of VmbSystem. The Interface class does not implement
a context manager on its own. The following code snippet prints all features of the first detected Interface.
from vmbpy import *
with VmbSystem.get_instance() as vmb:
interface = vmb.get_all_interfaces()[0]
for feat in interface.get_all_features():
print(feat)
API usage
See also
For a quick start, we recommend using the examples.
Listing cameras
See also
To list available cameras, see the list_ cameras.py example
Cameras are detected automatically on context entry of the Vimba X instance. The order in which detected cameras are listed is determined by the order of camera discovery and therefore not deterministic. The discovery of GigE cameras may take several seconds. Before opening cameras, camera objects contain all static details of a physical camera that do not change throughout the object’s lifetime such as the camera ID and the camera model.
Cameras and hardware interfaces such as USB can be detected at runtime by registering a callback at the Vimba X instance. The following code snippet registers a callable, creating a log message as soon as a camera or an interface is connected or disconnected. It runs for 10 seconds waiting for changes of the connected hardware.
from time import sleep
from vmbpy import *
@ScopedLogEnable(LOG_CONFIG_INFO_CONSOLE_ONLY)
def print_device_id(dev , state ):
msg = 'Device: {}, State: {}'.format(str(dev), str(state ))
Log.get_instance(). info(msg)
with VmbSystem.get_instance() as vmb:
vmb.register_camera_change_handler(print_device_id)
vmb.register_interface_change_handler(print_device_id)
sleep(10)
Listing features
See also
To list the features of a camera and its physical interface, see the list_ features.py example.
Accessing features
As an example for reading and writing a feature, the following code snippet reads the current exposure time and increases it. Depending on your camera model and camera firmware, feature naming may be different.
from vmbpy import *
with VmbSystem.get_instance() as vmb:
cams = vmb.get_all_cameras()
with cams[0] as cam:
exposure_time = cam.ExposureTime
time = exposure_time.get()
inc = exposure_time.get_increment()
exposure_time.set(time + inc)
Acquiring images
The Camera class supports synchronous and asynchronous image acquisition. For high performance, acquire frames asynchronously and keep the registered callable as short as possible.
See also
The SDK Manual, section Synchronous and asynchronous image acquisition, provides background knowledge. The C API Manual, section Image Capture vs. Image Acquisition, provides detailed information about functions of the underlying C API.
To activate “alloc and announce” (optional): Use the optional parameter /x to overwrite
allocation_ mode, see the AsynchronousGrab example.
# Synchronous grab
from vmbpy import *
with VmbSystem.get_instance() as vmb:
cams = vmb.get_all_cameras()
with cams[0] as cam:
# Aquire single frame synchronously
frame = cam.get_frame()
# Aquire 10 frames synchronously
for frame in cam.get_frame_generator(limit=10):
pass
Acquire frames asychronously by registering a callable being executed with each incoming frame:
# Asynchronous grab
import time
from vmbpy import *
def frame_handler(cam: Camera, stream: Stream, frame: Frame):
cam.queue_frame(frame)
with VmbSystem.get_instance() as vmb:
cams = vmb.get_all_cameras()
with cams[0] as cam:
cam.start_streaming(frame_handler)
time.sleep(5)
cam.stop_streaming()
The asynchronous_ grab.py example shows how to grab images and prints information about the acquired frames to the console.
The asynchronous_ grab_ opencv.py example shows how to grab images. It runs for 5 seconds and displays the images via OpenCV.
Changing the pixel format
Note
Always use the convenience functions instead of the PixelFormat feature of the Camera.
To easily change the pixel format, always use the convenience functions instead
of the PixelFormat feature of the Camera. The convenience function set_pixel_format(fmt)
changes the Camera pixel format by passing the desired member of the PixelFormat enum. When
using the PixelFormat feature (not recommended), a correctly pre-formatted string has to be used
instead.
Before image acquisition is started, you can get and set pixel formats within the Camera class:
# Camera class methods for getting and setting pixel formats
# Apply these methods before starting image acquisition
get_pixel_formats() # returns a tuple of all pixel formats supported by the camera
get_pixel_format() # returns the current pixel format
set_pixel_format(fmt) # enables you to set a new pixel format
Note
The pixel format cannot be changed while the camera is acquiring images.
After image acquisition in the camera, the Frame contains the pixel format of the camera. Now you can
convert the pixel format with the convert_ pixel_ format() method.
See also
See the AsynchronousGrab example, it contains a pixel format conversion.
Listing chunk data
Note
To use the chunk feature, make sure your camera supports it.
Chunk data are image metadata such as the exposure time that are available in the Frame. To activate chunk, see the user documentation of your camera.
# Before using chunk, open your camera as usual
def chunk_callback(features: FeatureContainer):
chunk_timestamp = features.ChunkTimestamp.get()
print(f'Chunk callback executed, ChunkTimestamp={chunk_timestamp}')
def frame_callback(cam: Camera, stream: Stream, frame: Frame):
print(f'Frame callback executed for {frame}')
# Calling this method only works if chunk mode is activated!
frame.access_chunk_data(chunk_callback)
stream.queue_frame(frame)
try:
cam.start_streaming(frame_callback),
time.sleep(1)
finally:
cam.stop_streaming()
See also
The list_ chunk_ data.py example shows in detail how to list chunk data such as the frame count or feature values such as the exposure time. See List Chunk data.
Loading and saving user sets
See also
To save the camera settings as a user set in the camera and load it, use the user_ set.py example.
Loading and saving settings
Additionally to the user sets stored in the camera, you can save the feature values as an XML file to your host PC. For example, you can configure your camera with Vimba X Viewer, save the settings, and load them with any Vimba X API.
See also
See the load_ save_ settings.py example, see Load and save settings.
Software trigger
Software trigger commands are supported by all Allied Vision cameras. To get started with triggering and explore the possibilities, you can use Vimba X Viewer. To program a software trigger application, use the following code snippet.
# Software trigger for continuous image acquisition
import time
from vmbpy import *
def handler(cam: Camera, stream: Stream, frame: Frame):
print('Frame acquired: {}'.format(frame), flush=True)
cam.queue_frame(frame)
def main():
with VmbSystem.get_instance() as vmb:
cam = vmb.get_all_cameras()[0]
with cam:
cam.TriggerSource.set('Software')
cam.TriggerSelector.set('FrameStart')
cam.TriggerMode.set('On')
cam.AcquisitionMode.set('Continuous')
try:
cam.start_streaming(handler)
time.sleep(1)
cam.TriggerSoftware.run()
time.sleep(1)
cam.TriggerSoftware.run()
time.sleep(1)
cam.TriggerSoftware.run()
finally:
cam.stop_streaming()
if __name__ == '__main__':
main()
Trigger over Ethernet - Action Commands
You can broadcast a trigger signal simultaneously to multiple GigE cameras via GigE cable. Action Commands must be set first to the camera(s) and then to the API, which sends the Action Commands to the camera(s).
See also
Find more details in the application note: Trigger over Ethernet (ToE) - Action Commands
Multithreading
To get started with multithreading, use the multithreading_opencv.py example, see Multithreading OpenCV. You can use the example with one or multiple cameras. The FrameConsumer thread displays images of the first detected camera via OpenCV in a window of 480 x 480 pixels, independent of the camera’s image size. The example automatically constructs, starts, and stops FrameProducer threads for each connected or disconnected camera.
Migrating to the C or C++ API
The Python API is optimized for quick and easy prototyping. To migrate to the C API, we recommend using VmbPy’s extensive logging capabilities. In the log file, the order of operations is the same as in the C API. Migrating to the C++ API is eased by similar names of the functions and by a similar API structure.
Troubleshooting
Frequent questions:
To use the VmbPy API, the installation of a compatible C API version and Image Transform version is required. To check the versions, use
VmbSystem.get_ version().Error: “Invalid VmbC Version” although the correct C API version is installed: Updating Vimba X does not automatically update any installed VmbPy site packages. Please perform the installation again manually.
For changing the pixel format, always use the convenience functions instead of the camera feature, see section Changing the pixel format.
For general issues, see Troubleshooting.
Logging
You can enable and configure logging to:
Create error reports
Prepare the migration to the C API or the C++ API
Tip
If you want to send a log file to our Technical Support team, always use logging level Trace.
Logging levels
The Python API offers several logging levels. The following code snippet shows how to enable logging with level Warning. All messages are printed to the console.
from vmbpy import *
with VmbSystem.get_instance() as vmb:
vmb.enable_log(LOG_CONFIG_WARNING_CONSOLE_ONLY)
log = Log.get_instance()
log.critical('Critical, visible')
log.error('Error, visible')
log.warning('Warning , visible')
log.info('Info, invisible')
log.trace('Trace, invisible')
vmb.disable_log()
The logging level Trace enables the most detailed reports. Additionally, you can use it to prepare the
migration to the C API or the C++ API. Trace is always used with the TraceEnable()
decorator. The decorator adds a log entry of level Trace as soon as the decorated function is called. In
addition, a log message is added on function exit. This log message shows if the function exit occurred
as expected or with an exception.
See also
To create a trace log file, use the create_ trace_ log.py example, see Create Trace Log.
All previous examples enable and disable logging globally via the VmbSystem object. For more complex
applications, this may cause large log files. The ScopedLogEnable() decorator allows enabling and
disabling logging on function entry and exit. The following code snippet shows how to use
TraceEnable() and ScopedLogEnable().
from vmbpy import *
@TraceEnable()
def traced_function():
Log.get_instance(). info('Within Traced Function')
@ScopedLogEnable(LOG_CONFIG_TRACE_CONSOLE_ONLY)
def logged_function():
traced_function()
logged_function()