Troubleshooting¶
Error codes¶
Error Code |
Value |
Description |
|---|---|---|
VmbErrorSuccess |
0 |
No error |
VmbErrorInternalFault |
-1 |
Unexpected fault in Vmb or driver |
VmbErrorApiNotStarted |
-2 |
VmbStartup was not called before the current command |
VmbErrorNotFound |
-3 |
The designated instance (camera, feature, etc.) cannot be found |
VmbErrorBadHandle |
-4 |
The given handle is not valid |
VmbErrorDeviceNotOpen |
-5 |
Device was not opened for usage |
VmbErrorInvalidAccess |
-6 |
Operation is invalid with the current access mode |
VmbErrorBadParameter |
-7 |
One of the parameters is invalid (usually an illegal pointer) |
VmbErrorStructSize |
-8 |
The given struct size is not valid for this version of the API |
VmbErrorMoreData |
-9 |
More data available in a string/list than space is provided |
VmbErrorWrongType |
-10 |
Wrong feature type for this access function |
VmbErrorInvalidValue |
-11 |
The value is not valid; either out of bounds or not an |
VmbErrorTimeout |
-12 |
Timeout during wait |
VmbErrorOther |
-13 |
Other error |
VmbErrorResources |
-14 |
Resources not available (e.g., memory) |
VmbErrorInvalidCall |
-15 |
Call is invalid in the current context (e.g. callback) |
VmbErrorNoTL |
-16 |
No transport layers are found |
VmbErrorNotImplemented |
-17 |
API feature is not implemented |
VmbErrorNotSupported |
-18 |
API feature is not supported |
VmbErrorIncomplete |
-19 |
The current operation was not completed (e.g. a multiple |
VmbErrorIO |
-20 |
There was an error during read or write with devices |
General issues¶
Transport layer not found¶
Feature not usable¶
If a feature is not usable, use the latest camera firmware.
Issues by camera interface¶
GigE cameras¶
To use your GigE camera with best possible performance, follow the instructions in the User Guide of your camera.
5 GigE Vision cameras¶
To get your 5 GigE Vision camera up and running, see the user guide for your camera.
PacketSize¶
Make sure to set the PacketSize feature of GigE cameras to a value supported by your network card. If you use more than one camera on one interface, the available bandwidth has to be shared between the cameras.
GVSPAdjustPacketSizeconfigures GigE cameras to use the largest possible packets.DeviceThroughputLimitenables to configure the individual bandwidth if multiple cameras are used.The maximum packet size might not be available on all connected cameras. Try to reduce the packet size.
Other issues¶
Access Mode “Config” is not available in this SDK. Please use IP Config instead.
By default, the Allied Vision GigE TL is set to Broadcast (instead of Discovery Once), which constantly consumes bandwidth. For a higher bandwidth, use Discovery Once every time you connect a GigE camera.
USB cameras¶
Windows only: Make sure the correct driver is applied.
Camera Link cameras¶
Camera Link: Windows only.
The pixel format, all features affecting the image size, and
DeviceTapGeometrymust be identical for the SDK and the frame grabber software.Select an image size supported by the frame grabber.
The baud rate of the camera and the frame grabber must be identical.
CSI-2 cameras¶
Install the CSI-2 driver before installing the SDK.
See also
For compatible ARM boards, installation instructions, and additional information, see github.com/alliedvision.
Typical Linux issues¶
Transport layers not found¶
In most cases, Install.sh automatically registers the GENICAM_GENTL64_PATH environment variables in /etc/profile.d, so that every GenICam GenTL consumer can access the Vimba transport layers. If the transport layers are not found:
If multiple users work with the system, make sure all users can access /etc/profile.d.
If your display manager doesn’t support the install script (for example, lightdm and wdm): Please add the required environment variables to the /etc/environment file.
If login shell support is not supported, Install.sh in /etc/profile.d will not be loaded for X-Session. In this case, please copy the following line into the ~/.bashrc file and reboot.
export GENICAM_GENTL64_PATH=$GENICAM_GENTL64_PATH: "/PATH_TO_VIMBAFOLDER/VimbaGigETL/CTI/x86_64bit/"