Image Transform Manual¶
General aspects of the library¶
Usage with the C API or C++ API¶
The Image Transform library receives images from the C API or the C++ API. You can transform these images into several common image formats without knowing GenICam’s PFNC (Pixel Format Naming Convention) naming scheme.
Image transformation with the .NET or Python API¶
Frame.Fill() without accessing
the Image Transform library.Variants¶
The Image Transform Library is available in two variants:
The standard variant executes a function call in a single thread.
The OpenMP variant distributes the function calls over multiple processor cores (parallel computing).
The OpenMP variant is recommended for achieving a high performance with multi-core PCs: Although additional time is required to schedule the subtasks, its performance roughly scales by the number of free cores. Both library variants have the same interface and the same name, but are delivered in different directories in the SDK installation, allowing you to use the variant you want. The OpenMP variant is located in the subdirectory OpenMP of the single-threaded library variant.
Windows supports OpenMP V2.0, whereas Unix-based systems support OpenMP V4.0.
Optimizing OpenMP performance¶
The motivation behind OpenMP is to speed up computations by distributing them to the available computing cores (hyper-threading or real cores). To minimize the additional cost of thread management (starting or stopping threads), the OpenMP runtime environment tries to reuse threads as much as possible. Since the default values are not adjusted to your particular use case, we recommend optimizing them to achieve high performance with low CPU load.
Active waiting tasks and CPU load¶
Ideally, threads are created when OpenMP is first used in an application, and they are always reused without being interrupted by the system. In cases where the application has no work items ready when tasks finish, the waiting tasks consume CPU power for a certain time and then become passive. During active waiting, OpenMP uses high CPU load while no real work is done. This may lead to situations where OpenMP consumes too many resources although the use case isn’t demanding (low image resolution, slow frame rate).
Example
If frames arrive at 10 frames per second, there is one work item every 100 ms. Even if image transformation only takes 10 ms, the threads are active for about 100 ms. OpenMP is underutilized in this case because 90% of what it’s doing is waiting for new work. If frames arrive at 100 frames per second (frames arrive at 10 ms intervals), OpenMP is working to capacity, and all threads can take on new work directly after they have finished the previous one.
Tip
It is recommended to use the same OpenMP runtime environment that the Image Transform library uses (Windows: Visual Studio 10 or higher; Linux: gomp). In this case, Image Transform and the application share OpenMP threads, workload is optimally distributed between worker tasks, and waiting threads get new work fast.
Setting up environment variables¶
To optimize OpenMP, set up environment variables that determine the number of threads used and OpenMP’s waiting time behavior.
Linux and Windows:
OMP_NUM_THREADS=[number of threads for OpenMP usage] Limits the number of threads that are utilized by OpenMP. Lower this value to reduce the CPU load that OpenMP is taking away from other application threads.
OMP_WAIT_POLICY=[ACTIVE|PASSIVE] (for VS 2010) Changes the policy OpenMP uses when threads wait for new work to arrive. ACTIVE is the default setting. Under Windows, you can change it only after installing Microsoft KB2686593 Hotfix https://support.microsoft.com/de-de/topic/visual-studio-fix-high-cpu-usage-when-you-run-a-visual-c-2010-application-built-together-with-the-openmp-option-in-visual-studio-2010-05d60597-1496-c514-2470-0c1a9f8b5592. If a too long active waiting time causes high CPU load, change the environment variable to PASSIVE. Then threads don’t consume CPU power while waiting for new work.
Linux:
If OpenMP is set to OMP_WAIT_POLICY=ACTIVE, this variable determines how long a thread waits actively with consuming CPU power before waiting passively without consuming CPU power. If work items arrive at a high rate, it is best to let the thread’s spin wait actively for the next work load. If work items arrive sporadically, a high spin count leads to unnecessary high CPU load. Setting GOMP_SPINCOUNT to 0 is the same as setting OMP_WAIT_POLICY to PASSIVE.
Supported image data formats¶
Image file formats vs image data formats¶
In contrast to image file formats such as PNG, image data formats contain no embedded metadata, but only pure images as rectangular arrays of pixels. The pixels have characteristics such as:
Color
Bit depth
Endianness for a bit depth greater than eight
Order
The pixel format name describes these characteristics.
Vimba pixel formats and PFNC pixel formats¶
The Image Transform library uses:
Pixel formats from the GigE Vision and USB Vision interface specification
Pixel formats from GenICam’s Pixel Format Naming Convention (PFNC)
Common display formats on Windows and Linux platforms
Note
All implemented image transformations only accept multi-byte pixel formats in little-endian byte order.
The names of the pixel formats mainly match the list of values of the
PixelFormat feature in the SFNC (Standard Features Naming Convention) of GenICam,
but the actual name depends on the interface standard according to the following table:
Vimba Pixel format |
GigE Vision <2.0, |
PFNC (USB3 Vision, |
|
|---|---|---|---|
Mono8 |
Mono8 |
Mono8 |
|
Mono10 |
Mono10 |
Mono10 |
|
Mono10p |
Mono10p |
||
Mono12 |
Mono12 |
Mono12 |
|
Mono12p |
Mono12Packed |
Mono12p |
|
Mono12Packed |
Mono12Packed |
not available |
|
Mono14 |
Mono14 |
Mono14 |
|
Mono16 |
Mono16 |
Mono16 |
|
BayerXY*8 |
BayerXY*8 |
BayerXY*8 |
|
BayerXY*10 |
BayerXY*10 |
BayerXY*10 |
|
BayerXY*10p |
BayerXY*10p |
||
BayerXY*12 |
BayerXY*12 |
BayerXY*12 |
|
BayerXY*12p |
BayerXY*12p |
||
BayerXY*12Packed |
BayerXY*12Packed |
not available |
|
BayerXY*16 |
BayerXY*16 |
BayerXY*16 |
|
Rgb8 |
RGB8Packed |
RGB8 |
|
Bgr8 |
BGR8Packed |
BGR8 |
|
Rgba8 |
RGBa8Packed |
RGBa8 |
|
Bgra8 |
BGRa8Packed |
BGRa8 |
|
Rgb10 |
RGB10Packed |
RGB10 |
|
Bgr10 |
BGR10Packed |
BGR10 |
|
Rgba10 |
RGBa10 |
||
Bgra10 |
BGRa10 |
||
Rgb12 |
RGB12Packed |
RGB12 |
|
Bgr12 |
BGR12Packed |
BGR12 |
|
Rgba12 |
RGBa12 |
||
Bgra12 |
BGRa12 |
||
Rgb16 |
RGB16Packed |
RGB16 |
|
Bgr16 |
BGR16Packed |
BGR16 |
|
Rgba16 |
RGBa16 |
||
Bgra16 |
BGRa16 |
||
Yuv411 |
Yuv411Packed |
YUV411_8_UYYVYY |
|
Yuv422 |
Yuv422Packed |
YUV422_8_UYVY |
|
Yuv444 |
Yuv444Packed |
YUV8_UYV |
|
YCbCr411_8_CbYYCrYY |
YCbCr411_8_CbYYCrYY** |
||
YCbCr422_8_CbYCrY |
YCbCr422_8_CbYCrY** |
||
YCbCr422_8_YCbYCr |
YCbCr422_8_YCbYCr** |
||
YCbCr8_CbYCr |
YCbCr8_CbYCr (4:4:4) |
||
* BayerXY is any of BayerGR, BayerRG, BayerGB, or BayerBG |
|||
** Layout/values same as Yuv422 |
|||
Because the following pixel formats span a few bytes, or in some cases several lines, their width and height or size (in pixels) must be divisible by the following values:
Pixel format |
Width |
Height |
Size |
|---|---|---|---|
Mono12Packed,Mono12p |
1 |
1 |
2 |
BayerXY… |
2 |
2 |
1 |
Yuv411 |
4 |
1 |
1 |
Yuv422 |
2 |
1 |
1 |
Supported transformations¶
Tip
For applying transformations, see the section Transformation examples in this manual and the AsynchrounousGrab example.
Note
Converting an image from a lower to a higher bit depth aligns the image data to the least significant bit. The remaining bits are set to zero.
All pixel formats can be transformed into:
Mono8, Rgb/Bgr8
Rgba/Bgra8
Note
Transformations from higher into lower bit depths or from color into mono are lossy.
Note
Transforming a pixel format into itself (for troublechecking purposes) is not always supported, but you can always apply the transformations listed above.
Additionally, the following transformations are supported:
All 10-bit pixel formats including “p” and “Packed” can be transformed into:
Mono10
Rgb/Bgr10, Rgba/Bgra10
All 12-bit pixel formats including “p” and “Packed” can be transformed into:
Mono12
Rgb/Bgr12, Rgba/Bgra12
Mono14 can be transformed into Rgb/Bgr14, Rgba/Bgra14.
All 16-bit pixel formats including “p” and “Packed” can be transformed into:
Mono16
Rgb/Bgr16, Rgba/Bgra16
The following pixel formats can be transfomed into Yuv422:
Mono8
BayerXY8
Additionally to the lossless transformations described above, lossy transformations are supported: Mono10p, Mono12p, and Mono12Packed have a lossy conversion to 8-bit formats and a lossless conversion to Mono10 and Mono12 (both LSB and Little Endian). The same is true for Bayer and RGB formats. Additionally, they have a lossy conversion to Mono formats.
The following sections of this document describe how to apply a transformation.
API usage¶
General aspects¶
Every concrete image transformation must specify its three parameters:
The fully-qualified input image (including complete format specification)
The complete output format (plus a pointer to enough memory to hold the transformed image)
The transformation itself (including transformation options if there is more than one possible way from the input format to the output format)
The main function VmbImageTransform() covers all required transformation parameters.
The function uses two pointers of the VmbImage struct to specify the source and
destination image and a list of VmbTransformInfo structs to specify the
transformation.
VmbImageTransform ( &sourceImage , &destinationImage , &info , 1 );
To ease filling the structs that are needed for a successful call of
VmbImageTransform(), several helper functions for initializing them are available:
Methods for filling the necessary format information of either the input or the output image (described below in chapter Filling Image Information).
Methods for filling optional transformation parameters to invoke special and additional functionality.
Filling Image Information¶
The Image Transform library offers several methods to find an set a compatible destination format.
To easily set a compatible destination image format, you can initialize the VmbImage struct with:
VmbSetImageInfoFromInputImage()by providing an input image from the C or C++ API, the output layout, and bit depthVmbSetImageInfoFromInputParameters()by providing the input format, the input image size, the output layout, and bit depthVmbSetImageInfoFromPixelFormat()by providing a VmbPixelFormat_t value and the size
Experts can use VmbSetImageInfoFromString() by providing a string
that describes the pixel format and the size.
Not recommended: Although it is not recommended, it is possible to fill the fields explicitly one by one.
Specifying transformation options¶
Depending on your application and the desired image characteristics, you can choose between several transformation options.
Adding color transformations¶
A common way to transform color images is using a 3x3 matrix with method
VmbSetColorCorrectionMatrix3x3(). The matrix you have to specify is a
3x3 row order float matrix.
Changing the debayering algorithm¶
Every transformation of a Bayer image requires defining how to interpolate
or combine the color pixels. For best system performance,
a simple 2x2 demosaicing algorithm is the default. You can change this algorithm
with an additional transformation parameter to
VmbImageTransform(), which can be filled with function
VmbSetDebayerMode(), using a VmbDebayerMode() as input.
Possible values of VmbDebayerMode() are listed in the following table:
Value |
Description |
|---|---|
VmbDebayerMode2x2 |
2x2 with green averaging (default, OpenMP only) |
VmbDebayerMode3x3 |
3x3 with equal green weighting per line |
VmbDebayerModeLCAA* |
Debayering with horizontal local color anti-aliasing |
VmbDebayerModeLCAAV* |
Debayering with horizontal and vertical local color anti-aliasing |
VmbDebayerModeYUV422* |
Debayering with YUV422-alike sub-sampling |
* For 8-bit images only |
|
Note
If VmbDebayerModeLCAA, VmbDebayerModeLCAAV, or
VmbDebayerModeYUV422 is used, the input buffers serve as intermediate
buffers for the transformation for performance reasons. To use the
input buffer for another purpose, debayer afterwards or copy the input buffer
beforehand.
Transforming images¶
When all the parameters of a transformation are prepared, use the pre-filled structs and call
VmbImageTransform().
Note
Inapplicable transformation options are ignored (for example, debayering options to a monochrome input image).
Transformation examples¶
Debayering into an Rgb8 image¶
Transformation of a BayerGR8 image with 640x480 pixels into an Rgb8 image of the same size:
VmbImage sourceImage;
VmbImage destinationImage;
VmbTransformInfo info;
// Set size member for verification inside API
sourceImage.Size = sizeof ( sourceImage );
destinationImage.Size = sizeof ( destinationImage );
// Attach the data buffers
sourceImage.Data = pInBuffer;
destinationImage.Data = pOutBuffer;
// Fill image info from pixel format
VmbSetImageInfoFromPixelFormat ( VmbPixelFormatBayerGR8 ,
640,
480,
&sourceImage );
// Fill destination image info from input image
VmbSetImageInfoFromInputImage ( &sourceImage ,
VmbPixelLayoutRGB ,
8,
&destinationImage );
// Set the debayering algorithm to 2x2
VmbSetDebayerMode ( VmbDebayerMode2x2 , &info );
// Perform the transformation
VmbImageTransform ( &sourceImage , &destinationImage , &info , 1 );
Debayering into a Mono8 image¶
Preparing a transformation of a BayerRG8 image with 640x480 pixels into a Mono8 image of the same size:
VmbImage sourceImage;
VmbImage destinationImage;
VmbTransformInfo info;
// Set size member for verification inside API
sourceImage.Size = sizeof ( sourceImage );
destinationImage.Size = sizeof ( destinationImage );
// Attach the data buffers
sourceImage.Data = pInBuffer;
destinationImage.Data = pOutBuffer;
// Fill image info from pixel format string
std:: string name ( "PixelFormatBayerRG8" );
VmbSetImageInfoFromString ( name.c_str(),
static_cast <VmbUint32_t >( name.size() ),
640,
480,
&sourceImage );
// Fill image info from pixel known input parameters
VmbSetImageInfoFromInputParameters ( VmbPixelFormatBayerRG8 ,
640,
480,
VmbPixelLayoutMono ,
8
&destinationImage );
// Set the debayering algorithm to 3x3
VmbSetDebayerMode ( VmbDebayerMode3x3 , &info );
// Perform the transformation
VmbImageTransform ( &sourceImage , &destinationImage , &info , 1 );
Color correction of an Rgb8 image¶
Applying a color correction to an Rgb8 image with 640x480 pixels:
VmbImage sourceImage;
VmbImage destinationImage;
VmbTransformInfo info;
const VmbFloat_t mat[] = { 1.0f, 0.0f, 0.0f,
0.0f, 1.0f, 0.0f,
0.0f, 0.0f, 1.0f };
// Set size member for verification inside API
sourceImage.Size = sizeof ( sourceImage );
destinationImage.Size = sizeof ( destinationImage );
// Attach the data buffers
sourceImage.Data = pInBuffer;
destinationImage.Data = pOutBuffer;
// Fill image info from pixel format
VmbSetImageInfoFromPixelFormat ( VmbPixelFormatRgb8 ,
640,
480,
&sourceImage );
// Fill destination image info from input image
VmbSetImageInfoFromInputImage ( &sourceImage ,
VmbPixelLayoutRGB ,
8,
&destinationImage );
// Set the transformation matrix
VmbSetColorCorrectionMatrix3x3 ( mat , &info );
// Perform the transformation
VmbImageTransform ( &sourceImage , &destinationImage , &info , 1 );
Advanced transformation with debayering¶
Transformation of a BayerGR12 image with 640x480 pixels into a Mono16 image of the same size:
VmbImage sourceImage;
VmbImage destinationImage;
VmbTransformInfo info [2];
const VmbFloat_t mat[] = { 1.0f, 0.0f, 0.0f,
0.0f, 1.0f, 0.0f,
0.0f, 0.0f, 1.0f };
// Set size member for verification inside API
sourceImage.Size = sizeof ( sourceImage );
destinationImage.Size = sizeof ( destinationImage );
// Attach the data buffers
sourceImage.Data = pInBuffer;
destinationImage.Data = pOutBuffer;
// Fill image info from pixel format
VmbSetImageInfoFromPixelFormat ( VmbPixelFormatRgb8 ,
640,
480,
&sourceImage );
// Fill destination image info from input image
VmbSetImageInfoFromInputImage ( &sourceImage ,
VmbPixelLayoutMono ,
16,
&destinationImage );
// Set the debayering algorithm to 2x2
VmbSetDebayerMode ( VmbDebayerMode2x2 , &info [0] );
// Set the transformation matrix
VmbSetColorCorrectionMatrix3x3 ( mat , &info [1] );
// Perform the transformation
VmbImageTransform ( &sourceImage , &destinationImage , &info , 2 );
Function reference¶
Information¶
VmbGetVersion()¶
This function inquires the library version. It can be called at anytime, even before the library is initialized.
Type |
Name |
Description |
|
|---|---|---|---|
out |
VmbUint32_t* |
pValue |
Contains the library version |
VmbErrorBadParameter: If the given pointer is NULL
VmbGetErrorInfo()¶
Type |
Name |
Description |
|
|---|---|---|---|
in |
VmbError_t |
errorCode |
The error code to get a readable string for |
out |
VmbANSIChar_t* |
pInfo |
Pointer to a zero terminated string that |
in |
VmbUint32_t |
maxInfoLength |
The length of the pInfo buffer |
VmbGetApiInfoString()¶
Type |
Name |
Description |
|
|---|---|---|---|
in |
VmbAPIInfo_t |
infoType |
Type of information to return |
out |
VmbANSIChar_t* |
pInfo |
Pointer to a zero terminated string that |
contains error information on return |
|||
in |
VmbUint32_t |
maxInfoLength |
The length of the pInfo buffer |
The parameter infoType may have one of the following values:
Value |
Description |
|---|---|
VmbAPIInfoAll |
Return all information about the API |
VmbAPIInfoPlatform |
Return information about the platform (x86 or x64) |
VmbAPIInfoBuild |
Return info about the API build (debug or release) |
VmbApiInfoTechnology |
Return info about supported technologies, like OpenMP |
Transformation¶
VmbImageTransform()¶
This function transforms images from one pixel format to another with possible transformation options. The transformation is defined by the provided images and the desired transformation.
Type |
Name |
Description |
|
|---|---|---|---|
in |
const VmbImage* |
pSource |
Image to transform |
in/out |
VmbImage* |
pDestination |
Destination image |
in |
const VmbTransformInfo* |
pParameter |
Optional transform parameters |
in |
VmbUint32_t |
parameterCount |
Number of transform parameters |
VmbErrorBadParameter:
If any image pointer or their “Data” members is NULL
If Width or Height doesn’t match between source and destination
If one of the parameters for the conversion does not fit
Tip
Fill the source and destination image info struct with
VmbSetImageInfoFromPixelFormat() or
VmbSetImageInfoFromString() and keep those structs as template. For
calls to transform, attach the image to the “Data” member. When set, the
optional parameters are constraints on the transform.
Helper functions¶
VmbSetImageInfoFromInputImage()¶
This function sets image info member values in VmbImage from input VmbImage. Use simple target layout and bit per pixel values to set the desired target format.
Type |
Name |
Description |
|
|---|---|---|---|
in |
const VmbImage* |
pInputmage |
Image source to transform |
in |
VmbPixelLayout_t |
OutputPixelLayout |
Pixel layout of the target image |
in |
VmbUint32_t |
BitPerPixel |
Bits per pixel of the target image |
in/out |
VmbImage* |
pOutputImage |
Pointer to Vmb image to set the info to |
VmbErrorBadParameter:
If the given pointer is NULL
If one of the parameters for the conversion does not fit
VmbErrorNotImplemented: Transformation is not supported
VmbSetImageInfoFromInputParameters()¶
Set image info member values in VmbImage from pixel format. Use simple target layout and bit per pixel values to set the desired target format.
Type |
Name |
Description |
|
|---|---|---|---|
in |
VmbPixelFormat_t |
pInputmage |
Image source to transform |
in |
VmbUint32_t |
Width |
Image width in pixels |
in |
VmbUint32_t |
Height |
Image height in pixels |
in |
VmbPixelLayout_t |
OutputPixelLayout |
Pixel layout of the target image |
in |
VmbUint32_t |
BitPerPixel |
Bits per pixel of the target image |
in/out |
VmbImage* |
pOutputImage |
Pointer to Vimba image to set the info to |
VmbSetImageInfoFromPixelFormat()¶
This is an expert function. Set image info member values in VmbImage from pixel format. As a reference, refer to section Supported transformations.
Type |
Name |
Description |
|
|---|---|---|---|
in |
const VmbANSIChar_t* |
imageFormat |
Image format as a (const) case insensitive |
in |
VmbUint32_t |
StringLength |
The length of the pixel format string |
in |
VmbUint32_t |
Width |
Image width in pixels |
in |
VmbUint32_t |
Height |
Image height in pixels |
in/out |
VmbImage* |
pImage |
Pointer to Vimba image to set the info to |
Tip
VmbPixelFormat_t can be obtained from the C/C++ API’s frame or from the
PixelFormat feature. For displaying images, you can use
VmbSetImageInfoFromString() or to look up a matching VmbPixelFormat.
VmbSetImageInfoFromString()¶
This is an expert function. Set image info member values in VmbImage from string.
Type |
Name |
Description |
|
|---|---|---|---|
in |
const VmbANSIChar_t* |
imageFormat |
Image format as a (const) case insensitive |
in |
VmbUint32_t |
StringLength |
The length of the pixel format string |
in |
VmbUint32_t |
Width |
Image width in pixels |
in |
VmbUint32_t |
Height |
Image height in pixels |
in/out |
VmbImage* |
pImage |
Pointer to Vimba image to set the info to |
VmbErrorBadParameter:
If one of the given pointers or the “Data” member in the image is NULL
If Width or Height don’t match between source and destination
If one of the parameters for the conversion does not fit
VmbSetDebayerMode()¶
Set transformation options to a predefined debayering mode.
Note
Debayering is only applicable to image formats with both an even width and an even height.
Type |
Name |
Description |
|
|---|---|---|---|
in |
VmbDebayerMode_t |
DebayerMode |
Used for debayering the source raw |
in/out |
VmbTransformInfo_t* |
pTransformInfo |
Parameter that contains information about |
VmbErrorBadParameter: If the given pointer is NULL
VmbSetColorCorrectionMatrix3x3()¶
Set transformation options to a 3x3 color matrix transformation.
Type |
Name |
Description |
|
|---|---|---|---|
in |
const VmbFloat_t* |
DebayerMode |
Color correction matrix |
in/out |
VmbTransformInfo_t* |
pTransformInfo |
Parameter that contains information about |
VmbErrorBadParameter: If one of the given pointers is NULL
Structs¶
VmbImage¶
VmbImage encapsulates image data for the transformation function.
Struct entry |
Purpose |
|
|---|---|---|
VmbUint32_t |
Size |
Size of the structure |
void* |
Data |
Pointer to the payload received from the C/C++ API |
VmbImageInfo |
ImageInfo |
Internal information data for mapping the images |
VmbImageInfo¶
VmbImageInfo contains image information needed for the transformation function.
Struct entry |
Purpose |
|
|---|---|---|
VmbUint32_t |
Width |
Image width in pixels or sub-pixels for macro pixel |
VmbUint32_t |
Height |
The height of the image in pixels |
VmbInt32_t |
Stride |
The offset from the current line to the next line, |
VmbPixelInfo |
PixelInfo |
Information about the pixel format |
VmbPixelInfo¶
The pixel format of an image is described within VmbPixelInfo.
Struct entry |
Purpose |
|
|---|---|---|
VmbUint32_t |
VmbUint32_t |
Number of bits for one image pixel or sub-pixel in macro pixel formats |
VmbUint32_t |
BitsUsed |
Number of bits used per pixel, e.g. RGB12 has 48 bits per pixel and 36 bits used |
VmbAlignment_t |
Alignment |
For image formats where BitsPerPixel is not equal to bitsUsed, the alignment specifies the bit layout of the pixel |
VmbEndianness_t |
Endianness |
Specifies the endianness of pixels that are larger than one byte |
VmbPixelLayout_t |
PixelLayout |
Describes the layout of the pixel component, e.g., RGB or BGR layout |
VmbBayerPattern_t |
BayerPattern |
For raw image data, this field specifies the color filter |
VmbTransformInfo¶
Transformation parameters given as a pointer to a VmbTransformInfo struct are
used to invoke special and additional functionality, which is applied while
interpreting the source image (debayering) or transforming the images (color correction).
Struct entry |
Purpose |
|
|---|---|---|
VmbTransformType_t |
TransformType |
Transform info type, may be |
VmbTransformParameter |
Parameter |
Transform info variant, may be |