About Vimba 6.1¶
Introduction¶
Vimba is Allied Vision’s established SDK. Since Vimba is based on GenICam, common third-party software solutions can easily be used with Vimba’s transport layers (TLs).
Compatibility¶
Vimba for Linux and Linux ARM64 supports Allied Vision GigE and USB cameras. Vimba for ARM64 additionally supports Alvium MIPI cameras.
See also
See the Release Notes for details about supported OS, ARM boards, and camera models.
Note
Alvium MIPI camera users: The camera driver must be installed before using Vimba. It is available at:
Third-party software¶
Vimba’s transport layers (GenTL producers) are based on GenICam and therefore can be used with any third-party software that includes a GenTL consumer.
To use Vimba with GenICam-compliant third-party software:
Install at least Vimba’s transport layers. We recommend you to install Vimba Viewer additionally.
Follow the instructions of the third-party software on how to use cameras via the camera vendor’s transport layer.
Tip
Before starting the third-party software, make sure no other application uses the camera.
Before first use, follow the instructions of the camera user guide or technical manual.
Camera recognition may take a while, especially with GigE cameras.
If your camera does not reach the maximum frame rate, check if the exposure time is short enough. Example: If the exposure time is 100 ms, the camera cannot acquire more than approximately 10 fps.
If you have issues with the third-party software, check the camera functionality with Vimba Viewer.