C API Manual¶
Introduction to the API¶
The C API is Vimba’s underlying API. It can also be used as API for C++ applications, especially if you prefer an API with less design patterns than the C++ API.
For accessing functionality of either Vimba or the connected cameras, you have two ways of control: You can use the fixed set of API functions and you can use GenICam Features by calling functions such as VmbFeatureXXXSet or VmbFeatureXXXGet on entities like Vimba or the cameras. This manual mainly deals with the API functions.
See also
To understand the API, read the SDK Manual first: It contains essential information. For a quick start, use the examples.
API usage¶
API version¶
Even if new features are introduced to the C API, your software
remains backward compatible. Use VmbVersionQuery() to check
the version number of the C API. You can run this function without
initializing the API.
API startup and shutdown¶
To start and shut down the API, use these paired functions:
The function
VmbStartup()initializes the API.The function
VmbShutdown()shuts down the API as soon as all callbacks are finished.
The functions VmbStartup() and VmbShutdown() must always be paired.
Calling the pair several times within the same program is possible,
but not recommended.
To free resources, shut down the API when you don’t use it. Shutting down
the API closes all opened cameras.
Listing cameras¶
See also
For a quick start, see the ListCameras example of the Vimba SDK.
The function VmbCamerasList() enumerates all cameras recognized by
the underlying transport layers. With this command, you can
fetch all static details of a camera such as:
Camera ID
Camera model
Name or ID of the connected interface (for example, the NIC)
The order in which the detected cameras are listed is determined by the order of camera discovery and therefore not deterministic. Moreover, the order may change depending on your system configuration and the accessories (for example, hubs or long cables).
GigE cameras¶
Listing cameras over the network is a two-step process:
To enable camera discovery events, run one of the following commands: GeVDiscoveryAllOnce discovers all connected cameras once. GeVDiscoveryAllAuto continually emits discovery packets and thus constantly consumes bandwidth. Use it only if you need to stay aware of changes to your network structure and new cameras.
Both commands require a certain amount of time (GeVDiscoveryAllDuration) before returning.
To stop the camera discovery, run command GeVDiscoveryAllOff.
USB and 1394 cameras:¶
Changes to the plugged cameras are detected automatically. Therefore, all changes to the camera list are announced via discovery event. All listed commands are applied to all network interfaces, see the code snippet below.
Camera Link cameras:¶
The specifications of Camera Link and GenCP do not support plug & play or discovery events. To detect changes to the camera list, shutdown and startup the API by calling VmbShutdown and VmbStartup consecutively.
bool bGigE;
VmbUint32_t nCount;
VmbCameraInfo_t* pCameras;
// We ask Vimba for the presence of a GigE transport layer
VmbError_t err = VmbFeatureBoolGet( gVimbaHandle , "GeVTLIsPresent", &bGigE );
if ( VmbErrorSuccess == err )
{
if ( true == bGigE )
{
// We use all network interfaces using the global Vimba handle
err = VmbFeatureCommandRun( gVimbaHandle , "GeVDiscoveryAllOnce" );
}
}
if ( VmbErrorSuccess == err )
{ // Get the number of connected cameras
err = VmbCamerasList( NULL , 0, &nCount , sizeof *pCameras );
if ( VmbErrorSuccess == err )
{
// Allocate accordingly
pCameras = (VmbCameraInfo_t *) malloc( nCount * sizeof *pCameras );
// Get the cameras
err = VmbCamerasList( pCameras , nCount , &nCount , sizeof *pCameras );
// Print out each camera 's name
for ( VmbUint32_t i=0; i<nCount; ++i )
{
printf( " %s\n", pCameras[i]. cameraName );
}
}
}
Struct VmbCameraInfo_t¶
Struct VmbCameraInfo_t provides the entries listed in the table below for obtaining information about a camera.
Type |
Field |
Purpose |
|---|---|---|
const char* |
cameraIdString |
Unique identifier for each camera |
const char* |
cameraName |
Name of the camera |
const char* |
modelName |
The model name |
const char* |
serialString |
The serial number |
VmbAccessMode_t |
permittedAccess |
See VmbAccessModeType |
const char* |
interfaceIdString |
Unique value for each interface or bus |
Similiar to listing available cameras, VmbInterfacesList() can be used to list available
interfaces, see Listing interfaces.
Enabling notifications of changed camera states¶
To get notified whenever a camera is detected, disconnected, or changes its open state:
Run command feature GeVDiscoveryAllAuto on the System entity (GigE cameras only).
Use
VmbFeatureInvalidationRegister()to register a callback with the Vimba System that gets executed on the according event. The function pointer to the callback function has to be of typeVmbInvalidationCallback*.
Note
VmbShutdown() blocks until all callbacks have finished execution.
Note
Functions that must not be called within the camera notification callback:
VmbStartup
VmbShutdown
VmbCameraOpen
VmbCameraClose
VmbFeatureIntSet (and any other VmbFeature*Set function)
VmbFeatureCommandRun
Opening and closing a camera¶
A camera must be opened to control it and to capture images.
Call VmbCameraOpen() and provide the ID of the camera and the desired access mode.
The API provides several access modes:
VmbAccessModeFull: read and write access. Use this mode to configure the camera features and to acquire images (Goldeye CL cameras: configuration only).
VmbAccessModeConfig: enables configuring the IP address of your GigE camera.
VmbAccessModeRead: read-only access. Setting features is not possible. However, for GigE cameras that are already in use by another application, the acquired images can be transferred to the API (Multicast).
The enumerations are defined in VmbAccessModeType (or its VmbUint32_t representation VmbAccessMode_t).
Enumeration Integer Value |
Integer Value |
Purpose |
|---|---|---|
VmbAccessModeNone |
0 |
No access |
VmbAccessModeFull |
1 |
Read and write access |
VmbAccessModeRead |
2 |
Read-only access |
VmbAccessModeConfig |
4 |
Configuration access (GigE) |
When a camera has been opened successfully, a handle for further access is returned.
An example for opening a camera retrieved from the camera list is shown in the code snippet below.
VmbCameraInfo_t *pCameras;
VmbHandle_t hCamera;
// Get all known cameras as described in chapter "Listing available cameras"
// Open the first camera
if ( VmbErrorSuccess == VmbCameraOpen( pCameras [0]. cameraIdString ,
VmbAccessModeFull , hCamera ) )
{
printf( "Camera opened , handle [0x%p] retrieved .\n", hCamera );
}
The code snippet below shows how to close a camera using VmbCameraClose and the previously retrieved handle.
if ( VmbErrorSuccess == VmbCameraClose( hCamera ) )
{
printf( "Camera closed .\n" );
}
Accessing features¶
See also
For a quick start, see the ListFeatures example of the Vimba SDK.
Feature types¶
The Vimba C API provides several feature types, which all have their specific properties and functionalities. The API provides its own set of access functions for every feature data type.
Feature Type |
Operation |
Function |
|---|---|---|
Enumeration |
Set |
VmbFeatureEnumSet |
Get |
Get VmbFeatureEnumGet |
|
Range |
Range |
VmbFeatureEnumRangeQuery |
Other |
VmbFeatureEnumIsAvailable |
|
VmbFeatureEnumAsInt |
||
VmbFeatureEnumAsString |
||
VmbFeatureEnumEntryGet |
||
Integer |
Set |
VmbFeatureIntSet |
Get |
VmbFeatureIntGet |
|
Range |
VmbFeatureIntRangeQuery |
|
Other |
VmbFeatureIntIncrementQuery |
|
Float |
Set |
VmbFeatureFloatSet |
Get |
VmbFeatureFloatGet |
|
String |
Set |
VmbFeatureStringSet |
Get |
VmbFeatureStringGet |
|
Range |
VmbFeatureStringMaxlengthQuery |
|
Boolean |
Set |
VmbFeatureBoolSet |
Get |
VmbFeatureBoolGet |
|
Command |
Set |
VmbFeatureCommandRun |
Get |
VmbFeatureCommandIsDone |
|
Raw data |
Set |
VmbFeatureRawSet |
Get |
VmbFeatureRawGet |
|
Range |
VmbFeatureRawLengthQuery |
|
Struct VmbFeatureInfo_t¶
The static properties of a feature are held in struct VmbFeatureInfo_t.
Struct Entry |
Purpose |
|---|---|
const char* name |
Name used in the API |
VmbFeatureData_t featureDataType |
Data type of this feature |
VmbFeatureFlags_t featureFlags |
Access flags for this feature |
const char* category |
Category this feature can be found in |
const char* displayName |
Feature name to be used in GUIs |
VmbUint32_t pollingTime |
Predefined polling time for volatile features |
const char* unit |
Measuring unit as given in the XML file |
const char* representation |
const char* representation |
VmbFeatureVisibility_t visibility |
GUI visibility |
const char* tooltip |
Short description, e.g. for a tooltip |
const char* description |
Longer description |
const char* sfncNamespace |
Namespace this feature resides in |
VmbBool_t isStreamable |
Indicates if a feature can be stored to or loaded from a file |
VmbBool_t hasAffectedFeatures |
Indicates if the feature potentially affects other features |
VmbBool_t hasSelectedFeatures |
Indicates if the feature selects other features |
Enumeration |
Integer Value |
Purpose |
VmbFeatureDataInt |
1 |
64-bit integer feature |
VmbFeatureDataFloat |
2 |
64-bit floating point feature |
VmbFeatureDataEnum |
3 |
Enumeration feature |
VmbFeatureDataString |
4 |
String feature |
VmbFeatureDataBool |
5 |
Boolean feature |
VmbFeatureDataCommand |
6 |
Command feature |
VmbFeatureDataRaw |
7 |
Raw (direct register access) feature |
VmbFeatureDataNone |
8 |
Feature with no data |
Enumeration |
Integer Value |
Purpose |
|---|---|---|
VmbFeatureFlagsNone |
0 |
No additional information is provided |
VmbFeatureFlagsRead |
1 |
Static info about read access. Current status depends |
VmbFeatureFlagsWrite |
2 |
Static info about write access. Current status depends |
VmbFeatureFlagsVolatile |
8 |
Value may change at any time |
VmbFeatureFlagsModifyWrite |
16 |
Value may change after a write |
Enumeration |
Integer value |
Purpose |
|---|---|---|
VmbFeatureVisibilityUnknown |
0 |
Feature visibility is not known |
VmbFeatureVisibilityBeginner |
1 |
Feature is visible in feature list (beginner) |
VmbFeatureVisibilityExpert |
2 |
Feature is visible in feature list (expert level) |
VmbFeatureVisibilityGuru |
3 |
Feature is visible in feature list (guru level) |
VmbFeatureVisibilityInvisible |
4 |
Feature is not visible in feature list |
VmbFeatureInfo_t *pFeatures;
VmbUint32_t nCount = 0;
VmbHandle_t hCamera;
// Open the camera as shown in chapter "Opening and closing a camera"
// Get the number of features
VmbError_t err = VmbFeaturesList( hCamera , NULL , 0, &nCount , sizeof *pFeatures );
if ( VmbErrorSuccess == err && 0 < nCount )
{
// Allocate accordingly
pFeatures = (VmbFeatureInfo_t *) malloc( nCount * sizeof *pFeatures );
// Get the features
err = VmbFeaturesList( hCamera , pFeatures , nCount , &nCount ,
sizeof *pFeatures );
// Print out their name and data type
for ( int i=0; i<nCount; ++i )
{
printf( "Feature '%s' of type: %d\n", pFeatures[i].name ,
pFeatures[i]. featureDataType );
}
}
VmbHandle_t hCamera;
// Open the camera as shown in chapter "Opening a camera"
VmbInt64_t nWidth;
if ( VmbErrorSuccess == VmbFeatureIntGet( hCamera , "Width", &nWidth ))
{
printf("Width: %ld\n", nWidth );
}
VmbHandle_t hCamera;
// Open the camera as shown in chapter "Opening a camera"
if ( VmbErrorSuccess == VmbFeatureEnumSet( hCamera , "AcquisitionMode",
"Continuous" ))
{
if ( VmbErrorSuccess = VmbFeatureCommandRun( hCamera , "AcquisitionStart" ))
{
printf( "Acquisition successfully started\n" );
}
}
Camera features¶
To query all available features of a camera, use VmbFeaturesList().
This list does not change while the camera is opened.
Information about enumeration features, such as string and integer representation,
is held in struct VmbFeatureEnumEntry_t.
Struct VmbFeatureEnumEntry_t¶
Struct entry |
Purpose |
const char* name |
Name used in the API |
const char* displayName |
Enumeration entry name to be used in GUIs |
VmbFeatureVisibility_t visibility |
GUI visibility |
const char* tooltip |
Short description, e.g. for a tooltip |
const char* description |
Longer description |
const char* sfncNamespace |
Namespace this feature resides in |
VmbInt64_t intValue |
Integer value of this enumeration entry |
Note
Some features aren’t always available. For example, some features
cannot be accessed while the camera is acquiring images. To query the
current accessibility of a feature, call VmbFeatureAccessQuery().
The following table shows basic features of all cameras. A feature has a name, a type, and access flags such as read-permitted and write-permitted.
Feature Type |
Type |
Access flags |
Description |
|---|---|---|---|
AcquisitionMode |
Enumeration |
R/W |
Acquisition mode of the camera. Value |
AcquisitionStart |
Command |
Start acquiring images. |
|
AcquisitionStop |
Command |
Stop acquiring images. |
|
PixelFormat |
Enumeration |
R/W |
The image format (Mono8 etc.) |
Width |
Uint32 |
Image width, in pixels. |
|
Height |
Uint32 |
Image height, in pixels. |
|
PayloadSize |
Uint32 |
Recommendation: Use VmbPayloadSizeGet() |
To get notified whenever a feature value changes, use VmbFeatureInvalidationRegister() to
register a callback that gets executed on the according event. For camera features, use the camera
handle for registration. The function pointer to the callback function has to be of type
VmbInvalidationCallback*().
Acquiring images¶
See also
The SDK Manual describes synchronous and asynchronous image acquisition.
See also
For a quick start, see the SynchronousGrab example.
Image Capture vs. Image Acquisition¶
Image capture and image acquisition are two independent operations: The API captures images, the camera acquires images. To obtain an image from your camera, setup the API to capture images before starting the acquisition on the camera:
Typical asynchronous application with the C API¶
Image Capture¶
To enable image capture, frame buffers must be allocated and the API must be prepared for incoming frames.
To capture images sent by the camera, follow these steps:
Open the camera as described in chapter Opening and closing a camera.
Query the necessary buffer size through the
PayloadSize()function.Announce the frame buffers. If you announce NULL buffers, the TL announces buffers with a suitable value.
Start the capture engine.
Queue the frame you have just created with
VmbCaptureFrameQueue(), so that the buffer can be filled when the acquisition has started.
The API is now ready. Start and stop image acquisition on the camera as described in chapter Image Acquisition. How you proceed depends on the acquisition model you need:
Synchronous: Use VmbCaptureFrameWait to receive an image frame while blocking your execution thread.
Asynchronous: Register a callback that gets executed when capturing is complete. Use the camera handle for registration. The function pointer to the callback function has to be of type
VmbFrameCallback*`(). Within the callback routine, queue the frame again after you have processed it.
Stop the capture engine with
VmbCaptureEnd().Call
VmbCaptureQueueFlush()to cancel all frames on the queue.Revoke the frames with
VmbFrameRevokeAll()to clear the buffers.
To assure correct continuous image capture, queue at least two or three frames. The appropriate number of frames to be queued in your application depends on the frames per second the camera delivers and on the speed with which you are able to re-queue frames (also depending on the load of your operating system). The image frames are filled in the same order in which they were queued.
Note
Always check that VmbFrame_t.receiveStatus equals VmbFrameStatusComplete when a frame is returned to ensure the data is valid.
Note
Functions that must not be called within the Frame callback routine:
VmbStartup
VmbShutdown
VmbCameraOpen
VmbCameraClose
VmbFrameAnnounce
VmbFrameRevoke
VmbFrameRevokeAll
VmbCaptureStart
VmbCaptureStop
Image Acquisition¶
As soon as the API is prepared (see Image Capture, you can start image acquisition on your camera:
Set the feature AcquisitionMode (for example, Continuous).
Run the command AcquisitionStart.
To stop image acquisition, run command AcquisitionStop.
#define FRAME_COUNT 3 // We choose to use 3 frames
VmbError_t err; // Functions return an error code to
// check for VmbErrorSuccess
VmbHandle_t hCamera // A handle to our opened camera
VmbFrame_t frames[FRAME_COUNT]; // A list of frames for streaming
VmbUInt64_t nPLS; // The payload size of one frame
// The callback that gets executed on every filled frame
void VMB_CALL FrameDoneCallback( const VmbHandle_t hCamera, VmbFrame_t *pFrame )
{
if ( VmbFrameStatusComplete == pFrame ->receiveStatus )
{
printf( "Frame successfully received\n" );
}
else
{
printf( "Error receiving frame\n" );
}
VmbCaptureFrameQueue( hCamera , pFrame , FrameDoneCallback );
}
// Get all known cameras, see chapter "List available cameras"
// and open the camera as shown in chapter "Opening a camera"
// Get the required size for one image
err = VmbFeatureIntGet( hCamera , "PayloadSize", &nPLS );
for ( int i=0; i<FRAME_COUNT; ++i )
{
// Allocate accordingly
frames[i]. buffer = malloc( nPLS );
frames[i]. bufferSize = nPLS;
// Anounce the frame
VmbFrameAnnounce( hCamera , frames[i], sizeof(VmbFrame_t) );
}
// Start capture engine on the host
err = VmbCaptureStart( hCamera );
// Queue frames and register callback
for ( int i=0; i<FRAME_COUNT; ++i )
{
VmbCaptureFrameQueue( hCamera , frames[i],
FrameDoneCallback );
}
// Start acquisition on the camera
err = VmbFeatureCommandRun( hCamera , "AcquisitionStart" );
// Program runtime ...
// When finished , tear down the acquisition chain , close the camera and Vimba.
err = VmbFeatureCommandRun( hCamera , "AcquisitionStop" );
err = VmbCaptureEnd( hCamera );
err = VmbCaptureQueueFlush( hCamera );
err = VmbFrameRevokeAll( hCamera );
err = VmbCameraClose( hCamera );
err = VmbShutdown ();
Struct VmbFrame_t¶
The struct VmbFrame_t represents not only the actual image data, but also additional information. You can find the referenced data types in the tables below.
Tip
The field “void* buffer” of the struct can be NULL when the struct ist passed to
VmbFrameAnnounce. In this case, the “alloc and announce” function of the TL
allocates buffer memory.
Struct entry |
Type |
|---|---|
void* buffer |
Pointer to the actual image data |
VmbUint32_t bufferSize |
Size of the data buffer |
void* context[4] |
4 void pointers that can be employed by the |
VmbFrameStatus_t receiveStatus |
Resulting status of the receive operation |
VmbFrameFlags_t receiveFlags |
Flags indicating which additional frame |
VmbUint32_t chunkSize |
Size of the chunk data inside the data buffer |
VmbPixelFormat_t pixelFormat |
Pixel format of the image |
VmbUint32_t width |
Width of an image |
VmbUint32_t height |
Height of an image |
VmbUint32_t offsetX |
Horizontal offset of an image |
VmbUint32_t offsetY |
Vertical offset of an image |
VmbUint64_t frameID |
Unique ID of this frame in this stream |
VmbUint64_t timestamp |
Timestamp set by the camera |
Enumeration |
Integer Value |
Purpose |
|---|---|---|
VmbFrameStatusComplete |
0 |
Frame was completed without errors |
VmbFrameStatusIncomplete |
-1 |
Frame could not be filled to the end |
VmbFrameStatusInvalid |
-3 |
Frame buffer was invalid |
Enumeration |
Integer Value |
Purpose |
|---|---|---|
VmbFrameFlagsNone |
0 |
No additional information is provided |
VmbFrameFlagsDimension |
1 |
Frame’s dimension is provided |
VmbFrameFlagsOffset |
2 |
Frame’s offset is provided (ROI) |
VmbFrameFlagsFrameID |
4 |
Frame’s ID is provided |
VmbFrameFlagsTimestamp |
8 |
Frame’s timestamp is provided |
Transforming images¶
To transform images received via the API into common image formats, use the Image Transform Library.
See also
For a quick start, see the AsynchrounousGrab example, which contains an image transformation.
Using Events¶
Events serve many purposes and can have several origins such as generic
camera events or just feature changes.
All of these cases are handled in the C API uniformly with the same
mechanism: You simply register a notification callback with
VmbFeatureInvalidationRegister() for the feature of your
choice which gets called when there is a change to that feature.
Three examples are listed in this chapter:
Camera list notifications
Camera event features
Tracking invalidations of features
// 1. define callback function
void VMB_CALL CameraListCB( VmbHandle_t handle , const char* name , void* context )
{
char cameraName [255];
char callbackReason [255];
// Get the name of the camera due to which the callback was triggered
VmbFeatureStringGet( handle , "DiscoveryCameraIdent", cameraName );
// Get the reason why the callback was triggered. Possible values:
// Missing (0), a known camera disappeared from the bus
// Detected (1), a new camera was discovered
// Reachable (2), a known camera can be accessed
// Unreachable (3), a known camera cannot be accessed anymore
VmbFeatureEnumGet( handle , "DiscoveryCameraEvent", callbackReason );
printf( "Event was fired by camera %s because %s\n", cameraName ,
callbackReason );
}
// 2. register the callback for that event
VmbFeatureInvalidationRegister( gVimbaHandle , "DiscoveryCameraEvent",
CameraListCB , NULL );
// 3. for GigE cameras , invoke "GeVDiscoveryAllOnce"
VmbFeatureCommandRun( gVimbaHandle , "GeVDiscoveryAllOnce" );
Getting notified about feature changes:
void VMB_CALL WidthChangeCB( VmbHandle_t handle , const char* name , void* context )
{
printf( "Feature changed: %s\n", name );
}
// 2. register callback for changes to Width
VmbFeatureInvalidationRegister( cameraHandle , "Width", WidthChangeCB , NULL );
// as an example , binning is changed , so the callback will be run
VmbFeatureIntegerSet( cameraHandle , "Binning", 4 );
Getting notified about feature invalidations:
// 1. define callback function
void VMB_CALL WidthChangeCB( VmbHandle_t handle , const char* name , void* context )
printf( "Feature changed: %s\n", name );
}
// 2. register callback for changes to Width
VmbFeatureInvalidationRegister( cameraHandle , "Width", WidthChangeCB , NULL );
// as an example , binning is changed , so the callback will be run
VmbFeatureIntegerSet( cameraHandle , "Binning", 4 );
Getting notified about camera events:
GigE camera events are also handled with the same mechanism of feature invalidation.
// 1. define callback function
void VMB_CALL EventCB( VmbHandle_t handle , const char* name , void* context )
{
printf( "Event was fired: %s\n", name );
}
// 2. select "AcquisitionStart" event
VmbFeatureEnumSet( cameraHandle , "EventSelector", "AcquisitionStart" );
// 3. switch on the event notification
VmbFeatureEnumSet ( cameraHandle , "EventNotification", "On" );
// 4. register the callback for that event
VmbFeatureInvalidationRegister( cameraHandle , "EventAcquisitionStart",
EventCB , NULL );
Saving and loading settings¶
See also
For a quick start, see the LoadSaveSettings example.
Additionally to the user sets stored inside the cameras, you can save the feature values as an XML file to
your host PC. For example, you can configure your camera with Vimba Viewer, save the settings as a file,
and load them with Vimba API. To do this, use the functions
VmbSettingsLoad and VmbSettingsSave.
To control which features are saved, use the (optional) flags and struct listed below. You can manually edit the XML file if you want only certain features to be restored.
Note
Saving and loading all features including look-up tables may take several minutes.
The struct VmbFeaturePersistSettings_t contains the optional member cameraPersistFlags. It is only evaluated if a cameraHandle is passed to the load/save functions and ignored for the other module handles.
Struct Entry |
Purpose |
|---|---|
VmbFeaturePersist_t persistType |
Controls which features are saved. Valid values: |
VmbCameraPersistFlags_t |
Optional flags, see above |
Vmbuint32_t maxIterations |
Number of iterations. LoadCameraSettings iterates |
VmbUint32_t |
Logging level |
VmbCameraPersistFlagsNone |
0x00 |
|---|---|
VmbCameraPersistFlagsTransportLayer |
0x01 |
VmbCameraPersistFlagsInterface |
0x02 |
VmbCameraPersistFlagsRemoteDevice |
0x04 |
VmbCameraPersistFlagsLocalDevice |
0x08 |
VmbCameraPersistFlagsStreams |
0x10 |
VmbCameraPersistFlagsAll |
0ff |
If the flags are not set (=VmbCameraPersistFlagsNone), the default behavior is to only save/load the remote device features. The same behavior is applied if no VmbFeaturePersistSettings_t parameter is passed to the save/load functions.
Triggering¶
Note
Before triggering, startup the API and open the camera(s).
External trigger¶
The following code snippet shows how to trigger your camera with an external device.
// Startup Vimba, get cameras and open cameras as usual
// Trigger cameras according to their interface
// Configure trigger input line and selector , switch trigger on
switch( pInterfacetype )
{
case VmbInterfaceEthernet:
VmbFeatureEnumSet( pCameraHandle , "TriggerSelector", "FrameStart" );
VmbFeatureEnumSet( pCameraHandle , "TriggerSource", "Line1" );
VmbFeatureEnumSet( pCameraHandle , "TriggerMode", "On" );
break;
case VmbInterfaceUsb:
VmbFeatureEnumSet( pCameraHandle , "LineSelector", "Line0" );
VmbFeatureEnumSet( pCameraHandle , "LineMode", "Input" );
VmbFeatureEnumSet( pCameraHandle , "TriggerSelector", "FrameStart" );
VmbFeatureEnumSet( pCameraHandle , "TriggerSource", "Line0" );
VmbFeatureEnumSet( pCameraHandle , "TriggerMode", "On" );
break;
}
Trigger over Ethernet – Action Commands¶
See also
For a quick start, see the ActionCommands example.
See also
Find more details in the application note: Trigger over Ethernet (ToE) - Action Commands
Triggering via the AcquisitionStart command is supported by all cameras.
However, it is less precise than triggering with an external device connected
to the camera’s I/O port. Some GigE cameras additionally support Action Commands.
With Action Commands, you can broadcast a trigger signal simultaneously to
multiple GigE cameras via GigE cable.
Action Commands must be set first to the camera(s) and then to the TL,
which sends the Action Commands to the camera(s). As trigger source,
select Action0 or Action1.
ActionControl parameters
The following ActionControl parameters must be configured on the camera(s) and on the TL.
ActionDeviceKey must be equal on the camera and on the host PC. Before a camera accepts an Action Command, it verifies if the received key is identical with its configured key. Note that ActionDeviceKey must be set each time the camera is opened. Range (camera and host PC): 0 to 4294967295
ActionGroupKey means that each camera can be assigned to exactly one group for Action0 and a different group for Action1. All grouped cameras perform an action at the same time. If this key is identical on the sender and the receiving camera, the camera performs the assigned action. Range (camera and host PC): 0 to 4294967295
ActionGroupMask serves as filter that specifies which cameras within a group react on an Action Command. It can be used to create sub-groups. Range (camera): 0 to 4294967295 Range (host PC): 1 to 4294967295
Executing the feature ActionCommands sends the ActionControl parameters to the cameras and triggers the assigned action, for example, image acquisition. Before an Action Command is executed, each camera validates the received ActionControl parameter values against its configured values. If they are not equal, the camera ignores the command.
// Additionally to this code snippet:
// Configure the trigger settings and add image streaming
VmbUint32_t count;
VmbCameraInfo_t* cameras;
VmbHandle_t* handles;
int deviceKey = 11, groupKey = 22, groupMask = 33;
// Start Vimba and discover GigE cameras
VmbStartup( NULL );
// Get cameras
VmbCamerasList( NULL, 0, &count, sizeof(*cameras) );
cameras = (VmbCameraInfo_t *) malloc( count * sizeof(*cameras) );
VmbCamerasList( cameras, count, &count, sizeof(*cameras) );
// Allocate space for handles
handles = (VmbHandle_t*) malloc( count * sizeof(VmbHandle_t) );
for( int i=0; i<count; ++i )
{
const char* cameraId = cameras[i].cameraIdString;
// Open camera
VmbCameraOpen( cameraId, VmbAccessModeFull, &handles[i] );
// Set device key, group key and group mask
// Configure trigger settings (see programming example)
VmbFeatureIntSet( handles[i], "ActionDeviceKey", deviceKey );
VmbFeatureIntSet( handles[i], "ActionGroupKey", groupKey );
VmbFeatureIntSet( handles[i], "ActionGroupMask", groupMask );
}
// Set Action Command to API
// Allocate buffers and enable streaming (see programming example)
VmbFeatureIntSet( gVmbHandle, "ActionDeviceKey", deviceKey );
VmbFeatureIntSet( gVmbHandle, "ActionGroupKey", groupKey );
VmbFeatureIntSet( gVmbHandle, "ActionGroupMask", groupMask );
// Send Action Command
VmbFeatureCommandRun( gVmbHandle, "ActionCommand" );
// If no further Actions will be applied: close cameras, shutdown API, and
// free allocated space as usual
Listing interfaces¶
You can list all found interfaces such as frame grabbers or NICs.
VmbInterfacesList() enumerates all interfaces recognized
by the underlying transport layers.
VmbUint32_t nCount;
VmbInterfaceInfo_t *pInterfaces;
// Get the number of connected interfaces
VmbInterfacesList( NULL , 0, &nCount , sizeof *pInterfaces );
// Allocate accordingly
pInterfaces = (VmbInterfaceInfo_t *) malloc( nCount * sizeof *pInterfaces );
// Get the interfaces
VmbInterfacesList( pCameras , nCount , &nCount , sizeof *pInterfaces );
Struct VmbInterfaceInfo_t¶
Struct VmbInterfaceInfo_t provides the entries listed in the table below for obtaining read-only information about an interface.
Type |
Field |
Purpose |
|---|---|---|
const char* |
interfaceIdString |
Unique identifier for each interface |
VmbTransportLayerType_t |
interfaceType |
See VmbTransportLayerType |
const char* |
interfaceName |
Given by the TL |
VmbHandle_t |
transportLayerHandle |
For TL system module feature access |
VmbHandle_t |
interfaceHandle |
For interface module feature access |
Enabling notifications of changed interface states¶
To get notified whenever an interface is detected or disconnected, use
VmbFeatureInvalidationRegister() to register a callback that gets
executed on the according event.
Use the global Vmb handle for registration. The function pointer to
the callback function has to be of type VmbInvalidationCallback().
Interface enumerations¶
Enumeration |
Integer Value |
Interface |
VmbInterfaceUnknown |
0 |
Interface is not known to the API |
VmbInterfaceFirewire |
1 |
IEEE 1394 |
VmbInterfaceEthernet |
2 |
GigE |
VmbInterfaceUsb |
3 |
USB |
VVmbInterfaceCl |
4 |
Camera Link |
VmbTransportLayerTypeCXP |
5 |
CoaXPress |
VmbTransportLayerTypeCLHS |
6 |
Camera Link HS |
VmbTransportLayerTypeU3V |
7 |
USB3 Vision Standard |
VmbTransportLayerTypeEthernet |
8 |
Generic Ethernet |
VmbTransportLayerTypePCI |
9 |
PCI / PCIe |
VmbTransportLayerTypeCustom |
10 |
Non standard |
VmbTransportLayerTypeMixed |
11 |
Mixed (System module only) |
Note
Functions that must not be called be called within the callback routine:
VmbStartup
VmbShutdown
VmbFeatureIntSet (and any other VmbFeature*Set function)
VmbFeatureCommandRun
Error codes¶
Error Code |
Value |
Description |
|---|---|---|
VmbErrorSuccess |
0 |
No error |
VmbErrorInternalFault |
-1 |
Unexpected fault in Vmb or driver |
VmbErrorApiNotStarted |
-2 |
VmbStartup was not called before the current command |
VmbErrorNotFound |
-3 |
The designated instance (camera, feature, etc.) cannot be found |
VmbErrorBadHandle |
-4 |
The given handle is not valid |
VmbErrorDeviceNotOpen |
-5 |
Device was not opened for usage |
VmbErrorInvalidAccess |
-6 |
Operation is invalid with the current access mode |
VmbErrorBadParameter |
-7 |
One of the parameters is invalid (usually an illegal pointer) |
VmbErrorStructSize |
-8 |
The given struct size is not valid for this version of the API |
VmbErrorMoreData |
-9 |
More data available in a string/list than space is provided |
VmbErrorWrongType |
-10 |
Wrong feature type for this access function |
VmbErrorInvalidValue |
-11 |
The value is not valid; either out of bounds or not an |
VmbErrorTimeout |
-12 |
Timeout during wait |
VmbErrorOther |
-13 |
Other error |
VmbErrorResources |
-14 |
Resources not available (e.g., memory) |
VmbErrorInvalidCall |
-15 |
Call is invalid in the current context (e.g. callback) |
VmbErrorNoTL |
-16 |
No transport layers are found |
VmbErrorNotImplemented |
-17 |
API feature is not implemented |
VmbErrorNotSupported |
-18 |
API feature is not supported |
VmbErrorIncomplete |
-19 |
The current operation was not completed (e.g. a multiple |
VmbErrorIO |
-20 |
There was an error during read or write with devices |
See also
If your TL or camera is not found or if you experience other issues, see Troubleshooting.