NUC API Manual#
Introduction to the API#
Purpose and Scope#
VmbNUC API serves as a tool to calculate the NUC file.
Compatibility#
Supported cameras:
Goldeye cameras
Goldeye Pro cameras
Supported inputs:
Frames acquired with VmbC up to 16 bits
Images in PGM format
NUC generation with up to 100 images
Pixel formats: Mono8 up to Mono16
API usage#
See also
Use the examples provided in C:\Users\Public\Documents\Allied Vision\Vimba X\Examples\VmbNUC, and also provided as executables in VimbaX/bin.
To use VmbNUC API, perform these steps:
Configure the light source and camera settings for low exposure images.
Wait until the temperature is stable. Use the compiled examples LiveStreamToAverage.exe and ReadImages.exe avalailabe in Vimba X\bin with parameters, or use the sources to compile the examples with CMake.
Use example LiveStreamToAverage and adapt the values of exposure, gain and temperature to your needs. Specify an output directory for low exposure images. For details, use the ‘--help’ parameter or read the comments and strings in the example.
Repeat the steps above with high exposure.
Use example ReadImages with the same values for exposure, gain, and temperature and upload the file to your camera as usual with Vimba FileAccess.
// Example and output directory usage
// Temperature setpoint uses the current camera settings
// Make sure to use consistent parameters
mkdir "C:\Temp\low-exposure"
LiveStreamToAverage.exe --output-directory "C:\Temp\low-exposure" --frames 10 --
pixel-format Mono12 --exposure-time 10000 --gain 1
mkdir "C:\Temp\high-exposure"
LiveStreamToAverage.exe --output-directory "C:\Temp\high-exposure" --frames 10 --
pixel-format Mono12 --exposure-time 10000 --gain 1
ReadImages.exe "C:\Temp\low-exposure" "C:\Temp\high-exposure" --sensor-temp 20.0 --
pixel-format Mono12 --exposure-time 10000 --gain 1 --export-type "GoldeyeG"
Uploading files to the camera#
See also
FileAccessControl features are described in the Goldeye and Goldeye Pro Features Reference: https://www.alliedvision.com/en/support/camera-documentation/area-scan-cameras-documentation
Warning
Use one of the ‘.._User_..’ file slots to upload your data.
All uploaded NUC files must have a unique set of settings: Gain / Temperature / Exposure Time.
To upload the NUC files to the camera, follow these instructions:
Select and check a file#
- Select and check:
Select the NUC file and set FileSelector to the desired value.
To do this, use an available NUC_User_XXX file slot.
Check the current file status with the FileStatus feature.
If the status is not Closed, use FileOperationSelector to select file operation Close and execute the command
FileOperationExecute.
Tip
After every execution of
FileOperationExecute, you can check the status of the operation by reading the value of FileOperationStatus.If a file in the camera contains no data (value of FileSize is 0), you can see the name of the file slot, but you cannot open it for reading. You can open it only for writing.
Open the file#
- Open the file for write operations:
Set FileOperationSelector to Open and execute the command
FileOperationExecute.Set FileOpenMode to Write and execute the command
FileOperationExecute.
Load and upload the file#
- Load and upload the NUC file:
Load the complete NUC file from the host to an array to load it to the camera.
Set FileOperationSelector to Write and execute the command
FileOperationExecute.Use the range of the feature FileAccessLength to determine the maximum length of FileAccessBuffer.
Loop over the input vector, uploading chunks of data <= max. buffer length:
Fill the feature FileAccessBuffer with data.
Write the current buffer size into FileAccessLength.
Execute the command
FileOperationExecute.Get the number of transferred bytes from the camera. To do this, read the value of FileOperationResult.
Move to the next vector position using the number of transferred bytes.
Execute the file operation: Set FileOperationSelector to Close and execute the command
FileOperationExecute.