Vimba X for ARM64 Release Notes
Version: 2026-1
Summary
Main changes in this release:
New component: VmbNUC API for Goldeye and Goldeye Pro
VmbPy: Deprecated support for Python <3.10
New VmbC behavior: Lazy feature initialization allows faster camera listing
Real-time thread scheduling policies can be set for root and other users, see chapter “Real-time thread scheduling policies” in the documentation.
Transport Layer |
Version |
|---|---|
GigE Transport Layer (VimbaGigETL.cti) |
1.10.3 |
USB Transport Layer (VimbaUSBTL.cti) |
1.7.1* |
CSI Transport Layer (VimbaCSITL.cti) |
2.2.1* |
APIs |
Version |
|---|---|
VmbC API (libVmbC.dll) |
1.3.0* |
VmbCPP API (libVmbCPP.dll) |
1.3.0* |
VmbNET API |
1.3.2* |
VmbPy API |
1.2.1* |
Image Transform Library (libVmbImageTransform.dll) |
2.3.0 |
VmbNUC API |
1.0.0* |
Tools |
Version |
|---|---|
Vimba X Viewer |
1.4.4* |
Vimba X Firmware Updater |
2.2.0* |
* Changed in this release of Vimba X
Hardware requirements
ARM board with ARMv8-compatible 64-bit processor
GigE cameras
A built-in Gigabit Ethernet network interface or Gigabit Ethernet network card (one or more) is required.
Note for IP configuration: By default, IP Configuration Mode is set to DHCP. You can use the IP Configuration dialog of Vimba X Viewer to apply changes or to force the IP address.
Allied Vision USB cameras
A built-in USB 3.0 (or higher) controller for PCI Express bus is required.
Testing has been performed on host controllers that are based on Asmedia chip sets. The driver may run on host controllers that are based on chip sets from other vendors, too. If there are any problems please feel free to contact our Technical Support.
Tested platforms
Ubuntu 22.04 LTS (JetPack6.2.1)
GigE and USB TL:
Vimba X was tested with NVIDIA JetPack 6.2.1 on on the following Jetson SOM:
AGX Orin Developer Kit
CSI TL:
Vimba X was tested with NVIDIA JetPack 6.2.1 on on the following Jetson SOMs:
AGX Orin Developer Kit
Orin Nano 8GB Developer Kit
Orin NX 16GB + forecr carrier board
Orin Nano 4GB + forecr carrier board
For supported camera models, the latest known issues, and other useful information, see: Getting Started with GenICam for CSI-2
Installation
To install Vimba X:
Uncompress the archive with the command tar -xf ./VimbaX.tgz to a directory you have writing privileges for like /opt. Under this directory, Vimba X will be installed in its own folder. In the following, we will refer to this path as [InstallDir].
Go to [InstallDir]/cti/and call (as needed, using sudo) Install_GenTL_Path.sh.
Reboot your system.
If you have issues, see the Developer Guide, section Troubleshooting.
Vimba X Viewer: Vimba X Viewer can be found in[InstallDir]/bin/.
Examples: Vimba X includes precompiled examples that you can find in: [InstallDir]/bin. Uncompiled examples are located in: [InstallDir]/api/examples.
Uninstalling Vimba X: To uninstall Vimba X, go to [InstallDir]/bin and run the uninstall scripts as super user. This prevents any GenTL consumer from loading the Vimba Transport Layers. Then remove the installation directory.
Known issues
The following issues are known:
When experiencing trouble with image acquisition, try to increase the priority of your application with “sudo -E nice -n -20
”.
Camera detection:
If multiple IP addresses are configured on one physical Ethernet adapter, then Vimba X sends GVCP discovery requests only to the last added IP address. Therefore, the camera is detected only if its IP address was added last.
Vimba X Viewer:
With some camera models, the message “Vimba X Viewer is not responding” appears for a few seconds when the camera is opened.
If the IP address is changed within the same network, the camera list doesn’t update automatically. Please click the Refresh button.
Sporadic issue: If a GigE camera was opened and then closed with Vimba X Viewer, it is displayed as locked and Vimba X Viewer does not open it again. Workaround: Close and open Vimba X Viewer.
With CSI-2 cameras, the Trigger IO tab is unavailable.
Moving test image from Camera Simulator: With Bayer pixel formats, the color interpolation causes wrong colors.
GigE Transport Layer:
A change of the available camera access modes cannot be reported for cameras in different subnets or with malconfigured IP addresses.
Not all ARM boards come with a GigE network interface. When acquiring images with only 100 Mbit/s, make sure to set the “StreamBytesPerSecond” feature to a reasonable small value (12 400 000). This adjustment is done automatically when the camera is connected directly to a 100 Mbit/s interface.
GigE cameras may be listed on a wrong Ethernet interface.
If many dropped frames occur especially with a small ROI, set GVSP Timeout to a higher value.
Vimba X APIs:
When API startup and shutdown is performed excessively within the same process, camera initialization may fail sporadically, which may cause exceptions. We recommend to have only one API session during one process.
Load/Save Settings: Not all LUT settings are saved.
Examples:
If a camera is already open, sometimes a misleading error message occurs (“Bad parameter”).
The ListFeatures example does not list all Interface features.
Sporadic issue of the AsynchronousGrab and Chunk example: stopping the stream causes an exception.
Camera detection:
If multiple IP addresses are configured on one physical Ethernet adapter, then Vimba X sends GVCP discovery requests only to the last added IP address. Therefore, the camera is detected only if its IP address was added last.
CSI-2:
For the latest known issues, see Getting Started with GenICam for CSI-2
If your application causes dropped frames, try to increase the number of frame buffers to approximately 7.
Switching the camera from GenICam for CSI-2 to V4L2 or vice versa requires rebooting the board.
Exposure times greater than approx. 1 second: Stopping acquisition may cause an error. Please close and open the camera to start streaming again.
Changes and release history
Changes in Vimba X 2026-1
VmbC:
Lazy feature initialization for faster camera listing
VmbCPP:
Internal changes
VmbNET:
Minor internal changes
VmbPy:
Fixed: VmbPy error codes differ from VmbC
Several minor bug fixes
Deprecated support for Python <3.10
VmbNUC:
First release, Goldeye and Goldeye Pro support
USBTL:
Minor internal changes
Camera Simulator TL:
Several bug fixes
CSITL:
Fixed: First frame invalid with Alvium GM2 cameras
Vimba X Viewer:
Minor internal changes
Firmware Updater:
Added info message if the update requires a hard reset (Alvium firmware v15)
Changes in Vimba X 2025-3
VmbC:
New logging implementation
OpenCV bridge header
VmbCPP:
OpenCV bridge header
VmbCPP example for Open CV bridge
VmbNET:
Minor bugfixes, updated README.md
DeinterlaceFrameis available
VmbPy:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
DeinterlaceFrameis availableImproved performance of
AllocationMode.AnnounceFrame
USBTL:
Minor internal changes
GigETL:
Added IP configuration features for Allied Vision legacy cameras (Manta, Mako, Goldeye, Prosilica GT)
CSITL:
Added ALECS / SmartCam support
Vimba X Viewer:
Minor bugfixes
Image Transform Library:
Added function
VmbDeinterlaceFrame()to support IMX900 sensor HDR processing
Firmware Updater:
Updating more than one selected Goldeye Pro camera is now possible
Changes in Vimba X 2025-2
VmbC:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
VmbCPP:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
VmbNET:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
Several minor bugfixes
Adjusted Nuget Package ID to include platform specifier
VmbPy:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
USBTL:
Added Stream leader/trailer received events
Added endpoint-flushing
GigETL:
Minor bugfixes
Vimba X Viewer:
Adaptations for Goldeye Pro support
Firmware Updater:
Added Goldeye Pro support
Changes in Vimba X 2025-1
VmbC:
Minor bugfixes
VmbCPP:
Minor bugfixes
VmbNET:
New API
VmbPy:
VmbC (+ GenAPI dependencies) included in Python wheel to make VmbPy self-contained
Image Transform Library:
Exported new function VmbGetCompatiblePixelFormat
GigETL:
Adjustments for support of future cameras
CSITL:
Bug fixes
JetPack 6 support
Vimba X Viewer:
Minor bug fixes
Changes in Vimba X 2024-1
VmbC:
Loads transport layers found in the same directory as VmbC.dll
Improved logging
VmbCPP:
Minor bug fixes
VmbPy:
Minor Bugfixes
VmbPy type hint improvements for better autocompletion in IDEs
GigETL:
Breaks compatibility with Vimba 6 (Vimba 6 Config mode not working anymore with latest Vimba X GigETL)
Cameras from Allied Vision Gilching (formerly SVS-Vistek) are enabled by default
Marked old statistic features as “deprecated”
Minor bug fixes
USBTL:
Added new GenTL Buffer Info “BUFFER_INFO_DATA_SIZE”
Updated uriparser to 0.9.8
Vimba X Viewer:
“Image Format tab” including Multi ROI
Event Viewer window access has moved to icons above the image
Image Processing tab:
Sobel horizontal/vertical was interchanged in the camera firmware until firmware 13.x and the Viewer GUI compensated for that. With firmware 14, this is corrected in the camera and aligned to firmware 14 in the Viewer GUI.
Better performance when using high frame rates > 1000 fps
Minor bugfixes
Firmware Updater:
Fixed: With some Alvium camera models, the firmware update may take up to 5 minutes.
Image Transform Library:
Added support for 3x3 debayering of packed formats
Changes in Vimba X 2023-4
VmbC:
Added macOS support
VmbCPP:
Added macOS support
VmbPy:
Added macOS support
ImageTransform:
Added macOS support
USBTL:
Added macOS support
Added Event support
Vimba X Viewer:
Added macOS support
Added Sequencer tab
Vimba X Firmware Updater:
Added macOS support
GigETL:
Improved Adjust PacketSize
Changes in Vimba X 2023-2
VmbC:
Fixed: Open camera by IP may take 15s
Added Exclusive Access mode
VmbCPP:
Fixed: Open camera by IP may take 15s
VmbPy:
Fixed: Open camera by IP may take 15s
Fixed type hints for Python <=3.7.5 and =3.8.0
Updated AccessMode enum for consistency with VmbC
Added option for visibility level to list_features.py
USBTL:
Improved: standard conformity of resend for control channel commands
Changes in Vimba X 2022-1
VmbC:
New API (similar, but not compatible to VimbaC)
VmbCPP:
New API (similar, but not compatible to VimbaCPP)
VmbPy:
New API (similar, but not compatible to VimbaPython)
Image Transform:
Added supported transformations (supports pixel formats of NET cameras)
Renamed VmbGetVersion to VmbGetImageTransformVersion
VmbSetImageInfoFromString: removed stringLength parameter
Vimba X Viewer:
New Viewer (based on Vimba Viewer)
Additional features: Chunk support, 5x5 Matrix, Scheduled Action commands
GigETL:
Display name: AVT GigE TL (instead of Vimba GigE TL)
Scheduled Action Commands support
Chunk support
Pending_Ack support
USBTL:
Display name: AVT USB TL (instead of Vimba USB TL)
No functional changes, version was incremented because of internal changes
Known issues
The following issues are known:
Load/Save settings: We recommend using FeaturePersistType Streamable. Loading settings may cause errors when FeaturePersistTypes All or NoLUT were selected.