Vimba X for Windows Release Notes
Version: 2026-1
Summary
Main changes in this release:
New component: Camera Link Config TL for Goldeye CL support (Windows only)
New component: VmbNUC API for Goldeye and Goldeye Pro
VmbPy: Deprecated support for Python <3.10
New VmbC behavior: Lazy feature initialization for faster camera listing
Transport Layer |
Version |
|---|---|
GigE Transport Layer (VimbaGigETL.cti) |
1.10.3 |
USB Transport Layer (VimbaUSBTL.cti) |
1.7.1* |
Camera Simulator TL |
1.0.1* |
RDMA Transport Layer (sv_gev_rdma_tl.cti) |
2.5.9.3116 (Beta) |
CL Config TL (VimbaCLSerialTL.cti) |
2.0.0* |
APIs |
Version |
|---|---|
VmbC API (libVmbC.dll) |
1.3.0* |
VmbCPP API (libVmbCPP.dll) |
1.3.0* |
VmbNET API |
1.3.2* |
VmbPy API |
1.2.1* |
Image Transform Library (libVmbImageTransform.dll) |
2.3.0 |
VmbNUC API |
1.0.0* |
Drivers |
Version |
|---|---|
Vimba X GigE Filter Driver |
2.5.13 |
Tools |
Version |
|---|---|
Vimba X Viewer |
1.4.4* |
Vimba X Firmware Updater |
2.2.0* |
Vimba X Driver Installer |
2.1.0 |
* Changed in this release of Vimba X
Hardware requirements
PC or laptop with 64-bit x86 processor or better.
GigE cameras
A built-in Gigabit Ethernet network interface or Gigabit Ethernet network card (one or more) is required.
Note for IP configuration: By default, IP Configuration Mode is set to DHCP. You can use the IP Configuration dialog of Vimba X Viewer to apply changes or to force the IP address.
Allied Vision USB cameras
A built-in USB 3.0 (or higher) controller for PCI Express bus is required.
Testing has been performed on host controllers that are based on Asmedia chip sets. The driver may run on host controllers that are based on chip sets from other vendors, too. If there are any problems please feel free to contact our Technical Support.
Installation
To install Vimba X, use VimbaX.exe and follow the instructions.
Correlations with other Allied Vision Software Packages
You can install and use Vimba and Vimba X on the same host. We recommend using our GigE filter driver with Vimba X or Vimba only.
Supported operating systems
Vimba X was tested with:
Windows 10 21H2 LTSC
Windows 11 24H2 Pro
Known issues
Setup:
Vimba X driver installation disconnects VPN. For a smooth installation, please disconnect VPN before installing Vimba X.
To install the USB driver, please connect your Allied Vision USB camera before starting Vimba X installation. After installation, you can always use Vimba X Driver Installer.
During installation, Vimba setup configures some environment variables that are - among others - used when compiling the examples. In order to use the new environment variables, it might be necessary to restart Microsoft Visual Studio, log off, or even restart the operating system.
In some cases, the Vimba X installer message about successfully installed drivers is incorrect.
Vimba X APIs:
When API startup and shutdown is performed excessively within the same process, camera initialization may fail sporadically, which may cause exceptions. We recommend to have only one API session during one process.
Load/Save Settings: Not all LUT settings are saved.
GigE Filter Driver:
If Vimba and Vimba X are installed on the same system: The Filter Driver provided with Vimba X overwrites Vimba’s Filter Driver. If you still work with Vimba: Use the included Driver Installer to deactivate and activate the correct Filter Driver.
Using other filter drivers additionally to the included GigE Filter Driver (including the Filter Driver of the Vimba SDK) may cause issues, even a blue screen.
Disabling the Vimba GigE Filter Driver while it is in use might lead to unexpected behavior up to blue screen.
GigE Transport Layer:
A change of the available camera access modes cannot be reported for cameras in different subnets or with malconfigured IP addresses.
GigE cameras may be listed on a wrong Ethernet interface.
If many dropped frames occur especially with a small ROI, set GVSP Timeout to a higher value.
5 GigE Vision cameras:
Unplugging an USB device while the camera is streaming may cause lost frames, especially when the socket driver is used.
Vimba X Viewer:
With some camera models, the message “Vimba X Viewer is not responding” appears for a few seconds when the camera is opened.
If the IP address is changed within the same network, the camera list doesn’t update automatically. Please click the Refresh button.
Sporadic issue: When multiple opened GigE cameras are disconnected at the same time while no other camera stays connected to the very same NIC, the Viewer’s camera windows stay open.
Legacy cameras: The All tab supports all legacy cameras. The other tabs only support GenICam-compliant features.
Moving test image from Camera Simulator: With Bayer pixel formats, the color interpolation causes wrong colors.
Examples:
If a camera is already open, sometimes a misleading error message occurs (“Bad parameter”).
The ListFeatures example does not list all Interface features.
Sporadic issue of the AsynchronousGrab and Chunk example: stopping the stream causes an exception.
Changes and release history
Changes in Vimba X 2026-1
VmbC:
Lazy feature initialization for faster camera listing
VmbCPP:
Internal changes
VmbNET:
Minor internal changes
VmbPy:
Fixed: VmbPy error codes differ from VmbC
Several minor bug fixes
Deprecated support for Python <3.10
VmbNUC:
First release, Goldeye and Goldeye Pro support
USBTL:
Minor internal changes
Camera Simulator TL:
Several bug fixes
CL Config TL:
First release in Vimba X (migrated from Vimba)
Vimba X Viewer:
Minor internal changes
Firmware Updater:
Added info message if the update requires a hard reset (Alvium firmware v15)
Changes in Vimba X 2025-3
VmbC:
New logging implementation
OpenCV bridge header
VmbCPP:
OpenCV bridge header
VmbCPP example for Open CV bridge
VmbNET:
Minor bugfixes, updated README.md
DeinterlaceFrameis available
VmbPy:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
DeinterlaceFrameis availableImproved performance of
AllocationMode.AnnounceFrame
USBTL:
Minor internal changes
GigETL:
Added IP configuration features for Allied Vision legacy cameras (Manta, Mako, Goldeye, Prosilica GT)
Filter driver:
Internal changes, no changes for users
Driver installer:
Adaptions for new filter driver version
SVS-Vistek RDMA TL (Beta)
Transport layer with RDMA support for SVS-Vistek cameras (Beta)
Restrictions of this beta version:
AllocAndAnnounce is not available
Open by IP is not available
If VmbC is not used, the TL is not available
Vimba X Viewer:
Minor bugfixes
Image Transform Library:
Added function
VmbDeinterlaceFrame()to support IMX900 sensor HDR processing
Firmware Updater:
Updating more than one selected Goldeye Pro camera is now possible
Changes in Vimba X 2025-2
VmbC:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
VmbCPP:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
VmbNET:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
Several minor bugfixes
Adjusted Nuget Package ID to include platform specifier
VmbPy:
Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)
USBTL:
Added Stream leader/trailer received events
Added endpoint-flushing
USB driver:
Changed underlying driver (no impact on Vimba X or camera usage)
GigETL:
Minor bugfixes
Vimba X Viewer:
Adaptations for Goldeye and Goldeye Pro support
Firmware Updater:
Adaptations for Goldeye Pro support
Changes in Vimba X 2025-1
VmbC:
Minor bugfixes
VmbCPP:
Minor bugfixes
VmbNET:
New API
VmbPy:
VmbC (+ GenAPI dependencies) included in Python wheel to make VmbPy self-contained
Image Transform Library:
Exported new function VmbGetCompatiblePixelFormat
GigETL:
Adjustments for support of future cameras
CSITL:
Bug fixes
JetPack 6 support
Vimba X Viewer:
Minor bug fixes
Changes in Vimba X 2024-1
VmbC:
Loads transport layers found in the same directory as VmbC.dll
Improved logging
VmbCPP:
Minor bug fixes
VmbPy:
Minor Bugfixes
VmbPy type hint improvements for better autocompletion in IDEs
GigETL:
Breaks compatibility with Vimba 6 (Vimba 6 Config mode not working anymore with latest Vimba X GigETL)
Cameras from SVS-Vistek are enabled by default
Marked old statistic features as “deprecated”
Minor bug fixes
Filter driver:
Minor bugfixes
USBTL:
Added new GenTL Buffer Info “BUFFER_INFO_DATA_SIZE”
Updated uriparser to 0.9.8
Vimba X Viewer:
“Image Format tab” including Multi ROI
Event Viewer window access has moved to icons above the image
Image Processing tab:
Sobel horizontal/vertical was interchanged in the camera firmware until firmware 13.x and the Viewer GUI compensated for that. With firmware 14, this is corrected in the camera and aligned to firmware 14 in the Viewer GUI.
Better performance when using high frame rates > 1000 fps
Minor bugfixes
Firmware Updater:
Fixed: With some Alvium camera models, the firmware update may take up to 5 minutes.
Image Transform Library:
Added support for 3x3 debayering of packed formats
Changes in Vimba X 2023-4
VmbC:
Added macOS support
VmbCPP:
Added macOS support
VmbPy:
Added macOS support
ImageTransform:
Added macOS support
USBTL:
Added macOS support
Added Event support
Filter Driver:
Bug fixes
Vimba X Viewer:
Added macOS support
Added Sequencer tab
Vimba X Firmware Updater:
Added macOS support
GigETL:
Improved Adjust PacketSize
Changes in Vimba X 2023-2
VmbC:
Fixed: Open camera by IP may take 15s
Added Exclusive Access mode
VmbCPP:
Fixed: Open camera by IP may take 15s
VmbPy:
Fixed: Open camera by IP may take 15s
Fixed type hints for Python <=3.7.5 and =3.8.0
Updated AccessMode enum for consistency with VmbC
Added option for visibility level to list_features.py
GigETL:
Fixed: Vimba X freezes if the NIC is disabled during image acquisition.
GigE Filter Driver:
Supports extended status codes packet resend
USBTL:
Improved: standard conformity of resend for control channel commands
Changes in Vimba X 2022-1
VmbC:
New API (similar, but not compatible to VimbaC)
VmbCPP:
New API (similar, but not compatible to VimbaCPP)
VmbPy:
New API (similar, but not compatible to VimbaPython)
Image Transform:
Added supported transformations (supports pixel formats of NET cameras)
Renamed VmbGetVersion to VmbGetImageTransformVersion
VmbSetImageInfoFromString: removed stringLength parameter
Vimba X Viewer:
New Viewer (based on Vimba Viewer)
Additional features: Chunk support, 5x5 Matrix, Scheduled Action commands
GigETL:
Display name: AVT GigE TL (instead of Vimba GigE TL)
Scheduled Action Commands support
Chunk support
Filter Driver:
Chunk Support
Bug fixes
USBTL:
Display name: AVT USB TL (instead of Vimba USB TL)
Driver Installer:
The version was incremented to 2.0.0 because of internal changes (no functional changes for the user)