Vimba X for Linux x86_64 Release Notes

Version: 2026-1

Summary

Main changes in this release:

  • New component: VmbNUC API for Goldeye and Goldeye Pro

  • New component: RDMA TL (Beta)

  • VmbPy: Deprecated support for Python <3.10

  • New VmbC behavior: Lazy feature initialization allows faster camera listing

  • Real-time thread scheduling policies can be set for root and other users, see chapter “Real-time thread scheduling policies” in the documentation.

Transport Layer

Version

GigE Transport Layer (VimbaGigETL.cti)

1.10.3

USB Transport Layer (VimbaUSBTL.cti)

1.7.1*

RDMA Transport Layer (sv_gev_rdma_tl.cti)

2.5.9.3116 (Beta)*

APIs

Version

VmbC API (libVmbC.dll)

1.3.0*

VmbCPP API (libVmbCPP.dll)

1.3.0*

VmbNET API

1.3.2*

VmbPy API

1.2.1*

Image Transform Library (libVmbImageTransform.dll)

2.3.0

VmbNUC API

1.0.0*

Tools

Version

Vimba X Viewer

1.4.4*

Vimba X Firmware Updater

2.2.0*

* Changed in this release of Vimba X

Hardware requirements

PC or laptop with 64-bit x86 processor or better.

GigE cameras

A built-in Gigabit Ethernet network interface or Gigabit Ethernet network card (one or more) is required.

Note for IP configuration: By default, IP Configuration Mode is set to DHCP. You can use the IP Configuration dialog of Vimba X Viewer to apply changes or to force the IP address.

Allied Vision USB cameras

A built-in USB 3.0 (or higher) controller for PCI Express bus is required.

Testing has been performed on host controllers that are based on Asmedia chip sets. The driver may run on host controllers that are based on chip sets from other vendors, too. If there are any problems please feel free to contact our Technical Support.

Tested platforms and cameras

Vimba X was tested with:

  • Ubuntu 24.04 LTS

Installation

To install Vimba X:

  • Uncompress the archive with the command tar -xf ./VimbaX.tgz to a directory you have writing privileges for like /opt. Under this directory, Vimba X will be installed in its own folder. In the following, we will refer to this path as [InstallDir].

  • Go to [InstallDir]/cti/and call (as needed, using sudo) Install_GenTL_Path.sh.

  • Reboot your system.

  • If you have issues, see the Developer Guide, section Troubleshooting.

Vimba X Viewer: Vimba X Viewer can be found in[InstallDir]/bin.

Examples: Vimba X includes precompiled examples that you can find in: [InstallDir]/bin. Uncompiled examples are located in: [InstallDir]/api/examples.

Uninstalling Vimba X: To uninstall Vimba X, go to [InstallDir]/bin and run the uninstall scripts as super user. This prevents any GenTL consumer from loading the Vimba Transport Layers. Then remove the installation directory.

Known issues

The following issues are known:

  • When experiencing trouble with image acquisition, try to increase the priority of your application with “sudo -E nice -n -20 ”.

Camera detection:

  • If multiple IP addresses are configured on one physical Ethernet adapter, then Vimba X sends GVCP discovery requests only to the last added IP address. Therefore, the camera is detected only if its IP address was added last.

Vimba X Viewer:

  • With some camera models, the message “Vimba X Viewer is not responding” appears for a few seconds when the camera is opened.

  • If the IP address is changed within the same network, the camera list doesn’t update automatically. Please click the Refresh button.

  • Sporadic issue: If a GigE camera was opened and then closed with Vimba X Viewer, it is displayed as locked and Vimba X Viewer does not open it again. Workaround: Close and open Vimba X Viewer.

  • Legacy cameras: The All tab supports all legacy cameras. The other tabs only support GenICam-compliant features.

  • Moving test image from Camera Simulator: With Bayer pixel formats, the color interpolation causes wrong colors.

Vimba X APIs:

  • When API startup and shutdown is performed excessively within the same process, camera initialization may fail sporadically, which may cause exceptions. We recommend to have only one API session during one process.

  • Load/Save Settings: Not all LUT settings are saved.

GigE Transport Layer:

  • GigE cameras may be listed on a wrong Ethernet interface.

  • If many dropped frames occur especially with a small ROI, set GVSP Timeout to a higher value.

Examples:

  • If a camera is already open, sometimes a misleading error message occurs (“Bad parameter”).

  • The ListFeatures example does not list all Interface features.

  • Sporadic issue of the AsynchronousGrab and Chunk example: stopping the stream causes an exception.

Changes and release history

Changes in Vimba X 2026-1

VmbC:

  • Lazy feature initialization for faster camera listing

VmbCPP:

  • Internal changes

VmbNET:

  • Minor internal changes

VmbPy:

  • Fixed: VmbPy error codes differ from VmbC

  • Several minor bug fixes

  • Deprecated support for Python <3.10

VmbNUC:

  • First release, Goldeye and Goldeye Pro support

USBTL:

  • Minor internal changes

Camera Simulator TL:

  • Several bug fixes

RDMA TL (Beta)

  • Transport layer with RDMA support for camera from Allied Vision Gilching (Beta)

  • Restrictions of this beta version:

    • AllocAndAnnounce is not available

    • Open by IP is not available

    • If VmbC is not used, the TL is not available

Vimba X Viewer:

  • Minor internal changes

Firmware Updater:

  • Added info message if the update requires a hard reset (Alvium firmware v15)

Changes in Vimba X 2025-3

VmbC:

  • New logging implementation

  • OpenCV bridge header

VmbCPP:

  • OpenCV bridge header

  • VmbCPP example for Open CV bridge

VmbNET:

  • Minor bugfixes, updated README.md

  • DeinterlaceFrame is available

VmbPy:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

  • DeinterlaceFrameis available

  • Improved performance of AllocationMode.AnnounceFrame

USBTL:

  • Minor internal changes

GigETL:

  • Added IP configuration features for Allied Vision legacy cameras (Manta, Mako, Goldeye, Prosilica GT)

Vimba X Viewer:

  • Minor bugfixes

Image Transform Library:

  • Added function VmbDeinterlaceFrame() to support IMX900 sensor HDR processing

Firmware Updater:

  • Updating more than one selected Goldeye Pro camera is now possible

Changes in Vimba X 2025-2

VmbC:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

VmbCPP:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

VmbNET:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

  • Several minor bugfixes

  • Adjusted Nuget Package ID to include platform specifier

VmbPy:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

USBTL:

  • Added Stream leader/trailer received events

  • Added endpoint-flushing

GigETL:

  • Minor bugfixes

Vimba X Viewer:

  • Adaptations for Goldeye Pro support

Firmware Updater:

  • Added Goldeye Pro support

Changes in Vimba X 2025-1

VmbC:

  • Minor bugfixes

VmbCPP:

  • Minor bugfixes

VmbNET:

  • New API

VmbPy:

  • VmbC (+ GenAPI dependencies) included in Python wheel to make VmbPy self-contained

Image Transform Library:

  • Exported new function VmbGetCompatiblePixelFormat

GigETL:

  • Adjustments for support of future cameras

CSITL:

  • Bug fixes

  • JetPack 6 support

Vimba X Viewer:

  • Minor bug fixes

Changes in Vimba X 2024-1

VmbC:

  • Loads transport layers found in the same directory as VmbC.dll

  • Improved logging

VmbCPP:

  • Minor bug fixes

VmbPy:

  • Minor Bugfixes

  • VmbPy type hint improvements for better autocompletion in IDEs

GigETL:

  • Minor bug fixes

  • Cameras from SVS-Vistek are enabled by default

  • Breaks compatibility with Vimba 6 (Vimba 6 Config mode not working anymore with latest Vimba X GigETL)

  • Marked old statistic features as “deprecated”

USBTL:

  • Added new GenTL Buffer Info “BUFFER_INFO_DATA_SIZE”

  • Updated uriparser to 0.9.8

Vimba X Viewer:

  • “Image Format tab” including Multi ROI

  • Event Viewer window access has moved to icons above the image

  • Image Processing tab:

    • Sobel horizontal/vertical was interchanged in the camera firmware until firmware 13.x and the Viewer GUI compensated for that. With firmware 14, this is corrected in the camera and aligned to firmware 14 in the Viewer GUI.

  • Better performance when using high frame rates > 1000 fps

  • Minor bugfixes

Firmware Updater:

  • Fixed: With some Alvium camera models, the firmware update may take up to 5 minutes.

Image Transform Library:

  • Added support for 3x3 debayering of packed formats

Changes in Vimba X 2023-4

VmbC:

  • Added macOS support

VmbCPP:

  • Added macOS support

VmbPy:

  • Added macOS support

ImageTransform:

  • Added macOS support

USBTL:

  • Added macOS support

  • Added Event support

Vimba X Viewer:

  • Added macOS support

  • Added Sequencer tab

Vimba X Firmware Updater:

  • Added macOS support

GigETL:

  • Improved Adjust PacketSize

Changes in Vimba X 2023-2

VmbC:

  • Fixed: Open camera by IP may take 15s

  • Added Exclusive Access mode

VmbCPP:

  • Fixed: Open camera by IP may take 15s

VmbPy:

  • Fixed: Open camera by IP may take 15s

  • Fixed type hints for Python <=3.7.5 and =3.8.0

  • Updated AccessMode enum for consistency with VmbC

  • Added option for visibility level to list_features.py

Changes in Vimba X 2022-1

VmbC:

  • New API (similar, but not compatible to VimbaC)

VmbCPP:

  • New API (similar, but not compatible to VimbaCPP)

VmbPy:

  • New API (similar, but not compatible to VimbaPython)

Image Transform:

  • Added supported transformations (supports pixel formats of NET cameras)

  • Renamed VmbGetVersion to VmbGetImageTransformVersion

  • VmbSetImageInfoFromString: removed stringLength parameter

Vimba X Viewer:

  • New Viewer (based on Vimba Viewer)

  • Additional features: Chunk support, 5x5 Matrix, Scheduled Action commands

GigETL:

  • Display name: AVT GigE TL (instead of Vimba GigE TL)

  • Scheduled Action Commands support

  • Chunk support

USBTL:

  • Improved: standard conformity of resend for control channel commands

  • Display name: AVT USB TL (instead of Vimba USB TL)