Vimba CSI TL Release Notes
Version: 2.2.1
Components and Version Reference
Component |
Version |
|---|---|
CSI-2 Transport Layer (VimbaCSITL.cti) |
2.2.1 |
Supported hardware and driver
Vimba X was tested with NVIDIA JetPack 6.2 (Jetson Linux 36.4.3) on the following Jetson SOMs:
AGX Orin Developer Kit
Orin Nano 8GB Developer Kit
Orin NX 16GB + forecr carrier board
Orin Nano 4GB + forecr carrier board
All SOMs were tested with the driver for Allied Vision Alvium cameras.
See Getting Started with GenICam for CSI-2 for supported camera models, the latest known issues, and other useful information.
Installation
Prerequisites: NVIDIA JetPack 6.2 (Jetson Linux 36.4.3) and driver for Allied Vision Alvium cameras
Correlations with other Allied Vision Software Packages
You can install and use Vimba and Vimba X on the same host.
Known issues
For the latest known issues, see Getting Started with GenICam for CSI-2
If your application causes dropped frames, try to increase the number of frame buffers to approximately 7.
Switching the camera from GenICam for CSI-2 to V4L2 or vice versa requires rebooting the board.
Exposure times greater than approx. 1 second: Stopping acquisition may cause an error. Please close and open the camera to start streaming again.
Changes and release history
Changes in version 2.2.1
Fixed: First frame invalid with Alvium GM2 cameras
Changes in version 2.2.0
Added ALECS / SmartCam support
Changes in version 2.1.0
Bug fixes
JetPack 6 support
Changes in version 2.0.0
Added support for streaming on boards with i.MX 8M Plus EVK and Xilinx ZCU106 in our Yocto project, see https://github.com/alliedvision
Changes in version 1.2.0
Display name: AVT CSI TL (instead of Vimba CSI TL)
Fixed: Does not reset allocated buffers to Null
Changes in version 1.0.1
Support of new streaming format (better performance in Announce mode), latest camera firmware required.
Changes in version 1.0.0
Vimba CSITL new release