LocalDevice#

class vmbpy.LocalDevice#

This class provides access to the Local Device of a Camera.

get_all_features() → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get access to all discovered features.

Returns:

A set of all currently detected Features.

Raises:

RuntimeError – If called outside of with context.

get_feature_by_name(feat_name: str) → IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature#

Get a feature by its name.

Parameters:

feat_name – Name used to find a feature.

Returns:

Feature with the associated name.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

  • VmbFeatureError – If no feature is associated with feat_name.

get_features_by_category(category: str) → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get all features of a specific category.

Parameters:

category – Category that should be used for filtering.

Returns:

A set of features of category category.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

get_features_by_type(feat_type: Type[IntFeature] | Type[FloatFeature] | Type[StringFeature] | Type[BoolFeature] | Type[EnumFeature] | Type[CommandFeature] | Type[RawFeature]) → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get all features of a specific feature type.

Valid FeatureTypes are: IntFeature, FloatFeature, StringFeature, BoolFeature, EnumFeature, CommandFeature, RawFeature

Parameters:

feat_type – FeatureType used to find features of that type.

Returns:

A set of features of type feat_type`.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

get_features_selected_by(feat: IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature) → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get all features selected by a specific feature.

Parameters:

feat – Feature used to find features that are selected by feat.

Returns:

A set of features selected by feat.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

  • VmbFeatureError – If feat is not a valid feature.

load_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = <ModulePersistFlags.None_: 0>, max_iterations: int = 0)#

Load settings from XML file.

Parameters:
  • file_path – The location for loading current settings. The given file must be a file ending with “.xml”.

  • persist_type – Parameter specifying which setting types to load. For an overview of the possible values and their implication see the PersistType enum

  • persist_flags – Flags specifying the modules to load. By default only features of the calling module itself are persisted. For an overview of available flags see the ModulePersistFlags type

  • max_iterations – Number of iterations when storing settings. If 0 is given (default) the value found in the XML file is used

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside with context.

  • ValueError – If argument path is no “.xml” file.

save_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = <ModulePersistFlags.None_: 0>, max_iterations: int = 0)#

Save settings to XML File.

Parameters:
  • file_path – The location for storing the current settings. The given file must be a file ending with “.xml”.

  • persist_type – Parameter specifying which setting types to store. For an overview of the possible values and their implication see the PersistType enum

  • persist_flags – Flags specifying the modules to store. By default only features of the calling module itself are persisted. For an overview of available flags see the ModulePersistFlags type

  • max_iterations – Number of iterations when loading settings. If 0 is given (default) the VmbC default is used

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside with context.

  • ValueError – If argument path is no “.xml”- File.