Error#

class vmbpy.VmbCameraError#

Errors related to cameras

Error Type to indicate camera-related errors like:

  • Access of a disconnected Camera object

  • Lookup of non-existing cameras

class vmbpy.VmbChunkError#

Errors related to chunk data and chunk access

class vmbpy.VmbFeatureError#

Error related to Feature access

Error type to indicate invalid Feature access like:

  • Invalid access mode on Feature access.

  • Out of range values upon setting a value.

  • Failed lookup of features.

class vmbpy.VmbFrameError#

Error related to Frame data

class vmbpy.VmbInterfaceError#

Errors related to Interfaces

Error Type to indicated interface-related errors like:

  • Access on a disconnected Interface object

  • Lookup of a non-existing Interface

class vmbpy.VmbSystemError#

Errors related to the underlying Vimba X System

Error type to indicate system-wide errors like:

  • Incomplete Vimba X installation

  • Incompatible version of the underlying C-Layer

  • An unsupported OS

class vmbpy.VmbTimeout#

Indicates that an operation timed out

class vmbpy.VmbTransportLayerError#

Errors related to Transport Layers

Error type to indicate Transport Layer related errors like:

  • Lookup of a non-existing Transport Layer