Interface#

class vmbpy.Interface#

This class allows access to an interface such as USB detected by VmbC.

get_all_features() → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get access to all discovered features.

Returns:

A set of all currently detected Features.

Raises:

RuntimeError – If called outside of with context.

get_cameras() → CamerasTuple#

Get access to cameras associated with the Interface instance

Returns:

A tuple of all cameras associated with this Interface

Raises:

RuntimeError – If called outside of VmbSystem with context.

get_feature_by_name(feat_name: str) → IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature#

Get a feature by its name.

Parameters:

feat_name – Name used to find a feature.

Returns:

Feature with the associated name.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

  • VmbFeatureError – If no feature is associated with feat_name.

get_features_by_category(category: str) → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get all features of a specific category.

Parameters:

category – Category that should be used for filtering.

Returns:

A set of features of category category.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

get_features_by_type(feat_type: Type[IntFeature] | Type[FloatFeature] | Type[StringFeature] | Type[BoolFeature] | Type[EnumFeature] | Type[CommandFeature] | Type[RawFeature]) → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get all features of a specific feature type.

Valid FeatureTypes are: IntFeature, FloatFeature, StringFeature, BoolFeature, EnumFeature, CommandFeature, RawFeature

Parameters:

feat_type – FeatureType used to find features of that type.

Returns:

A set of features of type feat_type`.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

get_features_selected_by(feat: IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature) → Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]#

Get all features selected by a specific feature.

Parameters:

feat – Feature used to find features that are selected by feat.

Returns:

A set of features selected by feat.

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside of with context.

  • VmbFeatureError – If feat is not a valid feature.

get_id() → str#

Get Interface Id such as ‘VimbaUSBInterface_0x0’.

get_name() → str#

Get Interface Name such as ‘VimbaX USB Interface’.

get_transport_layer() → TransportLayer#

Get the Transport Layer associated with this instance of Interface

get_type() → TransportLayerType#

Get Interface Type such as TransportLayerType.GEV.

Note

This uses the TransportLayerType enum to report the connection type of the Interface as there is no dedicated interface type enum. The TransportLayerType covers all interface types.

load_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = <ModulePersistFlags.None_: 0>, max_iterations: int = 0)#

Load settings from XML file.

Parameters:
  • file_path – The location for loading current settings. The given file must be a file ending with “.xml”.

  • persist_type – Parameter specifying which setting types to load. For an overview of the possible values and their implication see the PersistType enum

  • persist_flags – Flags specifying the modules to load. By default only features of the calling module itself are persisted. For an overview of available flags see the ModulePersistFlags type

  • max_iterations – Number of iterations when storing settings. If 0 is given (default) the value found in the XML file is used

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside with context.

  • ValueError – If argument path is no “.xml” file.

read_memory(addr: int, max_bytes: int) → bytes#

Read a byte sequence from a given memory address.

Parameters:
  • addr – Starting address to read from.

  • max_bytes – Maximum number of bytes to read from addr.

Returns:

Read memory contents as bytes.

Raises:
  • TypeError – If parameters do not match their type hint.

  • ValueError – If addr is negative.

  • ValueError – If max_bytes is negative.

  • ValueError – If the memory access was invalid.

save_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = <ModulePersistFlags.None_: 0>, max_iterations: int = 0)#

Save settings to XML File.

Parameters:
  • file_path – The location for storing the current settings. The given file must be a file ending with “.xml”.

  • persist_type – Parameter specifying which setting types to store. For an overview of the possible values and their implication see the PersistType enum

  • persist_flags – Flags specifying the modules to store. By default only features of the calling module itself are persisted. For an overview of available flags see the ModulePersistFlags type

  • max_iterations – Number of iterations when loading settings. If 0 is given (default) the VmbC default is used

Raises:
  • TypeError – If parameters do not match their type hint.

  • RuntimeError – If called outside with context.

  • ValueError – If argument path is no “.xml”- File.

write_memory(addr: int, data: bytes)#

Write a byte sequence to a given memory address.

Parameters:
  • addr – Address to write the content of ‘data’ to.

  • data – Byte sequence to write at address ‘addr’.

Raises:
  • TypeError – If parameters do not match their type hint.

  • ValueError – If addr is negative.

class vmbpy.InterfaceEvent#

Enum specifying an Interface Event

Missing = 0#

A known interface disappeared from the bus

Detected = 1#

A new interface was discovered

Reachable = 2#

A known interface can be accessed

Unreachable = 3#

A known interface cannot be accessed anymore