Stream
- class vmbpy.Stream
This class provides access to a Stream of a Camera
- get_all_features() Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get access to all discovered features.
- Returns:
A set of all currently detected Features.
- Raises:
RuntimeError – If called outside of
withcontext.
- get_feature_by_name(feat_name: str) IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature
Get a feature by its name.
- Parameters:
feat_name – Name used to find a feature.
- Returns:
Feature with the associated name.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.VmbFeatureError – If no feature is associated with
feat_name.
- get_features_by_category(category: str) Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get all features of a specific category.
- Parameters:
category – Category that should be used for filtering.
- Returns:
A set of features of category
category.- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.
- get_features_by_type(feat_type: Type[IntFeature] | Type[FloatFeature] | Type[StringFeature] | Type[BoolFeature] | Type[EnumFeature] | Type[CommandFeature] | Type[RawFeature]) Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get all features of a specific feature type.
Valid FeatureTypes are:
IntFeature,FloatFeature,StringFeature,BoolFeature,EnumFeature,CommandFeature,RawFeature- Parameters:
feat_type – FeatureType used to find features of that type.
- Returns:
A set of features of type feat_type`.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.
- get_features_selected_by(feat: IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature) Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get all features selected by a specific feature.
- Parameters:
feat – Feature used to find features that are selected by
feat.- Returns:
A set of features selected by
feat.- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.VmbFeatureError – If
featis not a valid feature.
- get_frame(timeout_ms: int = 2000, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame) Frame
- get_frame_generator(limit: int | None = None, timeout_ms: int = 2000, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame)
- get_frame_with_context(timeout_ms: int = 2000, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame)
- is_streaming() bool
Returns
Trueif the camera is currently in streaming mode. If not, returnsFalse.
- load_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = ModulePersistFlags.None_, max_iterations: int = 0)
Load settings from XML file.
- Parameters:
file_path – The location for loading current settings. The given file must be a file ending with “.xml”.
persist_type – Parameter specifying which setting types to load. For an overview of the possible values and their implication see the
PersistTypeenumpersist_flags – Flags specifying the modules to load. By default only features of the calling module itself are persisted. For an overview of available flags see the
ModulePersistFlagstypemax_iterations – Number of iterations when storing settings. If 0 is given (default) the value found in the XML file is used
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If argument path is no “.xml” file.
- save_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = ModulePersistFlags.None_, max_iterations: int = 0)
Save settings to XML File.
- Parameters:
file_path – The location for storing the current settings. The given file must be a file ending with “.xml”.
persist_type – Parameter specifying which setting types to store. For an overview of the possible values and their implication see the
PersistTypeenumpersist_flags – Flags specifying the modules to store. By default only features of the calling module itself are persisted. For an overview of available flags see the
ModulePersistFlagstypemax_iterations – Number of iterations when loading settings. If
0is given (default) the VmbC default is used
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If argument path is no “.xml”- File.
- start_streaming(handler: FrameHandler, buffer_count: int = 5, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame)
- stop_streaming()