Frame
- class vmbpy.Frame
This class allows access to Frames acquired by a camera. The Frame is basically a buffer that wraps image data and some metadata.
- access_chunk_data(callback: Callable[[FeatureContainer], None]) None
Access chunk data for a frame.
This function blocks until the user supplied callback has been executed. It may only be called inside a frame callback.
- Parameters:
callback – A callback function that takes one argument. That argument will be a populated
FeatureContainerinstance. Only inside this callback is it possible to access the chunk features of theFrameinstance.- Raises:
Any Exception – Any Exception raised in the user supplied callback
VmbFrameError – If the frame does not contain any chunk data
VmbChunkError – If some other error occurred during chunk handling
- as_numpy_ndarray() numpy.ndarray
Construct
numpy.ndarrayview on VmbCFrame.- Returns:
numpy.ndarrayon internal image buffer.- Raises:
ImportError – If numpy is not installed.
VmbFrameError – If current PixelFormat can’t be converted to a
numpy.ndarray.
- as_opencv_image() numpy.ndarray
Construct OpenCV compatible view on VmbCFrame.
- Returns:
OpenCV compatible
numpy.ndarray- Raises:
ImportError – If numpy is not installed.
ValueError – If current pixel format is not compatible with opencv. Compatible formats are listed in
OPENCV_PIXEL_FORMATS.
- contains_chunk_data() bool | None
Does the frame contain chunk data?
- Returns:
Trueif frame contains chunk data,Falseif frame does not contain chunk data.Noneif this information is not provided by the underlying Transport Layer.
- convert_pixel_format(target_fmt: PixelFormat, debayer_mode: Debayer | None = None, destination_buffer: memoryview | None = None) Frame
Return a converted version of the frame in the given format.
This method always returns a new frame object and leaves the original instance unchanged. The returned frame object does not include the chunk data associated with the original instance. The original instance may for example be used for future frame transmissions.
Note: This method allocates a new buffer for the returned image data leading to some runtime overhead. For performance reasons, it might be better to set the value of the camera’s
PixelFormatfeature instead. In addition, a non-default debayer mode can be specified.- Parameters:
target_fmt – PixelFormat to convert to.
debayer_mode – Non-default algorithm used to debayer images in Bayer Formats. If no mode is specified, default debayering mode of the image transform library is applied. If the current format is not a Bayer format, this parameter is silently ignored.
destination_buffer – A buffer that the transformation result should be written to. The buffer must be large enough to hold the transformation result, writeable and be contiguous in memory. The recommended way to create a compatible buffer is to let
convert_pixel_formatperform a conversion without adestination_bufferand reuse the memory that was allocated for that transformation on future calls toconvert_pixel_format. See the convert_pixel_format.py example.
- Raises:
TypeError – If parameters do not match their type hint. ValueError if the current format can’t be converted into
target_fmt. Convertible Formats can be queried viaget_convertible_formats()ofPixelFormat.AssertionError – If image width or height can’t be determined.
BufferError – If user supplied
destination_bufferis too small, not writeable, or not contiguous in memory.
- deinterlace(pixel_pattern: Tuple[Tuple[int, ...], ...]) Tuple[Frame, ...]
Extracts multiple images from a single interlaced image.
This method takes a single image which contains interlaced image data for multiple exposures and separates the interlaced image data into separate images. Deinterlacing takes place on a 2x2 pattern basis.
- Parameters:
pixel_pattern – A 2x2 pattern explaining which output image the corresponding pixel should be included in. If multiple pixels are included in the same output image their value is averaged. The pattern should be passed as nested tuple such as
((0, 1), (2, 3)). The index values should start at 0 and count up with no gaps. The number of different indices determines how many output images are used.- Returns:
A tuple of
Frameobjects that hold the deinterlaced images.- Return type:
output_images
- Raises:
ValueError – If one of the following conditions is not met -
pixel_patternfollows required format as described in this docstring - input frame does not providewidthorheightinformation - input frame has an unsupportedPixelFormat
- get_buffer() Array
Get internal buffer object containing image data and (if existent) chunk data.
- get_buffer_size() int
Get byte size of internal buffer.
- get_height() int | None
Get image height in pixels.
- Returns:
Image height in pixels if dimension data is provided by the camera.
Noneif dimension data is not provided by the camera.
- get_id() int | None
Get Frame ID.
- Returns:
Frame ID if the id is provided by the camera.
Noneif frame id is not provided by the camera.
- get_offset_x() int | None
Get horizontal offset in pixels.
- Returns:
Horizontal offset in pixel if offset data is provided by the camera.
Noneif offset data is not provided by the camera.
- get_offset_y() int | None
Get vertical offset in pixels.
- Returns:
Vertical offset in pixels if offset data is provided by the camera.
Noneif offset data is not provided by the camera.
- get_payload_type() PayloadType | None
Returns the frame’s payload type.
- get_pixel_format() PixelFormat
Get format of the acquired image data
- get_status() FrameStatus
Returns current frame status.
- get_timestamp() int | None
Get Frame timestamp.
- Returns:
Timestamp if provided by the camera.
Noneif timestamp is not provided by the camera.
- get_width() int | None
Get image width in pixels.
- Returns:
Image width in pixels if dimension data is provided by the camera.
Noneif dimension data is not provided by the camera.
- class vmbpy.FrameStatus
Enum specifying the current status of internal Frame data.
- Complete = 0
Frame data is complete without errors
- Incomplete = -1
Frame could not be filled to the end
- TooSmall = -2
Frame buffer was too small
- Invalid = -3
Frame buffer was invalid
- class vmbpy.AllocationMode
Enum specifying the supported frame allocation modes.
- AnnounceFrame = 0
The buffer is allocated by vmbpy
- AllocAndAnnounceFrame = 1
The buffer is allocated by the Transport Layer
- class vmbpy.PixelFormat
Enum specifying all PixelFormats. Note: Not all Cameras support all Pixelformats.
- Mono8 = 17301505
Monochrome, 8 bits (PFNC Mono8)
- Mono10 = 17825795
Monochrome, 10 bits in 16 bits (PFNC Mono10)
- Mono10p = 17432646
Monochrome, 4x10 bits continuously packed in 40 bits (PFNC Mono10p)
- Mono12 = 17825797
Monochrome, 12 bits in 16 bits (PFNC Mono12)
- Mono12Packed = 17563654
Monochrome, 2x12 bits in 24 bits (GEV Mono12Packed)
- Mono12p = 17563719
Monochrome, 2x12 bits continuously packed in 24 bits (PFNC Mono12p)
- Mono14 = 17825829
Monochrome, 14 bits in 16 bits (PFNC Mono14)
- Mono16 = 17825799
Monochrome, 16 bits (PFNC Mono16)
- BayerGR8 = 17301512
Bayer-color, 8 bits, starting with GR line (PFNC BayerGR8)
- BayerRG8 = 17301513
Bayer-color, 8 bits, starting with RG line (PFNC BayerRG8)
- BayerGB8 = 17301514
Bayer-color, 8 bits, starting with GB line (PFNC BayerGB8)
- BayerBG8 = 17301515
Bayer-color, 8 bits, starting with BG line (PFNC BayerBG8)
- BayerGR10 = 17825804
Bayer-color, 10 bits in 16 bits, starting with GR line (PFNC BayerGR10)
- BayerRG10 = 17825805
Bayer-color, 10 bits in 16 bits, starting with RG line (PFNC BayerRG10)
- BayerGB10 = 17825806
Bayer-color, 10 bits in 16 bits, starting with GB line (PFNC BayerGB10)
- BayerBG10 = 17825807
Bayer-color, 10 bits in 16 bits, starting with BG line (PFNC BayerBG10)
- BayerGR12 = 17825808
Bayer-color, 12 bits in 16 bits, starting with GR line (PFNC BayerGR12)
- BayerRG12 = 17825809
Bayer-color, 12 bits in 16 bits, starting with RG line (PFNC BayerRG12)
- BayerGB12 = 17825810
Bayer-color, 12 bits in 16 bits, starting with GB line (PFNC BayerGB12)
- BayerBG12 = 17825811
Bayer-color, 12 bits in 16 bits, starting with BG line (PFNC BayerBG12)
- BayerGR12Packed = 17563690
Bayer-color, 2x12 bits in 24 bits, starting with GR line (GEV BayerGR12Packed)
- BayerRG12Packed = 17563691
Bayer-color, 2x12 bits in 24 bits, starting with RG line (GEV BayerRG12Packed)
- BayerGB12Packed = 17563692
Bayer-color, 2x12 bits in 24 bits, starting with GB line (GEV BayerGB12Packed)
- BayerBG12Packed = 17563693
Bayer-color, 2x12 bits in 24 bits, starting with BG line (GEV BayerBG12Packed)
- BayerGR10p = 17432662
Bayer-color, 4x10 bits continuously packed in 40 bits, starting with GR line (PFNC BayerGR10p)
- BayerRG10p = 17432664
Bayer-color, 4x10 bits continuously packed in 40 bits, starting with RG line (PFNC BayerRG10p)
- BayerGB10p = 17432660
Bayer-color, 4x10 bits continuously packed in 40 bits, starting with GB line (PFNC BayerGB10p)
- BayerBG10p = 17432658
Bayer-color, 4x10 bits continuously packed in 40 bits, starting with BG line (PFNC BayerBG10p)
- BayerGR12p = 17563735
Bayer-color, 2x12 bits continuously packed in 24 bits, starting with GR line (PFNC BayerGR12p)
- BayerRG12p = 17563737
Bayer-color, 2x12 bits continuously packed in 24 bits, starting with RG line (PFNC BayerRG12p)
- BayerGB12p = 17563733
Bayer-color, 2x12 bits continuously packed in 24 bits, starting with GB line (PFNC BayerGB12p)
- BayerBG12p = 17563731
Bayer-color, 2x12 bits continuously packed in 24 bits, starting with BG line (PFNC BayerBG12p)
- BayerGR16 = 17825838
Bayer-color, 16 bits, starting with GR line (PFNC BayerGR16)
- BayerRG16 = 17825839
Bayer-color, 16 bits, starting with RG line (PFNC BayerRG16)
- BayerGB16 = 17825840
Bayer-color, 16 bits, starting with GB line (PFNC BayerGB16)
- BayerBG16 = 17825841
Bayer-color, 16 bits, starting with BG line (PFNC BayerBG16)
- Rgb8 = 35127316
RGB, 8 bits x 3 (PFNC RGB8)
- Bgr8 = 35127317
BGR, 8 bits x 3 (PFNC Bgr8)
- Rgb10 = 36700184
RGB, 10 bits in 16 bits x 3 (PFNC RGB10)
- Bgr10 = 36700185
BGR, 10 bits in 16 bits x 3 (PFNC BGR10)
- Rgb12 = 36700186
RGB, 12 bits in 16 bits x 3 (PFNC RGB12)
- Bgr12 = 36700187
BGR, 12 bits in 16 bits x 3 (PFNC BGR12)
- Rgb14 = 36700254
RGB, 14 bits in 16 bits x 3 (PFNC RGB14)
- Bgr14 = 36700234
BGR, 14 bits in 16 bits x 3 (PFNC BGR14)
- Rgb16 = 36700211
RGB, 16 bits x 3 (PFNC RGB16)
- Bgr16 = 36700235
BGR, 16 bits x 3 (PFNC BGR16)
- Rgba8 = 35651606
ARGB, 8 bits x 4 (PFNC RGBa8)
- Bgra8 = 35651607
RGBA, 8 bits x 4, legacy name
- Argb8 = 35651606
BGRA, 8 bits x 4 (PFNC BGRa8)
- Rgba10 = 37748831
RGBA, 10 bits in 16 bits x 4
- Bgra10 = 37748812
BGRA, 10 bits in 16 bits x 4
- Rgba12 = 37748833
RGBA, 12 bits in 16 bits x 4
- Bgra12 = 37748814
BGRA, 12 bits in 16 bits x 4
- Rgba14 = 37748835
RGBA, 14 bits in 16 bits x 4
- Bgra14 = 37748816
BGRA, 14 bits in 16 bits x 4
- Rgba16 = 37748836
RGBA, 16 bits x 4
- Bgra16 = 37748817
BGRA, 16 bits x 4
- Yuv411 = 34340894
YUV 411 with 8 bits (GEV YUV411Packed)
- Yuv422 = 34603039
YUV 422 with 8 bits (GEV YUV422Packed)
- Yuv444 = 35127328
YUV 444 with 8 bits (GEV YUV444Packed)
- YCbCr411_8_CbYYCrYY = 34340924
YCbCr 411 with 8 bits (PFNC YCbCr411_8_CbYYCrYY) - identical to Yuv411
- YCbCr422_8_CbYCrY = 34603075
YCbCr 422 with 8 bits (PFNC YCbCr422_8_CbYCrY) - identical to Yuv422
- YCbCr8_CbYCr = 35127354
YCbCr 444 with 8 bits (PFNC YCbCr8_CbYCr) - identical to Yuv444
- vmbpy.intersect_pixel_formats(fmts1: Tuple[PixelFormat, ...], fmts2: Tuple[PixelFormat, ...]) Tuple[PixelFormat, ...]
Build intersection of two sets containing PixelFormat.
- Parameters:
fmts1 – PixelFormats to intersect with fmts2
fmts2 – PixelFormats to intersect with fmts1
- Returns:
Set of PixelFormats that occur in
fmts1andfmts2- Raises:
TypeError – If parameters do not match their type hint.