Camera
- class vmbpy.Camera
This class provides access to a Camera. It corresponds to the GenTL Remote Device.
Camera is intended be used in conjunction with the
withcontext. On entering the context, all Camera features are detected and can be accessed within the context. Static Camera properties like Name and Model can be accessed outside the context.- get_access_mode() AccessMode
Get current camera access mode
- get_all_features() Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get access to all discovered features.
- Returns:
A set of all currently detected Features.
- Raises:
RuntimeError – If called outside of
withcontext.
- get_extended_id() str
Get the extended (globally unique) ID of a Camera.
- get_feature_by_name(feat_name: str) IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature
Get a feature by its name.
- Parameters:
feat_name – Name used to find a feature.
- Returns:
Feature with the associated name.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.VmbFeatureError – If no feature is associated with
feat_name.
- get_features_by_category(category: str) Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get all features of a specific category.
- Parameters:
category – Category that should be used for filtering.
- Returns:
A set of features of category
category.- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.
- get_features_by_type(feat_type: Type[IntFeature] | Type[FloatFeature] | Type[StringFeature] | Type[BoolFeature] | Type[EnumFeature] | Type[CommandFeature] | Type[RawFeature]) Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get all features of a specific feature type.
Valid FeatureTypes are:
IntFeature,FloatFeature,StringFeature,BoolFeature,EnumFeature,CommandFeature,RawFeature- Parameters:
feat_type – FeatureType used to find features of that type.
- Returns:
A set of features of type feat_type`.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.
- get_features_selected_by(feat: IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature) Tuple[IntFeature | FloatFeature | StringFeature | BoolFeature | EnumFeature | CommandFeature | RawFeature, ...]
Get all features selected by a specific feature.
- Parameters:
feat – Feature used to find features that are selected by
feat.- Returns:
A set of features selected by
feat.- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside of
withcontext.VmbFeatureError – If
featis not a valid feature.
- get_frame(timeout_ms: int = 2000, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame) Frame
Get copy of a single frame from camera. Synchronous frame acquisition.
Records a single frame from the camera, creates a copy of the frame and returns it to the caller. This frame may be used by users as long as they want but can not be used e.g. to access chunk data associated with it. See also
get_frame_with_contextto avoid the frame copy.- Parameters:
timeout_ms – Timeout in milliseconds of frame acquisition.
allocation_mode – Allocation mode deciding if buffer allocation should be done by vmbpy or the Transport Layer
- Returns:
Frame from camera
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If a timeout_ms is negative.
VmbTimeout – If Frame acquisition timed out.
- get_frame_generator(limit: int | None = None, timeout_ms: int = 2000, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame)
Construct frame generator, providing synchronous image acquisition.
The frame generator acquires a new frame with each execution. Frames may only be used inside their respective loop iteration. If a frame must be used outside the loop iteration, a copy of the frame must be created (e.g. via
copy.deepcopy(frame)).- Parameters:
limit – The number of images the generator shall acquire (>0). If limit is None, the generator will produce an unlimited amount of images and must be stopped by the user supplied code.
timeout_ms – Timeout in milliseconds of frame acquisition.
allocation_mode – Allocation mode deciding if buffer allocation should be done by vmbpy or the Transport Layer
- Returns:
Frame generator expression
- Raises:
RuntimeError – If called outside
withcontext.ValueError – If a limit is supplied and
<= 0.ValueError – If a
timeout_msis negative.VmbTimeout – If Frame acquisition timed out.
VmbCameraError – If Camera is streaming while executing the generator.
- get_frame_with_context(timeout_ms: int = 2000, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame)
Gets a single frame from camera to be used inside a context manager.
Records a single frame from the camera and yields it to the caller for use inside a with context manager. The frame may only be used inside the context, but may be copied for use outside of it (e.g. via
copy.deepcopy(frame)). The yielded frame can be used to access chunk data.- Parameters:
timeout_ms – Timeout in milliseconds of frame acquisition.
allocation_mode – Allocation mode deciding if buffer allocation should be done by vmbpy or the Transport Layer
- Yields:
Frame from camera for use in
withcontext manager- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If a
timeout_msis negative.VmbTimeout – If Frame acquisition timed out.
- get_id() str
Get Camera Id. For example ‘DEV_1AB22C00041B’
- get_interface_id() str
Get ID of the Interface this camera is connected to. For example ‘VimbaUSBInterface_0x0’
- get_local_device() LocalDevice
Returns the instance of
LocalDeviceassociated with this Camera.
- get_model() str
Get Camera Model. For example ‘1800 U-500m’
- get_name() str
Get Camera Name. For example ‘Allied Vision 1800 U-500m’
- get_permitted_access_modes() Tuple[AccessMode, ...]
Get a set of all access modes the camera can be accessed with.
- get_pixel_format()
Get current pixel format.
- Returns:
Current pixel format set on the camera.
- Raises:
RuntimeError – If called outside
withcontext.
- get_pixel_formats() Tuple[PixelFormat, ...]
Get supported pixel formats from Camera.
- Returns:
All pixel formats the camera supports
- Raises:
RuntimeError – If called outside
withcontext.
- get_serial() str
Get Camera serial number. For example ‘50-0503328442’
- get_streams() Tuple[Stream, ...]
Returns a Tuple containing all instances of
Streamassociated with this Camera.
- get_transport_layer() TransportLayer
Get the
TransportLayerinstance for this Camera.
- is_streaming() bool
Returns
Trueif the camera is currently in streaming mode. If not, returnsFalse.
- load_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = ModulePersistFlags.None_, max_iterations: int = 0)
Load settings from XML file.
- Parameters:
file_path – The location for loading current settings. The given file must be a file ending with “.xml”.
persist_type – Parameter specifying which setting types to load. For an overview of the possible values and their implication see the
PersistTypeenumpersist_flags – Flags specifying the modules to load. By default only features of the calling module itself are persisted. For an overview of available flags see the
ModulePersistFlagstypemax_iterations – Number of iterations when storing settings. If 0 is given (default) the value found in the XML file is used
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If argument path is no “.xml” file.
- queue_frame(frame: Frame)
Reuse acquired frame in streaming mode.
Add given frame back into the frame queue used in streaming mode. This should be the last operation on a registered
FrameHandler. If streaming mode is not active, it returns silently.- Parameters:
frame – The frame to reuse.
- Raises:
TypeError – If parameters do not match their type hint.
ValueError – If the given frame is not from the internal buffer queue.
RuntimeError – If called outside
withcontext.VmbCameraError – If reusing the frame was unsuccessful.
- read_memory(addr: int, max_bytes: int) bytes
Read a byte sequence from a given memory address.
- Parameters:
addr – Starting address to read from.
max_bytes – Maximum number of bytes to read from addr.
- Returns:
Read memory contents as bytes.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If
addris negative.ValueError – If
max_bytesis negative.ValueError – If the memory access was invalid.
- save_settings(file_path: str, persist_type: PersistType = PersistType.Streamable, persist_flags: ModulePersistFlags = ModulePersistFlags.None_, max_iterations: int = 0)
Save settings to XML File.
- Parameters:
file_path – The location for storing the current settings. The given file must be a file ending with “.xml”.
persist_type – Parameter specifying which setting types to store. For an overview of the possible values and their implication see the
PersistTypeenumpersist_flags – Flags specifying the modules to store. By default only features of the calling module itself are persisted. For an overview of available flags see the
ModulePersistFlagstypemax_iterations – Number of iterations when loading settings. If
0is given (default) the VmbC default is used
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If argument path is no “.xml”- File.
- set_access_mode(access_mode: AccessMode)
Set camera access mode.
Must be set before the camera connection is opened.
- Parameters:
access_mode – AccessMode for accessing a Camera.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called inside
withcontext.
- set_pixel_format(fmt: PixelFormat)
Set current pixel format.
- Parameters:
fmt – Pixel format to set on the camera.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If the given pixel format is not supported by the cameras.
- start_streaming(handler: Callable[[Camera, Stream, Frame], None], buffer_count: int = 5, allocation_mode: AllocationMode = AllocationMode.AnnounceFrame)
Enter streaming mode.
Enter streaming mode is also known as asynchronous frame acquisition. While active, the camera acquires and buffers frames continuously. With each acquired frame, a given FrameHandler is called with a new Frame.
- Parameters:
handler – Callable that is executed on each acquired frame.
buffer_count – Number of frames supplied as internal buffer.
allocation_mode – Allocation mode deciding if buffer allocation should be done by vmbpy or the Transport Layer
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If buffer is less or equal to zero.
VmbCameraError – If the camera is already streaming.
VmbCameraError – If anything went wrong on entering streaming mode.
- stop_streaming()
Leave streaming mode.
Leave asynchronous frame acquisition. If streaming mode was not activated before, it just returns silently.
- Raises:
RuntimeError – If called outside
withcontext.VmbCameraError – If anything went wrong on leaving streaming mode.
- write_memory(addr: int, data: bytes)
Write a byte sequence to a given memory address.
- Parameters:
addr – Address to write the content of ‘data’ too.
data – Byte sequence to write at address ‘addr’.
- Raises:
TypeError – If parameters do not match their type hint.
RuntimeError – If called outside
withcontext.ValueError – If
addris negative.
- class vmbpy.AccessMode
Enum specifying all available camera access modes.
- None_ = 0
No access.
- Full = 1
Read and write access.
- Read = 2
Read-only access. Setting features is not possible.
- Unknown = 4
Access type unknown.
- Exclusive = 8
Read and write access without permitting access for other consumers.