Vimba USB TL Release Notes¶
Version: 1.4.1
Components and Version Reference¶
Component |
Version |
|---|---|
USB Transport Layer (VimbaUSBTL.cti) |
1.4.1 |
Vimba USB Driver (Windows only) |
1.0.0 |
Vimba Driver Installer (VimbaDriverInstaller.exe) |
1.1.9 |
Hardware Requirements¶
PC or laptop with 1 GHz x86 processor or better.
ARMv8-compatible 64-bit embedded system, for example, Jetson Xavier.
Additionally, a built-in USB 3.0 controller for PCI Express bus is required.
Remark: Testing has been performed on host controllers that are based on Intel chip sets and Renesas chip sets. The driver may run on host controllers that are based on chip sets from other vendors, too. Nevertheless for best performance we highly recommend Intel chip sets. However, if there are any problems please feel free to contact our Technical Support.
Installation¶
The Vimba USB Transport Layer is part of the Vimba SDK. For instructions on how to install this module, please refer to the Vimba User Manual.
Correlations with other Allied Vision Software Packages¶
Please refer to the Vimba SDK Release Notes.
Known issues¶
MSI Uninstallation by new Windows 10 dialog “Apps&Features” is not supported by now. Please use the old “Programs and Features” dialog.
Changes and release history¶
Changes in version 1.4.1¶
Fixed: software trigger for multiple cameras (error applied to Windows only)
Changes in version 1.4.0¶
Fixed: Reset cameras streaming state when opened (Endpoint Halt)
New: Zero-Copy for Linux/libusb for better performance
Updated 3rd-party libraries
Changes in version 1.3.0¶
Increased default MaxTransferSize value for better performance with current Linux versions
Improved camera detection on Linux systems (plugin event handling)
Changes in version 1.2.2¶
Solved conflicts between customers’ boost version and the internally used version
Other internal bug fixes
Changes in version 1.2.1¶
Improved visibility of USB camera status
Other bug fixes
Vimba Driver Installer
Internal changes
Changes in version 1.2.0¶
GenTL 1.5 support
Changes in version 1.1.1¶
USB Transport Layer
Minor bug fixes
Installer and driver
New certificates for installer and driver (Windows 7, Windows 8, and Windows 8.1)
Changes in version 1.1.0¶
USB Transport Layer
Minor bug fixes
Added transport layer XML file caching
Changes in version 1.0.3¶
USB Transport Layer
Minor bug fixes
Interface features DeviceDriverPath and DeviceLocation added