Vimba GigE TL Release Notes¶
Version: 1.9.0
Components and Version Reference¶
Component |
Version |
|---|---|
GigE Transport Layer (VimbaGigETL.cti) |
1.9.0 |
Hardware Requirements¶
PC or laptop with 1 GHz x86 processor or better.
ARMv8-compatible 64-bit embedded system, for example, Jetson Xavier.
When using Allied Vision GigE cameras, a built-in Gigabit Ethernet network interface or Gigabit Ethernet network card (one or more) is required.
Installation¶
The Vimba GigE Transport Layer is part of the Vimba SDK. For instructions on how to install this module, please refer to the Vimba User Manual.
Known Issues¶
When experiencing trouble with image acquisition on Linux, try to increase the priority of your application with “sudo -E nice -n -20
”. A change of the available camera access modes cannot be reported for cameras in different subnets or with misconfigured IP addresses. These cameras can be accessed in configuration mode from different hosts simultaneously.
MSI Uninstallation by new Windows 10 dialog “Apps&Features” is not supported by now. Please use the old “Programs and Features” dialog.
GigE Filter Driver:
Disabling the Vimba GigE Filter Driver while it is in use might lead to unexpected behavior up to blue screen.
Using other filter drivers additionally to Vimba’s GigE Filter Driver may cause issues.
Changes and release history¶
Changes in version 1.9.0¶
GigETL
Changed behaviour of endianess handling (values must match host endianness in little-endian), for better compatibility with third-party software. Affected features that now have a changed byte order:
Config Mode
IP-related features including MulticastIPAddress
Action Commands
New feature DeviceUpdateTimeout (only applicable of GigE discovery is switched to Broadcast)
New GVSPMaxLookBack default value (0 instead of 1) for improved packet resend handling
Fixed: High memory usage during performance bottleneck (Nonpaged pool growing with multiple GigE cameras)
Fixed: Action commands caused an error message in the console log
Fixed: MulticastIPAdress range, better compatibility with third-party software
GigE Filter Driver
Reduced memory allocations
Hidden statistics
Changes in version 1.8.2¶
GigETL and GigE Filter Driver
Fixed: Vimba Viewer did not show single frame acquisitions (5 GigE)
Improved timeout handling (5 GigE)
Fixed limitations of certain GVSPPacketSize values
New GigETL feature: GVSPHostReceiveBufferSize (SO_RCVBUF, usable with the socket driver only) replaces GVSPHostReceiveBuffers (which is still usable in existing applications).
Changes in version 1.8.1¶
Prepared for use with 5 GigE Vision cameras
Changes in version 1.8.0¶
Standard-compliant ForceIP features instead of Allied Vision custom features
Prepared for use with extended IDs
Changes in version 1.7.1¶
Improved resend handling
By default, packet resends are enabled
Other bug fixes
Vimba Driver Installer
Internal changes
Changes in version 1.7.0¶
GenTL 1.5 support
Changes in version 1.6.0¶
Fixed: GVSPPacketSize now updates as expected (Linux)
Other minor bug fixes
Vimba GigE Filter Driver
Windows 10: Improved compatibility and performance with third-party filter drivers.
Installer and driver
New certificates for installer and driver (Windows 7, Windows 8, and Windows 8.1)
Changes in version 1.5.0¶
Added functionality for Action Commands
Fixed sending packet request after invalid timeout on Linux
The parameter BUFFER_INFO_DELIVERED_IMAGEHEIGHT is filled correctly
VimbaGigEFilter (Windows 10 x64/x86 only):
Fixed incompatibility with Intel 10 Gbit Ethernet cards (520/540/710)
Changed buffer list handling, driver removes streaming packets from buffer list:
Decreases system load formerly caused by stream packet duplication
Prevents additional system load when firewall is enabled
Does not allow Wireshark to see stream packets
Packet resend system load minimized
Fixed missing filterclass in driver inf
Fixed double counting of received packets
Fixed incompatibility with wireless network cards (removed binding to WAN)
Fixed incompatibilities with VPN connections (filter now optional)
Changes in version 1.4.4¶
-Bug fixes
Changes in version 1.4.2¶
Bug fixes
Changes in version 1.4.1¶
Solved cases where network problems led to a lost camera
Fixed range of GevHeartbeatInterval and GevHeartbeatTimeout
Bug fixes for multi-camera usage and missing cleanup
Changes in version 1.3.1¶
Support of GenICam GenTL standard 1.3
New GenTL SFNC feature categories BufferHandlingMode and StreamInformation
Separate features for heartbeat timeout and heartbeat interval
Adjustable device discovery waiting time
Fixed issues with alike serial numbers
Fixed issues with many network interfaces on Linux
Small bug-fixes to the Driver Installer
Changes in version 1.2.0¶
Improved performance in case of many events
Restriction to eight cameras removed
Corrected Heartbeat feature
Fixed support for small packets
Changes in version 1.1.0¶
Added feature DiscoveryBroadcastMode to the Interface module
Changed the documentation format to PDF
Slight changes for Linux compatibility
Correlations with other Allied Vision Software Packages¶
Please refer to the Vimba SDK Release Notes.