Vimba for ARM64 Release Notes¶
Version: 6.1
Summary¶
Vimba 6.1 is a release version for ARM64 only. This release contains mainly changes of the CSI TL and support of JetPack 4.6.1.
Components and version reference¶
Transport Layer |
Version |
|---|---|
CSI Transport Layer (VimbaCSITL.cti) |
1.1.0* |
GigE Transport Layer (VimbaGigETL.cti) |
1.9.0 |
USB Transport Layer (VimbaUSBTL.cti) |
1.4.1 |
APIs |
Version |
|---|---|
Vimba C API (libVimbaC.so) |
1.9.2* |
Vimba C++ API (libVimbaCPP.so) |
1.9.0 |
Vimba Python API |
1.3.0* |
Image Transform Library (libVimbaImageTransform.so) |
1.6.0 |
Tools |
Version |
|---|---|
Vimba Viewer (VimbaViewer) |
2.5.1* |
Vimba Class Generator (VimbaClassGenerator) |
1.0.6 |
Vimba Firmware Updater (VimbaFirmwareUpdater.exe) |
1.2.1* |
Vimba Firmware Updater Console (FWUpdaterConsole.exe) |
1.2.1* |
Third Party Libraries |
Version |
|---|---|
TinyXML (not shipped with Vimba) |
2.6.2 |
Qt |
4.8.5 |
Qwt |
6.1.3 |
libTIFF |
4.0.7 |
OpenCV |
3.0.0 |
* Changed in this release of Vimba
Hardware requirements¶
ARM board with ARMv8-compatible 64-bit processor
Allied Vision GigE cameras require a built-in Gigabit Ethernet network interface or at least one Gigabit Ethernet network card.
Note for IP configuration: By default, IP Configuration Mode is set to DHCP. You can also select LLA (link-local address) if you connect just one camera. If multiple cameras are connected at the same time, we recommend using DHCP or Persistent IP Address to enable discovery of all cameras.
Allied Vision USB cameras require a built-in USB 3.0 controller for PCI Express bus.
Tested platforms and cameras¶
GigE and USB cameras¶
Vimba was tested on NVIDIA Xavier AGX with JetPack 4.6.1 (L4T 32.7.1).
Alvium MIPI cameras¶
The following NVIDIA Jetson developer kit platforms with JetPack 4.6.1 (L4T 32.7.1) support the Alvium MIPI driver and the Vimba CSI TL:
AGX Xavier
Xavier NX
TX2 NX
Nano 4GB
Nano 2GB
For supported camera models, the latest known issues, and other useful information, see: Getting Started with GenICam for CSI-2
Installation¶
To install Vimba, see: Vimba installation under Linux
Short instruction:
Uncompress the archive with the command tar -xf ./Vimba.tgz to a directory you have writing privileges for like /opt. Under this directory Vimba will be installed in its own folder. In the following, we will refer to this path as [InstallDir].
Go to [InstallDir]/VimbaGigETL and/or [InstallDir]/VimbaUSBTL and execute the shell script Install.sh with super user privileges (e.g., sudo ./Install.sh). This registers the GENICAM_GENTL32_PATH and/or the GENICAM_GENTL64_PATH environment variable through a startup script in /etc/profile.d so that every GenICam GenTL consumer (such as the examples that ship with Allied Vision Vimba) can access the Allied Vision Gigabit Ethernet and USB Transport Layers. Please note that this is a per-user setting. If transport layers are not found, follow the instructions in this document: Vimba installation under Linux
Reboot computer
Vimba Viewer: Vimba Viewer can be found in, for example, [InstallDir]/Tools/Viewer/Bin/x86_64bit/. This program allows you to configure your Allied Vision cameras and capture images.
Ubuntu 18.04 LTS:
To build Vimba Viewer, install the libcanberra-gtk-module: apt-get install libcanberra-gtk-module
Vimba includes many precompiled examples that can be found in Vimba/VimbaC/Examples/Bin and Vimba/VimbaCPP/Examples/Bin. If you want to compile these examples yourself, please refer to the user manual for instructions and required packages.
For uninstalling Vimba, remove the startup scripts by running the shell scripts Uninstall.sh as super user. This prevents any GenTL consumer from loading the Vimba and USB Transport Layers. Then simply remove the installation directory.
Known issues¶
When experiencing trouble with image acquisition, try to increase the priority of your application with “sudo -E nice -n -20
”.
GigE Transport Layer:
A change of the available camera access modes cannot be reported for cameras in different subnets or with malconfigured IP addresses. These cameras can be accessed in configuration mode from different hosts simultaneously.
Not all ARM boards come with a GigE network interface. When acquiring images with only 100 Mbit/s, make sure to set the “StreamBytesPerSecond” feature to a reasonable small value (12 400 000). This adjustment is done automatically when the camera is connected directly to a 100 Mbit/s interface.
Tranport layers not found (Error -16):
Please follow the instructions in Vimba Installation under Linux:
Vimba Firmware Updater and FWUpdaterConsole.exe: Mako-U cameras are not detected after updating the firmware. To detect the camera, please reboot the board.
Camera detection:
If multiple IP addresses are configured on one physical Ethernet adapter, then Vimba sends GVCP discovery requests only to the last added IP address. Therefore, the camera is detected only if its IP address was added last.
Vimba Viewer:
If a GigE camera was opened and then closed with Vimba Viewer, it is displayed as locked and Vimba Viewer does not open it again. Workaround: Close and open Vimba Viewer.
When multiple opened GigE cameras are disconnected at the same time while no other camera stays connected to the very same NIC, the Vimba Viewer’s camera windows stay open.
qt error: please install libpng12 if it is missing.
After streaming several hours, the displayed image is not updated. Changing camera settings results in a black image. Stopping and starting image acquisition updates the displayed image. The issue affects only the displayed image, not the image itself.
Vimba code examples
qt error: please install libpng12 if it is missing.
Vimba APIs:
When API startup and shutdown is performed excessively within the same process, camera initialization may fail sporadically, which may cause exceptions. We recommend to have only one API session during one process.
CSI-2:
For the latest known issues, see Getting Started with GenICam for CSI-2
If your application causes dropped frames, try to increase the number of frame buffers to approximately 7.
Switching the camera from GenICam for CSI-2 to V4L2 or vice versa requires rebooting the board.
Exposure times greater than approx. 1 second: Stopping acquisition may cause an error. Please close and open the camera to start streaming again.
Changes and release history¶
Changes in Vimba 6.1.0¶
VimbaPython
Fixed: Missing frames from some cameras, especially with short exposure times.
VimbaC
Fixed: IP configuration
CSITL (supported camera models and ARM boards and known issues: see above)
Supports new streaming format (better performance in Announce mode), latest camera firmware required
Vimba Viewer
Improved performance with MIPI cameras
Firmware Updater
Main window now displays more information about an occured error
Firmware Updater Console
Fixed: ShowFailureMessage in case exception is raised
Changes in Vimba 6.0.0¶
VimbaC
Fixed: Issue with null terminator for zipped XML files
CSITL
First release (supported camera models and ARM boards and known issues: see above)
USBTL
Bug fix (relevant for Windows only)
VimbaPython:
Less restrictive C API version check
Changes in Vimba 5.1.0¶
VimbaC
New feature: Support for Alloc And Announce frame allocation mode
Feature endianess related fixes (corresponding to GigE TL)
VimbaCPP
New feature: Supports Alloc And Announce frame allocation mode
VimbaPython
New feature: Supports Alloc And Announce frame allocation mode
Vimba Viewer
Supports Alloc And Announce frame allocation mode
Chinese localization
Supports changes of GigE TL and VimbaC
Fixed: IP labels not updated after changing the IP via GevCameraForceAddressSend
Fixed: Auto ROI tab always resets ROI at startup
Firmware Updater
Supports Git hash representation
Firmware Updater Console
Supports Git hash representation
GigETL
Changed behaviour of endianess handling (values must match host endianness in little-endian), for better compatibility with third-party software. Affected features that now have a changed byte order:
Config Mode
IP-related features including MulticastIPAddress
Action Commands
New feature DeviceUpdateTimeout (only applicable if GigE discovery is switched to Broadcast)
New GVSPMaxLookBack default value (0 instead of 1) for improved packet resend handling
Fixed: High memory usage during performance bottleneck (Nonpaged pool growing with multiple GigE cameras)
Fixed: Action commands caused an error message in the console log
Fixed: Multicast IP address range, better compatibility with third-party software
USB TL
Updated 3rd-party libraries
Changes in Vimba 5.0.0¶
GigETL
New feature: GVSPHostReceiveBufferSize (SO_RCVBUF) replaces GVSPHostReceiveBuffers (which is still usable in existing applications).
Fixed for 5 GigE cameras:
Fixed limitations of certain GVSPPacketSize values
VimbaC
Fixed: Callbacks after stopping image acquisition caused exceptions in the Python API.
Fixed: ListAncillaryDataFeatures example (error “Could not queue frame”)
Vimba Firmware Updater
Prepared for CSI-2 support
Vimba Firmware Updater Console
Prepared for CSI-2 support
Vimba Viewer
Prepared for CSI-2 support
Changes in Vimba 4.3.0¶
GigETL
Prepared for use with 5 GigE Vision cameras
VimbaC
Prepared for use with 5 GigE Vision cameras
VimbaCPP
Preparations for use with 5 GigE Vision cameras in the underlying VimbaC API
Vimba Python
Updated for use with new VimbaC version
Fixed: read_memory now returns all 0_bytes
Vimba Firmware Updater
Preparations for use with 5 GigE Vision cameras
Vimba Firmware Updater Console
Preparations for use with 5 GigE Vision cameras
Vimba Viewer
Preparations for use with 5 GigE Vision cameras
Changes in Vimba 4.2.0¶
Vimba C
Standard-compliant ForceIP features instead of Allied Vision custom features, Updated VimbaC ForceIP example to use the standard-compliant ForceIP features
Vimba Python
Redirected the used Vimba version to the one delivered in this package.
Install.sh suggests compatible Python interpreter versions only
Install.sh and Uninstall.sh: Added support of virtual environments, Added debug flag
GigETL
Standard-compliant ForceIP features instead of Allied Vision custom features (see also Vimba C)
Prepared for use with extended IDs
USBTL
Increased default MaxTransferSize value for better performance with current Linux versions
Improved camera detection on Linux systems (plugin event handling)
Vimba Viewer
Added a dialog for enforcing IP settings to a GigE Vision camera
Changes in Vimba 4.1.0¶
USBTL
Solved conflicts between customers’ boost version and the internally used version
Other internal bug fixes
Changes in Vimba 4.0.0¶
Vimba C
Bug fixes
Vimba C++
Bug fixes
Vimba Python
New API
GigETL
Improved resend handling
By default, packet resends are enabled
Other bug fixes
USBTL
Improved visibility of USB camera status
Other bug fixes
Vimba GigE Filter Driver
Bug fixes
Vimba Viewer
Bug fixes
Changes in Vimba 3.1.0¶
Vimba C
Updated for use with GenTL 1.5
Vimba C++
Updated for use with GenTL 1.5
GigETL
GenTL 1.5 support
USBTL
GenTL 1.5 support
Vimba Viewer
Bug fixes
Changes in Vimba 3.0.0¶
Vimba C
Bug fixes
Vimba C++
Bug fixes
Vimba Viewer
Supports Alvium USB cameras
Fixed handling of float increments
Fixed occasional crashes with high frame rates
Several minor bug fixes
GigETL
Fixed: GVSPPacketSize now updates as expected
USBTL
Bug fixes
Changes in Vimba 2.1.3¶
Vimba C
Added ActionCommands programming example
Vimba C Manual: Updated documentation of Action Commands
Prepared the API for use with GenTL 1.5
Bug fixes
Vimba C++
Added ActionCommands programming example
Vimba CPP Manual: Updated documentation of Action Commands
Prepared the underlying C API for use with GenTL 1.5
Vimba CPP Manual: Added chapter Asynchronous image acquisition - overview
Bug fixes
Vimba Viewer
New plugin architecture
Vima Setup
Removed Vimba Class Generator desktop symbol
Vimba Manual
Integrated Vimba Features Manual
Changes in Vimba 2.1.0¶
Vimba C
Added functionality for Action Commands.
Bug fixes
Vimba C++
Added functionality for Action Commands.
Bug fixes
Vimba Image Transform Library
Support for conversion from 10-bit raw source formats to 16-bit color target formats.
Support for conversion from 12-bit raw source formats to 16-bit color target formats.
Support for conversion from 14-bit raw source formats to 16-bit color target formats.
Support for conversion from 10-bit mono source formats to 16-bit mono target formats.
Support for conversion from 12-bit mono source formats to 16-bit mono target formats.
Support for conversion from 14-bit mono source formats to 16-bit mono target formats.
Vimba Viewer
Allows now saving of 12-bit and 16-bit images (12-bit images are saved in 16-bit containers).
Added functionality for Action Commands.
Camera list shows the IP address of each device.
Bug fixes
GigE Transport Layer
The parameter BUFFER_INFO_DELIVERED_IMAGEHEIGHT is filled correctly.
Added functionality of Action Commands.
Bug fixes
Changes in Vimba 2.0.0¶
Vimba Setup
Added Vimba Viewer Guide document
Improved documents, new layout
Vimba C
Added functionality of loading and saving camera settings from / to XML
Bug fixes
Vimba C++
Added functionality of loading and saving camera settings from / to XML
Bug fixes
Vimba Image Transform Library
Support for conversion from BayerXX10,12 formats to 2 byte output formats (RGB[A], BGR[A])
Added interface functions VmbSetImageInfoFromInputParameters and VmbSetImageInfoFromInputImage
Vimba Viewer
Enabled making use of load / save settings functionality
Added tabsheet widgets for Brightness, ROI, Autofunction ROI, Trigger IO, Color
Bug fixes
USB Transport Layer
Minor bug fixes
GigE Transport Layer
Reworked and improved filter driver
Vimba Class Generator
Changes for Camera Link support (affects Windows only)
Changes in Vimba 1.4.1¶
Package for ARMv7
Support of USB Transport Layer
Package for other Linux systems
Support of USB Transport Layer
Improved documentation
Vimba C
Extended camera support (e.g. float increments)
Stability improvements
Improved some examples
Bug fixes
Vimba C++
Extended camera support (e.g. float increments, needs Vimba C 1.4)
Improved error handling
Improved some examples
Added and improved examples
Bug fixes
Vimba Image Transform Library
Added support for PFNC 10p and 12p formats
Improved the documentation
GigE Transport Layer
Improved stability on high traffic networks
Bug fixes for multi-camera usage and incomplete cleanup
Fixed range of GevHeartbeatInterval and GevHeartbeatTimeout
Vimba Viewer
Added open camera by ID
Added endianness switch in direct register dialog
Many bug fixes
Vimba Class Generator
Small improvements
Changes in Vimba 1.3.0¶
Package for ARMv7 (new)
Support of Vimba C API
Support of Vimba C++ API
Support of GigE Transport Layer
Package for other Linux systems
Added a Vimba Tour document and a Vimba Quickstart Guide
Improved the other documents
Added examples for Vimba C and C++
Added an OpenMP version of the Vimba Image Transform Library
Vimba C 1.3.0
Fixed feature access for ancillary data
Made device discovery blocking
Added system feature GeVDiscoveryAllDuration for adjustable waiting time
Fixed issues with mixed feature names
Bug-fixes for improving stability
Vimba C++ 1.3.0
Fixed feature access for ancillary data
Changes caused by bug fixes in Vimba C
Vimba Image Transform Library 1.2.0
Allowed more input for VmbSetImageInfoFromString
Corrected return codes
Removed transformations to Mono10/12/14 and big-endian data
Vimba Viewer 1.1.3
Improved handling for GigE camera list changes
Fixed issues around saving images
GUI usage improvements
GigE Transport Layer 1.3.1
Fixed GenTL compliance: Changed the Device ID from the serial number to a MAC-based ID. This changes the way all APIs (C, C++ and .Net) identify the cameras
Added a document for GigE camera features
Changed the supported GenTL version to 1.3 (e.g. new feature categories BufferHandlingMode and StreamInformation)
Separate features for heartbeat timeout and heartbeat interval
Adjustable device discovery waiting time
Fixed issues with similar serial numbers
Fixed issues with many network interfaces
Vimba Class Generator
Minor changes to appearance and documentation
Changes in Vimba 1.2.0¶
Vimba C 1.2.0
Version 1.2.0 is only compatible to AVT GigE TL Version 1.2.0 onwards
Name independent search for AVT transport layers
Made EnumEntries’ “pIsImplemented” condition equivalent to “pIsAvailable” to mimic the behavior of GenICam reference implementation
Vimba C++ 1.2.0
Fix for opening camera by IP address
Vimba .NET 1.2.0
Fix for 64bit version attempting to load 32bit transport layers
Fix for opening camera by IP address
Vimba Viewer 1.1.1
SFNC Features directly beneath the root category get listed
Many new pixel formats available for histogram support
GigE Transport Layer 1.2.0
Improved performance in case of many events
Restriction to eight cameras removed
Corrected Heartbeat feature
Fixed support for small packets