Vimba X for Windows Release Notes#

Version: 2026-3

Summary#

Main changes in this release:

  • RDMA TL first release

Transport Layer

Version

GigE Transport Layer (VimbaGigETL.cti)

1.11.0*

USB Transport Layer (VimbaUSBTL.cti)

1.7.1

Camera Simulator TL

1.0.1

RDMA Transport Layer (sv_gev_rdma_tl.cti)

2.5.9.3369

CL Config TL (VimbaCLSerialTL.cti)

2.0.0

APIs

Version

VmbC API (VmbC.dll)

1.3.2*

VmbCPP API (VmbCPP.dll)

1.3.2*

VmbNET API

1.3.4*

VmbPy API

1.2.3*

Image Transform Library (VmbImageTransform.dll)

2.3.0

VmbNUC API

1.0.1

Drivers

Version

Vimba X GigE Filter Driver

2.5.13

Tools

Version

Vimba X Viewer

1.4.6*

Vimba X Firmware Updater

2.3.2*

Vimba X Driver Installer

2.1.0

GCT Viewer

3.3.2

SVCam Assistants

1.0.0

Application Launcher

1.0.0

* Changed in this release of Vimba X

Hardware requirements#

PC or laptop with 64-bit x86 processor or better.

GigE cameras#

A built-in Gigabit Ethernet network interface or Gigabit Ethernet network card (one or more) is required.

Note for IP configuration: By default, IP Configuration Mode is set to DHCP. You can use the IP Configuration dialog of Vimba X Viewer to apply changes or to force the IP address.

Allied Vision USB cameras#

A built-in USB 3.0 (or higher) controller for PCI Express bus is required.

Testing has been performed on host controllers that are based on Asmedia chip sets. The driver may run on host controllers that are based on chip sets from other vendors, too. If there are any problems please feel free to contact our Technical Support.

Correlations with other Allied Vision Software Packages#

You can install and use Vimba and Vimba X on the same host. We recommend using our GigE filter driver with Vimba X or Vimba only.

Supported operating systems#

Vimba X was tested with:

  • Windows 10 21H2 LTSC

  • Windows 11 24H2 Pro

Known issues#

Setup:

  • Vimba X driver installation disconnects VPN. For a smooth installation, please disconnect VPN before installing Vimba X.

  • To install the USB driver, please connect your Allied Vision USB camera before starting Vimba X installation. After installation, you can always use Vimba X Driver Installer.

  • During installation, Vimba setup configures some environment variables that are - among others - used when compiling the examples. In order to use the new environment variables, it might be necessary to restart Microsoft Visual Studio, log off, or even restart the operating system.

  • In some cases, the Vimba X installer message about successfully installed drivers is incorrect.

Vimba X APIs:

  • When API startup and shutdown is performed excessively within the same process, camera initialization may fail sporadically, which may cause exceptions. We recommend to have only one API session during one process.

  • Load/Save Settings: Not all LUT settings are saved.

GigE Filter Driver:

  • If Vimba and Vimba X are installed on the same system: The Filter Driver provided with Vimba X overwrites Vimba’s Filter Driver. If you still work with Vimba: Use the included Driver Installer to deactivate and activate the correct Filter Driver.

  • Using other filter drivers additionally to the included GigE Filter Driver (including the Filter Driver of the Vimba SDK) may cause issues, even a blue screen.

  • Disabling the Vimba GigE Filter Driver while it is in use might lead to unexpected behavior up to blue screen.

GigE Transport Layer:

  • A change of the available camera access modes cannot be reported for cameras in different subnets or with malconfigured IP addresses.

  • GigE cameras may be listed on a wrong Ethernet interface.

  • If many dropped frames occur especially with a small ROI, set GVSP Timeout to a higher value.

5 GigE Vision cameras:

  • Unplugging an USB device while the camera is streaming may cause lost frames, especially when the socket driver is used.

Vimba X Viewer:

  • With some camera models, the message “Vimba X Viewer is not responding” appears for a few seconds when the camera is opened.

  • If the IP address is changed within the same network, the camera list doesn’t update automatically. Please click the Refresh button.

  • Sporadic issue: When multiple opened GigE cameras are disconnected at the same time while no other camera stays connected to the very same NIC, the Viewer’s camera windows stay open.

  • Legacy cameras: The All tab supports all legacy cameras. The other tabs only support GenICam-compliant features.

  • Moving test image from Camera Simulator: With Bayer pixel formats, the color interpolation causes wrong colors.

Examples:

  • If a camera is already open, sometimes a misleading error message occurs (“Bad parameter”).

  • The ListFeatures example does not list all Interface features.

  • Sporadic issue of the AsynchronousGrab and Chunk example: stopping the stream causes an exception.

Changes and release history#

Changes in Vimba X 2026-3#

VmbC:

  • Windows dlls are now signed with a digital signature

VmbCPP:

  • Internal changes, no impact on usage

VmbNET:

  • Fixed: Unhandled Exeption in Camera Event Callback

  • Fixed: Recovery after Ethernet loss while the camera is streaming

VmbPy:

  • Internal changes

RDMA TL:

  • First release

GigETL:

  • GigExpress support (Linux x86_64 only)

Vimba X Viewer:

  • Added a warning (not applicable to Windows)

Vimba X Firmware Updater:

  • Minor changes

Changes in Vimba X 2026-2#

VmbC:

  • New function reference

VmbCPP:

  • New function reference

VmbNET:

  • New function reference

VmbPy:

  • New function reference

VmbNUC:

  • New function reference

Vimba X Viewer:

  • Bugfix (not applicable for Windows)

GigETL:

  • Fixed: Reset of expected GevHeartbeatTimeout value.

Application Launcher:

  • New component

GCT Viewer:

  • New component

SVCam Assistants:

  • New components

Changes in Vimba X 2026-1#

VmbC:

  • Lazy feature initialization for faster camera listing

VmbCPP:

  • Internal changes

VmbNET:

  • Minor internal changes

VmbPy:

  • Fixed: VmbPy error codes differ from VmbC

  • Several minor bug fixes

  • Deprecated support for Python <3.10

VmbNUC:

  • First release, Goldeye and Goldeye Pro support

USBTL:

  • Minor internal changes

Camera Simulator TL:

  • Several bug fixes

CL Config TL:

  • First release in Vimba X (migrated from Vimba)

Vimba X Viewer:

  • Minor internal changes

Firmware Updater:

  • Added info message if the update requires a hard reset (Alvium firmware v15)

Changes in Vimba X 2025-3#

VmbC:

  • New logging implementation

  • OpenCV bridge header

VmbCPP:

  • OpenCV bridge header

  • VmbCPP example for Open CV bridge

VmbNET:

  • Minor bugfixes, updated README.md

  • DeinterlaceFrame is available

VmbPy:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

  • DeinterlaceFrameis available

  • Improved performance of AllocationMode.AnnounceFrame

USBTL:

  • Minor internal changes

GigETL:

  • Added IP configuration features for Allied Vision legacy cameras (Manta, Mako, Goldeye, Prosilica GT)

Filter driver:

  • Internal changes, no changes for users

Driver installer:

  • Adaptions for new filter driver version

SVS-Vistek RDMA TL (Beta)

  • Transport layer with RDMA support for SVS-Vistek cameras (Beta)

  • Restrictions of this beta version:

    • AllocAndAnnounce is not available

    • Open by IP is not available

    • If VmbC is not used, the TL is not available

Vimba X Viewer:

  • Minor bugfixes

Image Transform Library:

  • Added function VmbDeinterlaceFrame() to support IMX900 sensor HDR processing

Firmware Updater:

  • Updating more than one selected Goldeye Pro camera is now possible

Changes in Vimba X 2025-2#

VmbC:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

VmbCPP:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

VmbNET:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

  • Several minor bugfixes

  • Adjusted Nuget Package ID to include platform specifier

VmbPy:

  • Supports legacy events and chunk (tested with Manta, Mako, Goldeye and Prosilica GT)

USBTL:

  • Added Stream leader/trailer received events

  • Added endpoint-flushing

USB driver:

  • Changed underlying driver (no impact on Vimba X or camera usage)

GigETL:

  • Minor bugfixes

Vimba X Viewer:

  • Adaptations for Goldeye and Goldeye Pro support

Firmware Updater:

  • Adaptations for Goldeye Pro support

Changes in Vimba X 2025-1#

VmbC:

  • Minor bugfixes

VmbCPP:

  • Minor bugfixes

VmbNET:

  • New API

VmbPy:

  • VmbC (+ GenAPI dependencies) included in Python wheel to make VmbPy self-contained

Image Transform Library:

  • Exported new function VmbGetCompatiblePixelFormat

GigETL:

  • Adjustments for support of future cameras

CSITL:

  • Bug fixes

  • JetPack 6 support

Vimba X Viewer:

  • Minor bug fixes

Changes in Vimba X 2024-1#

VmbC:

  • Loads transport layers found in the same directory as VmbC.dll

  • Improved logging

VmbCPP:

  • Minor bug fixes

VmbPy:

  • Minor Bugfixes

  • VmbPy type hint improvements for better autocompletion in IDEs

GigETL:

  • Breaks compatibility with Vimba 6 (Vimba 6 Config mode not working anymore with latest Vimba X GigETL)

  • Cameras from SVS-Vistek are enabled by default

  • Marked old statistic features as “deprecated”

  • Minor bug fixes

Filter driver:

  • Minor bugfixes

USBTL:

  • Added new GenTL Buffer Info “BUFFER_INFO_DATA_SIZE”

  • Updated uriparser to 0.9.8

Vimba X Viewer:

  • “Image Format tab” including Multi ROI

  • Event Viewer window access has moved to icons above the image

  • Image Processing tab:

    • Sobel horizontal/vertical was interchanged in the camera firmware until firmware 13.x and the Viewer GUI compensated for that. With firmware 14, this is corrected in the camera and aligned to firmware 14 in the Viewer GUI.

  • Better performance when using high frame rates > 1000 fps

  • Minor bugfixes

Firmware Updater:

  • Fixed: With some Alvium camera models, the firmware update may take up to 5 minutes.

Image Transform Library:

  • Added support for 3x3 debayering of packed formats

Changes in Vimba X 2023-4#

VmbC:

  • Added macOS support

VmbCPP:

  • Added macOS support

VmbPy:

  • Added macOS support

ImageTransform:

  • Added macOS support

USBTL:

  • Added macOS support

  • Added Event support

Filter Driver:

  • Bug fixes

Vimba X Viewer:

  • Added macOS support

  • Added Sequencer tab

Vimba X Firmware Updater:

  • Added macOS support

GigETL:

  • Improved Adjust PacketSize

Changes in Vimba X 2023-2#

VmbC:

  • Fixed: Open camera by IP may take 15s

  • Added Exclusive Access mode

VmbCPP:

  • Fixed: Open camera by IP may take 15s

VmbPy:

  • Fixed: Open camera by IP may take 15s

  • Fixed type hints for Python <=3.7.5 and =3.8.0

  • Updated AccessMode enum for consistency with VmbC

  • Added option for visibility level to list_features.py

GigETL:

  • Fixed: Vimba X freezes if the NIC is disabled during image acquisition.

GigE Filter Driver:

  • Supports extended status codes packet resend

USBTL:

  • Improved: standard conformity of resend for control channel commands

Changes in Vimba X 2022-1#

VmbC:

  • New API (similar, but not compatible to VimbaC)

VmbCPP:

  • New API (similar, but not compatible to VimbaCPP)

VmbPy:

  • New API (similar, but not compatible to VimbaPython)

Image Transform:

  • Added supported transformations (supports pixel formats of NET cameras)

  • Renamed VmbGetVersion to VmbGetImageTransformVersion

  • VmbSetImageInfoFromString: removed stringLength parameter

Vimba X Viewer:

  • New Viewer (based on Vimba Viewer)

  • Additional features: Chunk support, 5x5 Matrix, Scheduled Action commands

GigETL:

  • Display name: AVT GigE TL (instead of Vimba GigE TL)

  • Scheduled Action Commands support

  • Chunk support

Filter Driver:

  • Chunk Support

  • Bug fixes

USBTL:

  • Display name: AVT USB TL (instead of Vimba USB TL)

Driver Installer:

  • The version was incremented to 2.0.0 because of internal changes (no functional changes for the user)