Vimba GigE TL Release Notes#
Version: 1.11.0
Components and Version Reference#
Component |
Version |
|---|---|
GigE Transport Layer (VimbaGigETL.cti) |
1.11.0 |
Vimba GigE Filter Driver |
2.5.13 |
Hardware Requirements#
PC or laptop with 1 GHz x86 processor or better.
ARMv8-compatible 64-bit embedded system, for example, Jetson Xavier.
MacBookPro or Mac mini with M2 chip
Remark (for macOS, see the macOS release notes):
When using Allied Vision GigE cameras, a built-in Gigabit Ethernet network interface or Gigabit Ethernet network card (one or more) is required.
Installation#
The Vimba GigE Transport Layer is part of the Vimba X SDK. Linux: For instructions on how to install this module, please refer to the Vimba X for Linux or ARM64 Release Notes.
Correlations with other Allied Vision Software Packages#
You can install and use Vimba and Vimba X on the same host. Windows: We recommend using our GigE filter driver with Vimba X or Vimba only.
Known Issues#
When experiencing trouble with image acquisition on Linux, try to increase the priority of your application with “sudo -E nice -n -20
”. A change of the available camera access modes cannot be reported for cameras in different subnets or with misconfigured IP addresses.
GigE cameras may be listed on a wrong Ethernet interface.
If many dropped frames occur especially with a small ROI, set GVSP Timeout to a higher value.
GigE Filter Driver:
If Vimba and Vimba X are installed on the same system: The Filter Driver provided with Vimba X overwrites Vimba’s Filter Driver. If you still work with Vimba: Use the included Driver Installer to deactivate and activate the correct Filter Driver.
Using other filter drivers additionally to the included GigE Filter Driver (including the Filter Driver of the Vimba SDK) may cause issues, even a blue screen.
Disabling the Vimba GigE Filter Driver while it is in use might lead to unexpected behavior up to blue screen.
Changes and release history#
Changes in version 1.11.0#
GigETL:
Added GigExpress support
Changes in version 1.10.4#
GigETL:
Fixed: Reset of expected GevHeartbeatTimeout value.
Changes in version 1.10.3#
GigETL:
Added IP configuration features for Allied Vision legacy cameras (Manta, Mako, Goldeye, Prosilica GT)
Filter driver:
Internal changes, no changes for users
Changes in version 1.10.2#
GigETL:
Minor bugfixes
Changes in version 1.10.1#
GigETL:
Adjustments for support of future cameras
Changes in version 1.10.0#
GigETL:
Breaks compatibility with Vimba 6 (Vimba 6 Config mode not working anymore with latest Vimba X GigETL)
Cameras from SVS-Vistek are enabled by default
Marked old statistic features as “deprecated”
Minor bug fixes
Filter driver:
Minor bugfixes
Changes in version 1.9.5#
GigETL
Improved Adjust PacketSize
Changes in version 1.9.3#
GigETL
Added Event support
Filter Driver:
Bug fixes
Changes in version 1.9.2#
GigETL
Fixed: Vimba X freezes if the NIC is disabled during image acquisition
Set camera to Extended ID mode if supported
Support Extended Status Codes Packet Resend
GigE Filter Driver:
Supports extended status codes packet resend
Changes in version 1.9.1#
GigETL
Display name: AVT GigE TL (instead of Vimba GigE TL)
Scheduled Action Commands support
Chunk support
Filter Driver
Chunk Support
Bug fixes
Changes in version 1.9.0#
GigETL
Changed behaviour of endianess handling (values must match host endianness in little-endian), for better compatibility with third-party software. Affected features that now have a changed byte order:
Config Mode
IP-related features including MulticastIPAddress
Action Commands
New feature DeviceUpdateTimeout (only applicable of GigE discovery is switched to Broadcast)
New GVSPMaxLookBack default value (0 instead of 1) for improved packet resend handling
Fixed: High memory usage during performance bottleneck (Nonpaged pool growing with multiple GigE cameras)
Fixed: Action commands caused an error message in the console log
Fixed: MulticastIPAdress range, better compatibility with third-party software
GigE Filter Driver
Reduced memory allocations
Hidden statistics
Changes in version 1.8.2#
GigETL and GigE Filter Driver
Fixed: Vimba Viewer did not show single frame acquisitions (5 GigE)
Improved timeout handling (5 GigE)
Fixed limitations of certain GVSPPacketSize values
New GigETL feature: GVSPHostReceiveBufferSize (SO_RCVBUF, usable with the socket driver only) replaces GVSPHostReceiveBuffers (which is still usable in existing applications).
Changes in version 1.8.1#
Prepared for use with 5 GigE Vision cameras
Changes in version 1.8.0#
Standard-compliant ForceIP features instead of Allied Vision custom features
Prepared for use with extended IDs
Changes in version 1.7.1#
Improved resend handling
By default, packet resends are enabled
Other bug fixes
Vimba Driver Installer
Internal changes
Changes in version 1.7.0#
GenTL 1.5 support
Changes in version 1.6.0#
Fixed: GVSPPacketSize now updates as expected (Linux)
Other minor bug fixes
Vimba GigE Filter Driver
Windows 10: Improved compatibility and performance with third-party filter drivers.
Installer and driver
New certificates for installer and driver (Windows 7, Windows 8, and Windows 8.1)
Changes in version 1.5.0#
Added functionality for Action Commands
Fixed sending packet request after invalid timeout on Linux
The parameter BUFFER_INFO_DELIVERED_IMAGEHEIGHT is filled correctly
VimbaGigEFilter (Windows 10 x64/x86 only):
Fixed incompatibility with Intel 10 Gbit Ethernet cards (520/540/710)
Changed buffer list handling, driver removes streaming packets from buffer list:
Decreases system load formerly caused by stream packet duplication
Prevents additional system load when firewall is enabled
Does not allow Wireshark to see stream packets
Packet resend system load minimized
Fixed missing filterclass in driver inf
Fixed double counting of received packets
Fixed incompatibility with wireless network cards (removed binding to WAN)
Fixed incompatibilities with VPN connections (filter now optional)
Changes in version 1.4.4#
-Bug fixes
Changes in version 1.4.2#
Bug fixes
Changes in version 1.4.1#
Solved cases where network problems led to a lost camera
Fixed range of GevHeartbeatInterval and GevHeartbeatTimeout
Bug fixes for multi-camera usage and missing cleanup
Changes in version 1.3.1#
Support of GenICam GenTL standard 1.3
New GenTL SFNC feature categories BufferHandlingMode and StreamInformation
Separate features for heartbeat timeout and heartbeat interval
Adjustable device discovery waiting time
Fixed issues with alike serial numbers
Fixed issues with many network interfaces on Linux
Small bug-fixes to the Driver Installer
Changes in version 1.2.0#
Improved performance in case of many events
Restriction to eight cameras removed
Corrected Heartbeat feature
Fixed support for small packets
Changes in version 1.1.0#
Added feature DiscoveryBroadcastMode to the Interface module
Changed the documentation format to PDF
Slight changes for Linux compatibility